Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Category:CCS UniFlash

From Texas Instruments Wiki
Jump to: navigation, search
Uniflash v4.PNG

Overview

Universal Flash Programmer for Texas Instruments devices. Provides a single interface for programming Flash memory and executing Flash based operations on supported targets.


UniFlash v4

See the UniFlash v4 Quick Guide for help in getting started. UniFlash is available in the cloud as well as a desktop application.

Cloud Version Access here.

Desktop Version(s):

  • Version - 4.5.0.2056

Windows DownloadLinux DownloadMac Download

Notes

  • For CC3100/CC3200 and Sitara, please continue to use UniFlash v3.4.1 (see below).
  • If you download the Windows package with Internet Explorer you may need to rename the file to an executable (.exe)
  • IMPORTANT! Uniflash 4.5.0 has issues installing XDS100 device drivers in a machine with no prior Uniflash or CCS install. Please check this e2e post for details to workaround this scenario.


Getting Started

  • (Coming soon ...) For MSP and SimpleLink Bootloader Programming Using UniFlash, please refer to the User Guide

--




Supported Devices and Release notes

The list of supported devices can be found in the Latest Release Notes.


Support

Please post questions, comments, recommendations to the TI E2E Community:
http://e2e.ti.com/support/development_tools/code_composer_studio/default.aspx


Troubleshooting

Please refer to the CCS Linux Host Support page for more information on Linux dependency requirements:
http://processors.wiki.ti.com/index.php/Linux_Host_Support_CCSv8

The SimpleLink CC31xx/CC32xx families require Python2.7 on Linux. If UniFlash hangs when starting a session for these families, please install python-minimal using apt-get.

In addition, UniFlash requires libudev.so.0, which may no longer be available on some distributions. You can, however, create a symlink from libudev.so.1 to libudev.so.0. For example:

sudo ln -sf /lib/x86_64-linux-gnu/libudev.so.1 /lib/x86_64-linux-gnu/libudev.so.0




Licensing Information

Please refer to the full license text: File:Uniflash v4 license.zip.


Previous Releases

Release Notes Archive/Download Links for all released versions: Release Notes Archive

For CC3100/CC3200 and Sitara please use v3.4.1 below.

Previous UniFlash version
Version Download link / Release Notes Comments
3.4.1.00012 Release Notes/Download This version supports CC3200, and Sitara AM335x and AM437x processors.

Licence information for version 3: File:UniFlashLicensing.zip

Subcategories

This category has only the following subcategory.