Category:Simulator Traces
From Texas Instruments Embedded Processors Wiki
Contents |
Simulator Traces
Simulator provides the following traces to capture and analyze CPU activity.
- Packed Differential Address and Time Stamp (PDATS) Trace
- Program Counter Discontinuity Trace (PCD) Trace
- Execute Packet (EP) Trace
Generate Traces using Scripting/Loadti
In CCSv4, simulator traces can be generated using DSS scripting or Loadti. Loadti is the generic script built on top of DSS scripting.
Loadti Simulator Enhancement
Loadti is available along with CCSv4 at "<CCSv4 install directory>\CCSv4\DebugServer\scripting\examples\loadti".
- Loadti simulator enhancement to generate traces - Loadti.zip
- Unzip the loadti.zip file at "<CCSv4 install directory>\CCSv4\DebugServer\scripting\examples\loadti" to get the enhancements.
Loadti Command Options
Loadti support the following set of options. To get this options use "--help" option in command line.
Usage: loadti [OPTION]... [OUT_FILE] [ARGUMENT]... Load OUT_FILE executable to TI target and run, passing ARGUMENT(s) to main. Mandatory arguments to long options are mandatory for short options too. Options: -a, --async-run -c, --ccfg-file=CCS_CONFIG_FILE -o, --o=out_file -h, --help -l, --load -mlr, --mem-load-raw="PAGE,ADDR,FILE,TYPE_SIZE,BYTE_SWAP" -mld, --mem-load-dat="PAGE,ADDR,FILE,LEN" -msr, --mem-save-raw="PAGE,ADDR,FILE,LEN,TYPE_SIZE,BYTE_SWAP" -msd, --mem-save-dat="PAGE,ADDR,FILE,LEN,IO_FORMAT,APPEND" -n, --no-profile -q, --quiet -r, --reset -s, --stdout-file=FILE -t, --timeout=VALUE -v, --verbose -x, --xml-log=FILE -trace=<trace1>:<trace2> - Enable Simulator traces. Trace options on Simulator - PCDT, PDATS & EPT -start_trace=<label_1>:<label_2>:<PC address> - Enable trace from start label or PC address. Can specify multiple labels/PC Address -end_trace=<label_1>:<label_2>:<PC address> - Disable trace at end label or PC address. Can specify multiple labels/PC Address
Loadti Usage
Loadti enables you to collect simulato traces for entire run or for selected function or between to any to PCs.
- Simple usage to generate trace for the full simulation.
loadti -c=tisim_tci6484_ca.ccxml –o=test1.out –trace=PCDT:PDATS:EPT
- Trace generation between two labels.
loadti –c=tisim_tci6484_ca.ccxml –trace=PCDT:PDATS –start_trace=startTrace –end_trace=endTrace –o=test1.out
- Trace generation between labels & PC address
loadti –c=tisim_tci6484_ca.ccxml –trace=PCDT:PDATS –start_trace=startTrace1:startTrace2:0xe0001456 –end_trace=endTrace1:endTrace2:0xe0001576 –o=test1.out
Note: PC address should be suffixed with ‘0x’
Note: PDATS/PCDT need to be enabled seperately in the configuration file. Refer the PDATS & PCDT on how to enable them in simulator configuration file.
Sample Simulator Configuration File
CCSv4 sample configuration file with PCDT & PDATS enabled in the configuration file - Sample_confile_file.zip
Simulator configuration file included
- C6416 Cycle Accurate Simulator
- C6416 Functional Simulator
- TCI6484 Cycle Accurate Simulator
Pages in category "Simulator Traces"
The following 5 pages are in this category, out of 5 total.