Chronos High 5 Me!
From Texas Instruments Embedded Processors Wiki
Follow us on twitter: TI_HighFive
Contents |
Authors
- Aldo Briano (a-briano@ti.com)
- Ryan Boesch (ryanboesch@ti.com)
- Brian Elies (elies.brian@ti.com)
Features
- High 5 Detection and Counter on Chronos Watch
- Automatic posting to Twitter and letshigh5 website
- Website Leader Boards
- Social Network integration
Let's High 5 Social Network
The Web 2.0 and social networks have revolutionized how we communicate, interact with each other, and take on our daily lives. With more than 500 million users on Facebook, there is no doubt that the market opportunity in social media / applications is huge. The emergence of the Iphone, smartphones, and other internet enabled phones have created on us a psycological attraction to express through blogs, tweets, etc. There are networks where people can post their current location, pictures, their current status, etc.
Wearable electronics bring forth innumerous applications and potential for social media. Let's High 5 takes advantage of ez430-Chronos' built in sensors and features to provide a unique application that cannot be implemented using a traditional iPhone or smartphone. By using the acceleration data in the wrist of a person, our application can detect its movement and decipher whether the person has just high 5ed.
The value our application brings to Texas Instruments is remarkable. We want to remove the misconception that Texas Instruments = Calculators. For the least minimum, we would like to be seen in public light as Texas Instruments = Calculators + Super Awesome Watch. With Let's High 5, TI can expose its technology through social media and a fun popular application suitable for anyone. Wouldn't TI want to be the reason for the high 5 to regain popularity?
Our website features a simple style, with top 10 high five leader board. Here, people can expose their awesomeness and popularity from the amount of high 5s they have received. Even more interesting is the automatic integration of the watch and Twitter, where your current high 5s will be tweet and exposed to the world. Nevertheless, the potential of our social application is endless.
Imagine logging in to your favorite social network and seeing your news feed filled with your closest friends recent high 5s. Imagine meeting people simply through high 5s. Instead of getting their name, or looking them through facebook, a high 5 between two strangers with the chronos could automatically trigger an exchange of social profiles. This way after you high 5 a stranger in a bar you'll get a friend request and you have expanded your social network. Imagine combining geolocation data of every high five and being able to map geographically every high 5 in realtime. This way you can see where your friends are having the most fun, or what bar currently has the most happy people. With the ez430-Chronos, this and much more is possible.
Visit us, leave us your comments on how to improve: http://www.letshighfive.com. Follow us on twitter: http://www.twitter.com/TI_HighFive.
High Five Detection Algorithm
Several methods for the detection of high fives were investigated throughout the course of this project. One of the first methods we tried was to look at the overall magnitude of the acceleration. If the magnitude of the acceleration exceeded a certain threshold the program interpreted the event as a high five. While this approach was computationally simply and provided reasonable accurate high five detection, it was difficult to reject other events such as clapping and and shaking.
Next we investigated using the altimeter in an attempt to detect when your hand was elevated. However the low sample rate of the altimeter ment that it was not suited to this application. In addition an elevated hand was typically only one code different from a low hand.
Finally we began to investigate correlation based high five detection. In this approach the unknown event is compared to a known event. If the two events are similar the correlation between them will be large. With this approach an event can have a high magnitude but still have a low correlation. To generate the know events we sampled different high fives and averaged the events for each axis where x and y are the sample means of X and Y, sx and sy are the sample standard deviations of X and Y.
The data was processed and plotted using MATLab. The following screenshots depict the mean behavior of the high 5 in each of the different axis. A trend is observed and precisely that behavior is being used to filter out any non-high5.
Fig. 1: Matlab plots for the average of a high 5 in each axis
After the correlation algorithm was established and tested, different data points were used to establish a threshold for a high 5. This filters out any behavior in each axis different from the ones depicted in the figure above. Before implementing the algorithm in the ez430-Chronos, a program in LabView was written to test and visualize its performance in real time. The following screenshots show the main features of the circuit block. The source code is found below.
Fig. 2: First three plots are realtime accelerometer data, bottom plot is result of correlation. Fig. 3: High 5 behavior and the coefficients for each axis
Usage Instructions
Labview Code
Installation Instructions
- Download and install the Labview Evaluation Software
- Download and install NI-VISA
- Download and install the drivers for the USB RF module
- Download the Labview Source Code
- Open the device manager and locate the COM# for the TI C1111 USB RF module, type this into the Serial Port control located on the front pannel of the Hi 5 Me.vi
How to Collect Acceleration Data
To collect acceleration data from the watch first open Hi 5 Me.vi and click the run arrow in the upper left corner of the front panel. If a watch is within range the connected light will light up. Next go to the ACC menu in the watch and press the lower right button to begin sending data. Click the Start ACC Data Collection button to begin collecting data from the watch. The first 3 graphs display the X, Y and Z acceleration data. When the value in the correlation graph exceeds the detection threshold the High Five! indicator will light up. To stop collecting data simply press Stop ACC Data Collection button.
Python GUI
Installation Instructions
- Download and install python from (Link)
- Download Python Source from below
Tutorial
Install, setup RF access point.
Press connect.
Connect watch.
Programing the Watch
Installation Instructions
Tutorial
Go to the Hi 5 mode on the watch by repeatedly pressing the lower left button.
Start high 5 mode by pressing the right lower button. (a heart and your total high 5 count should display).
Once you want to send your high 5s to the PC, click the right lower button again.
Future Work
Improve the High Five detection by having correlation functions for other events that are similar to high fives such as punches and clapping. The algorithm can compare the correlations of different events and then select the highest correlation. This way we can provide a better detection algorithm while filtering other types of movements.