Combining executable files

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   


Contents

Overview

TI customers use the TI compiler toolset to build application(s) into an executable file that can be loaded and executed on the TI devices. The result of this application build process is usually a single executable. If an RTOS is used, it is statically linked in with the applications to create a single executable. This executable is loaded on the device for execution.

There are many ways to load the executable on the device. One way is to ROM mask the executable’s load image on the device. Such ROM image can be executed in place or copied to RAM and executed. Currently the customers provide a single executable file to TI for ROM masking. The load image is represented in the executable file by initialized sections and their load addresses. Data from the initialized sections are masked in the device ROM at their specific load addresses.

Creating a single executable for ROM masking is not the only application development model anymore. Now executables are built and tested to run on multiple sockets. Customers build applications, boot loader and configuration data as separate executables and test them. Then they choose a set of executables as complete application to be ROM masked. This means multiple executable files are to be delivered for ROM masking. Though the ROM masking process can handle multiple executables for a single socket, the customers want to retain control over how these executables are combined for ROM masking. A mistake in ROM masking is very expensive and the customers want to avoid any potential problems. Delivering a single file for ROM masking has worked well and customers want to combine these executables at their end and deliver a single file for ROM masking.

The executable COFF or ELF file has much more information than what is required for ROM masking. For example, the symbol table, the relocation entries and the uninitialized sections are not used during ROM masking. Only the initialized sections and their load addresses are required. If we can copy all the initialized sections from the executables into a single file then such a file can be delivered for ROM masking. That is, tool support is needed to combine the load images from multiple executables into a single file. Since currently TI COFF or ELF files are delivered for ROM masking, the combined load image file should use TI COFF or ELF object format. Converting an executable file into a load image object file has other applications. For example, such an object file can be used to include an executable as a boot image in a subsequent link step.

Solution

The hex converter previously accepted an executable file and generates hex data from the initialized sections. It supports specifying a memory range and has the basic framework to create the load image file. The hex converter has been enhanced to generate the load image object file in TI COFF or ELF format from one or more executable files. Please refer to the Assembly Language Tools User’s Guide (SPNU118D) for more details on hex converter. Support for this capability has been added the the hex converter utilities in the TMS470 Code Generation Tools 4.6.0 and C6000 Code Generation Tools 7.0.0

Load Image Object File Generation

The hex converter supports many output formats: TI-Tagged, ASCII-hex, Intel, Motorola-S, Tektronix, etc. Support is now available to generate a load image object file. The load image object file’s format is determined by the input files. The load image format can be invoked with the following option

--load_image: Create a load image object file with format the same as the input files

Accept Multiple Input Files

The hex converter previously accepted a single input object file. Support has been added to accept one or more input object files. ELF and TI COFF object files cannot be mixed as input files. All currently supported formats accept multiple files as input.

The SECTIONS directive has been extended to accommodate multiple input files. Previously the directive had the following format:

SECTIONS
{
   sname: paddr=<value>
}

The directive has been extended to support multiple files by allowing the file name to be specified along with the section name. This is may be useful in the case of generating load image objects, but it is needed if multiple file support is added for all output formats. The format is as follows:

SECTIONS
{
   fname(sname): paddr=<value>
}

Load Image Section Formation

The load image sections are formed by collecting the initialized sections from the input executables. There are two ways the load image sections are formed as described below.


ASIDE: TI COFF executables only contain sections. ELF executables on the other hand contain segments and need not have sections. However, the TI ELF executables contain both segments and sections. Hence, in this proposal, we consider input sections from ELF executables for copying into load image sections. When an ELF executable only contains segments, the segments are used. However, the SECTION directive of the HEX converter will be ignored.


Using Address Ranges

The hex converter supports the ROMS directive to let the user specify an address range. The ROMS directive has the following format:

ROMS
{
  romname : [origin=value,] [length=value,] [romwidth=value,] 
            [ memwidth=value,] [fill=value] [files={filename1, filename2, ...}]
  ...
}

When using –load_image, the –image option must be specified. If it is not, an error will be generated. The keywords origin and length define an address range in memory. This memory range is given a name (romname above). When the user specifies the ROMS directive to build a load image object, a single load image section is created for this memory range. Any holes in this range are filled using the default value zero. Alternatively, the user can use the keyword fill to specify a fill value.

Default Load Image Section Formation

When no ROMS directive is used, the load image sections are formed by combining contiguous initialized sections in the input executables. The hex converter will consider input sections with holes smaller than target word size to be contiguous. For example, assume a TMS470 target which has 4-byte target word. Also assume an input section ends at address 0x3FFD and the next input section starts at 0x4000. Though there is a hole of 2 bytes, these input sections are considered contiguous.

Load Image Section Name

As was discussed above, there are two ways to form the load image sections. The load image section name in each case can be controlled differently.

When Using ROMS Directive

As mentioned above, a ROMS directive specifies memory range which results in a single load image section. Also each memory range has to have a name (romname above). This memory range name can be used to name the load image section. In the following example "App1" designates the name of the load image section for that memory range.

ROMS
{
   App1 : [origin=value,] [length=value,]
}

When Using Default Section Formation

In the absence of ROMS directive, the hex converter uses default load image section formation by collecting contiguous initialized sections. In this model, the user can specify a section prefix using a command line option. The hex converter supports the --section_name_prefix=<prefix> option. When this option is specified, the hex converter names the load image sections by suffixing a running number to <prefix>.

For example, ‘--section_name_prefix=sec’ option names the load image sections sec_1, sec_2, etc. This option is ignored if not generating TI COFF/ELF load image output. If the option is not specified, the default prefix "image" is used.

Load Image Section Characteristics

Load Image File Characteristics

Memory Width and ROM Width

The hex converter allows the user to specify a memory width and a ROM width. Please refer to the Assembly Language Tools User’s Guide (SPNU118D) for more details. A ROM width smaller than a memory width results in the hex converter splitting memory width bits from input into ROM width bits in multiple output files. The TI COFF/ELF object files contain raw data and there is no way to specify the size of each word. Hence, when generating TI load image object file, both the ROM width and memory are ignored. If the memory width or ROM width is specified, a warning will be issued informing the user that the values are being ignored.

Examples

This section contains three examples. The first example shows a simple use case where three executables are combined. The second example shows how the user can define memory ranges to control the output load image section formation. The third example shows building a boot loader with embedded boot image.

Example 1: A simple use case

Below, we show how three executables are combined using the default load section formation. The three executables in this example are an application (app.out), a boot loader (boot.out) and a configuration data out file (config.out). The contents of these executables are given below. Note that each executable contains contiguous set of initialized sections which form a single contiguous initialized area in load memory. For example, the app.out has three initialized sections, namely .text, .cinit and .const, and they are contiguous in memory from 0x20 through 0x4955.

> ofd470 app.out 
OBJECT FILE: app.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .bss 0x0005a000 0x0005a000 0x478 4 Y 4 .sysmem 0x00058000 0x00058000 0x2000 4 Y 5 .stack 0x00050000 0x00050000 0x8000 4 Y 6 .text 0x00000020 0x00000020 0x4700 4 Y 7 .cinit 0x00004720 0x00004720 0x134 4 Y 8 .const 0x00004854 0x00004854 0x101 4 Y ...
> ofd470 boot.out 
OBJECT FILE: boot.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .bss 0x00050500 0x00050500 0x256 4 Y 4 .sysmem 0x0005A000 0x0005A000 0x2000 4 Y 5 .stack 0x00060000 0x00060000 0x8000 4 Y 6 .text 0x00005000 0x00005000 0x954 4 Y 7 .cinit 0x00005954 0x00005954 0x48 4 Y 8 .const 0x0000599C 0x0000599C 0x80 4 Y ...
> ofd470 config.out 
OBJECT FILE: config.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .config 0x00007000 0x00007000 0x37a0 4 Y ...

The customers want to deliver the above executables for ROM masking and they want to deliver a single object file to make sure the components don’t interfere.

> hex470 app.out boot.out config.out --section_name_prefix="data" --load_image -o ROM_simple.obj
> ofd470 ROM_simple.obj 
OBJECT FILE: ROM_simple.obj ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 1 data_1 0x00000020 0x00000020 0x4938 4 Y 2 data_2 0x00005000 0x00005000 0x0a1c 4 Y 3 data_3 0x00007000 0x00007000 0x37a0 4 Y ...

Example 2: User control of load image section formation

Again, let us consider three executables, namely an application (app.out), a boot loader (boot.out) and configuration data (config.out). The contents of these executables are shown below. Note that the initialized sections in apps.out are not contiguous. But the user wants to get a single load image data section for each input executable. To accomplish this the user defines three memory ranges, one for each input execuable.

> ofd470 app.out 
OBJECT FILE: app.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .bss 0x0005a000 0x0005a000 0x478 4 Y 4 .sysmem 0x00058000 0x00058000 0x2000 4 Y 5 .stack 0x00050000 0x00050000 0x8000 4 Y 6 .text 0x00000020 0x00000020 0x4700 4 Y 7 .cinit 0x00004800 0x00004800 0x134 4 Y 8 .const 0x00004934 0x00004934 0x100 4 Y ...
> ofd470 boot.out 
OBJECT FILE: boot.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .bss 0x00050500 0x00050500 0x256 4 Y 4 .sysmem 0x0005A000 0x0005A000 0x2000 4 Y 5 .stack 0x00060000 0x00060000 0x8000 4 Y 6 .text 0x00005000 0x00005000 0x954 4 Y 7 .cinit 0x00005954 0x00005954 0x48 4 Y 8 .const 0x0000599C 0x0000599C 0x80 4 Y ...
> ofd470 config.out 
OBJECT FILE: config.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .config 0x00007000 0x00007000 0x37a0 4 Y ...

Given the above executables,

> cat rom.cmd 
app.out /* Apps input file */ boot.out /* Boot loader input file */ config.out /* Config input file */
--load_image /* TI COFF load image output format */ –o ROM.obj /* combined load image object */
ROMS { apps: origin=0x00000020 len=0x4FE0 bootloader: origin=0x00005000 len=0x1000 config: origin=0x00007000 len=0x4000 fill=0xABCD }
> hex470 rom.cmd
> ofd470 ROM.obj 
OBJECT FILE: ROM.obj ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 1 apps 0x00000020 0x00000020 0x4FE0 4 Y 2 bootloader 0x00005000 0x00005000 0x1000 4 Y 3 config 0x00007000 0x00007000 0x4000 4 Y ...

Example 3: Build boot loader with embedded boot image

This example shows how the user can build a boot loader with embedded boot image as a single executable. The executable app.out is converted into a load image and included in a subsequent link step to produce a single executable containing the boot loader and the application boot image. Note that the initialized sections in the executable app.out are contiguous.

> ofd470 app.out 
OBJECT FILE: app.out ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 3 .bss 0x0005a000 0x0005a000 0x478 4 Y 4 .sysmem 0x00058000 0x00058000 0x2000 4 Y 5 .stack 0x00050000 0x00050000 0x8000 4 Y 6 .text 0x00000020 0x00000020 0x4700 4 Y 7 .cinit 0x00004720 0x00004720 0x134 4 Y 8 .const 0x00004854 0x00004854 0x101 4 Y ...

Step 1:
Create the boot image of the application.

> hex470 app.out --section_name_prefix=”app_image” –-load_image -o app_image.obj
> ofd470 app_image.obj 
OBJECT FILE: app_image.obj ... Section Information id name load addr run addr size align alloc -- ---- --------- -------- ---- ----- ----- 1 app_image_1 0x00000020 0x00000020 0x4938 4 Y ...

Step 2:
Include the object app_image.obj in the boot loader link step. Note that the load image section app_image_1 can be loaded at any address but should be copied to the run address 0x00000020 before executing it.

> cat lnk.cmd 
-c /* LINK USING C CONVENTIONS */ --stack_size 0x8000 /* SOFTWARE STACK SIZE */ -heap 0x2000 /* HEAP AREA SIZE */
/* SPECIFY THE SYSTEM MEMORY MAP */ MEMORY { APP_MEM  : org = 0x00000020 len = 0x000040E0 /* APP RUN MEMORY (RAM) */ P_MEM  : org = 0x00005000 len = 0x00040000 /* PROGRAM MEMORY (ROM) */ D_MEM  : org = 0x00045000 len = 0x00050000 /* DATA MEMORY (RAM) */ }
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */
SECTIONS { .intvecs : {} > 0x0 /* INTERRUPT VECTORS */ .bss  : {} > D_MEM /* GLOBAL & STATIC VARS */ .sysmem  : {} > D_MEM /* DYNAMIC MEMORY ALLOCATION AREA */ .stack  : {} > D_MEM /* SOFTWARE SYSTEM STACK */
.text  : {} > P_MEM /* CODE */ .cinit  : {} > P_MEM /* INITIALIZATION TABLES */ .const  : {} > P_MEM /* CONSTANT DATA */ .pinit  : {} > P_MEM /* C++ CONSTRUCTOR TABLES */ .xref  : > P_MEM
.app_image: {*(app_image*)} > LOAD=P_MEM, RUN=APP_MEM, LOAD_START(_app_load_start), RUN_START(_app_run_start), SIZE(_app_size) }
>lnk470 boot_*.obj app_image.obj lnk.cmd –o boot.out

The output file boot.out contains the boot loader and the application boot image. The boot loader uses the symbols _app_load_start, _app_run_start and _app_size to copy the boot image from load address to run address.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox