Compatibility between DSP/BIOS versions and Code Generation Tools
From Texas Instruments Embedded Processors Wiki
Translate this page to
DSP/BIOS version 5.33 or greater has been modified to be compatible with the latest Code Generation Tools, this includes:
- Any version of 5.0.x and 5.1.x for the C2000 Code Generation Tools
- Any version of 4.1.x and 4.2.x for the C5500 Code Generation Tools
- Any version of 6.0.x and 6.1.x for the C6000 Code Generation Tools
- Version 6.1.x will issue a linker warning regarding the use of trampolines for certain DSP/BIOS calls (only affects C62x, C67x, C672x). This is a known issue and will be addressed in future DSP/BIOS releases. This does not affect functionality.
DSP/BIOS 5.33 can be obtained from the Update Advisor DSP/BIOS Product Releases page:
https://www-a.ti.com/downloads/sds_support/targetcontent/bios/index.html
Previous versions of DSP/BIOS (5.30, 5.31, 5.32) are only compatible with:
- Version 5.0.x or earlier for the C2000 Code Generation Tools
- Version 4.1.x or earlier for the C5500 Code Generation Tools
- Any version of 6.0.x and 6.1.x for the C6000 Code Generation Tools
- Any version of 4.1.x and 4.2.x for the C5400 Code Generation Tools (Note: Last version of DSP/BIOS supported for C5400 devices is v5.31.09).
Comments
Comments on Compatibility between DSP/BIOS versions and Code Generation Tools
TommyG said ...
Arnier said ...
No known constraints on C5400 CGTools with DSP/BIOS v5.31 or earlier. NOTE: C54x DSP/BIOS is not supported beyond v5.31. Topic updated!
--Arnier 11:36, 14 September 2009 (CDT)

Are there constraints for C5400 family?
--TommyG 08:49, 7 August 2009 (CDT)