<Linking> warning #10202-D: no suitable entry-point found; setting to 0
The linker has not found any entry points.
This would not be an issue with most C projects, as there is an entry point (defined by the C runtime library) which in turn calls main, and so sections will be pulled into the link. In the case of a single assembly source file, this is not the case.
Some background info on this is available here: https://processors.wiki.ti.com/index.php/C6000_EABI_Migration#Conditional_Linking_Feature This page was written for the C6000 tools but how the ELF/EABI feature works is the same for other devices as well.
How to set the entry point (example for assembly only project):
.cdecls C,LIST, "msp430x20x2.h"
;------------------------------------------------------------------------------
.text ; Program Start
.global RESET ; Define entry point
;------------------------------------------------------------------------------
RESET mov.w #0280h,SP ; Initialize stackpointer
StopWDT mov.w #WDTPW+WDTHOLD,&WDTCTL ; Stop WDT
SetupP1 bis.b #001h,&P1DIR ; P1.0 output
;
Mainloop bit.b #010h,&P1IN ;
; skipped lines of code
;------------------------------------------------------------------------------
; Interrupt Vectors
;------------------------------------------------------------------------------
.sect ".reset" ; MSP430 RESET Vector
.short RESET
NOTE: After doing above, if your application fails to load and debug then you may be experiencing bug SDSCM00043978. Setting the entry point should retain both .text and .reset sections, however for this bug, the .reset section is not being retained.
To work around this bug, see the remedy here.
An executable will not be created until this error is resolved.
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Compiler/diagnostic messages/10202 here. |