ControlSUITE Linux Installation

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Introduction

controlSUITE is not yet supported under Linux operating systems. We are planning on supporting it in the future.

Following are instructions for installing controlSUITE under Linux (with limited support) using Wine. These instructions have only been tested with the 32-bit version of Ubuntu Linux 10.04.

Setup

Install Wine

Before controlSUITE can be installed, Wine must be present in the system.

In Ubuntu, go to Applications->Ubuntu Software Center.


1.png

Use the search feature to find the Wine application, which might be labeled as "Wine Microsoft Windows Compatibility Layer". Click install.


2.png

Download controlSUITE

Download the Alternative .zip download (sprca85.zip) of controlSUITE.


3.png

Once the zip file has been downloaded, extract the files.

  • NOTE: Before running the Setup.exe, you might have to allow execution of the file.
    To do this, right click on the .exe file and select properties. Click on the "Permissions" tab and check the "Allow executing file as program" checkbox.


4.png

Install controlSUITE

After changing the file permissions, run the installer by clicking on the .exe file.


5.png

After the license agreement step, the installer will ask where controlSUITE should be installed. Click on Browse to select a different installation location.

Select the path "/home/<username>/" in the "Browse For Folder" window. Where <username> is the currently logged on username.


6.5.png


5.5.png

Click next and complete installing the application.

Import controlSUITE Projects into CCSv5

Once controlSUITE is installed, projects can be imported into CCSv5.


8.png

Once CCSv5 has been launched, go to Project->Import Existing CCS/CCE Eclipse Project.


9.png

Click on Browse and find your home directory, then browse into the controlSUITE directory.

Device example projects can be found under the controlSUITE/device_support/<device_name>/<version> directory.


10.png

Click Finish and the controlSUITE project should be in your CCSv5 workspace.

Final Note

The controlSUITE.exe application that is installed will not work under Wine. All of the files will have to be manually imported into controlSUITE.

E2e.jpg For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article ControlSUITE Linux Installation here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox