Cortex-R4 CPU Functional Simulator
From Texas Instruments Embedded Processors Wiki
Translate this page to
Cortex-R4 CPU Functional Simulator
This simulator is a Cortex-R4 CPU only simulator and it's a functional simulator. This is simulator comes with a flat memory attached to the external bus; Mainly used in algorithm development where the development is CPU centric.
Features
- Integrated with Code Composer Studio with unified loader support for both Microsoft Windows and Linux platforms
- Pin connect for injecting interrupts to peripherals
- Advanced profiling
- Ease of configuring the simulator through enhanced Code Composer Studio setup
- Endianness (Little, Big, BE-8: byte invariant; and BE-32: word invariant)
Limitations
- No cycle information
- Does not support Code Composer Studio advanced debug and analysis features.
- Java state is not supported.
The following components are not modelled
- MPU. No memory maps; entire memory is treated as a flat memory with 0 latency
- FPU
- Buses, Caches and buffers
- ARMv7R instructions for multi-core environment (event handling). They are treated as NOP’s
- Co-processor instructions for other than move instructions for CP15 registers. They are treated as NOP's
- Exclusive load/store instructions are treated as normal load/store instructions. Monitor is not modeled, hence instructions, other than load/store, using the monitors are treated as NOP’s.