Creating and Building codec combos in Windows
From Texas Instruments Embedded Processors Wiki
Contents |
Introduction
It is a common misconception that Codec Servers/Combos can only be created and built in Linux. In fairness it's easy to see how one arrives at such a conclusion since: -
- the majority of the collateral is focused on Linux
- the current codec combos in the DVSDK ship DVTB prebuilt Linux binaries (a bug has been filed to remove these)
This topic describes how to create and build codec combos in a Windows environment.
Audio / Video Use-case
Let's say we want to build a codec combo with MPEG4 decode and AAC HE decode. We obtained the following 2 packages: -
- omap3530_mpeg4dec_2_00_008_evaluation - MPEG4 decode v2.00.008 evaluation codec implementing IVIDDEC2, validated on OMAP3530 but works on any c64+ platform
- dm6446_aachedec_1_30_002_evaluation - AAC HE decode v1.30.002 evaluation codec implementing IAUDDEC1, validated on DM6446 but works on any c64+ platform
Both of these have already been wrapped with the Codec RTSC Package Wizard.
Using the GenServer combo wizard
We now want to create an Audio/Video codec combo.
To do this we leverage the Codec Engine GenServer Wizard. As per the FAQ this tool is available only in CE >= 2.22. As recommended we download the 'full' Codec Engine. This is extremely useful because it contains the right versions of all the sub-dependent components. It also makes setting the XDCPATH easier.
In this example, we downloaded CE 2.22. The CE release notes tell us that we also need >= DSP/BIOS 5.33.03 and >= XDCtools 3.10.03 - so we download these too.
We then set up our XDCPATH to contain: -
- the repository containing our MPEG4 and AAC HE decode codec packages
- codec_engine_2_22/packages
- codec_engine_2_22/cetools/packages
- bios_5_33_03/packages
On Windows this equates to: -
set XDCPATH=C:\win_codec_combos\dm6446_aachedec_1_30_002_evaluation\packages;C:\win_codec_combos\omap3530_mpeg4dec_2_00_008_evaluation\packages;C:\codec_engine_2_22\packages;C:\codec_engine_2_22\cetools\packages;C:\xdctools_3_10_03\packages;C:\bios_5_33_03\packages
Next we instantiate the Combo Wizard via: -
C:\xdctools_3_10_03\xs.exe ti.sdo.ce.wizards.genserver
We fill in the following fields in Step 1: -
The defaults in Step 2 are fine - this sets e.g. the priority of the audio and video algorithms. We leave these alone.
Upon completion the wizard tells us we need to fill in the memory assignments in server\av_combo\codec.cfg - this is because the wizard cant know which memory types you want to assign the config sections to.
Hence we edit codec.cfg as follows: -
AACHEDEC.alg.watermark = true; AACHEDEC.alg.codeSection = 'DDR2'; AACHEDEC.alg.udataSection = 'DDR2'; AACHEDEC.alg.dataSection = 'DDR2'; ... MPEG4DEC.alg.watermark = true; MPEG4DEC.alg.codeSection = 'DDR2'; MPEG4DEC.alg.udataSection = 'DDR2'; MPEG4DEC.alg.dataSection = 'DDR2';
Building the combo from the command line
First we create a simple config.bld to point to our Codegen Tools and Platform. We place it in the av_combo\packages directory since we already have that in our XDCPATH (1 less path to add)
/* * ======== config.bld ======== * User note: YOU MUST MODIFY THIS FILE TO SPECIFY THE COMPILER TOOL PATHS. * * Edit this file to specify compiler toolchain paths, and any custom * compiler/linker options. */ /* location of your C6000 codegen tools */ var C64P = xdc.useModule('ti.targets.C64P'); /* location of your CG tools */ var codegen = "" + java.lang.System.getenv("CODEGEN_INSTALL_DIR"); C64P.platform = "ti.platforms.evm3530"; /* Verify that CODEGEN_INSTALL_DIR was set as an environment variable */ if (codegen=="null" || codegen=="") { print("Warning: TI Code Generation Tools not found. Verify that " + "CODEGEN_INSTALL_DIR is set correctly in the Makefile."); } else if ( !java.io.File( codegen ).isDirectory() ) { print("Warning: CODEGEN_INSTALL_DIR is not set to a valid directory."); } C64P.rootDir = codegen; /* * ======== Build.targets ======== * list of targets (ISAs + compilers) to build for */ Build.targets = [ C64P, ];
We can then use the XDCPATH that we previously set at the command line and then invoke 'xdc' directly upon the generated server to build it.
set CODEGEN_INSTALL_DIR=c:\CCStudio_v3.3\C6000\cgtools c:\xdctools_3_10_03\xdc.exe -PR .
Building the combo via a Makefile
It gets tiring to keep setting a long XDCPATH. Hence you could create a simple Makefile. Here we pattern after the DVSDK style i.e. a simple Makefile that invokes 'xdc' and leverages a base Rules.make with all the tool settings.
Makefile: -
# # ======== Makefile ======== # This makefile is optional - you can use all of it or none of it. # Its purpose is to save time/typing when used from the context of the DVSDK. # All of the paths are preset in the $(DVSDK_INSTALL_DIR)/Rules.make. The wizards # (particularly the server wizard) requires many of these paths hence by setting # the XDCPATH here we save the user some typing and package-path setup. # Commands (make goals): - # - Start the codec packaging wizard # [>] make genpackage # - Start the server wizard # [>] make genserver # - Clean the codecs/server packages # [>] make clean # - Build the codecs/server packages # [>] make # - Release the codecs/server packages (generate tarballs) # [>] make release # Note : if your codec/server packages are in a different location outside # the DVSDK simply override the CODEC_INSTALL_DIR on the cmd line via e.g. # [>] make CODEC_INSTALL_DIR="/home/user/mycodecs" # Note : if your codecs come from different vendors you can do: - # [>] make CODEC_INSTALL_DIR="/home/user/ven1/codecs/packages;/home/user/ven2/codecs" # Note : if using the wizard standalone outside of the DVSDK you can still # leverage this makefile by modifying the include Import Tools Path below # to point to your DVSDK Rules.make # # Import Tools Path from Rules.make -include ../Rules.make # Set location of xdc executable XDC = $(XDC_INSTALL_DIR)/xdc # Set XDCPATH to contain necessary repositories. # Note that we put specify both CODEC_INSTALL_DIR and CODEC_INSTALL_DIR/packages # since our config.bld is typically in CODEC_INSTALL_DIR. # If instead you're running XDCPATH = ^;$(CURDIR);$(CODEC_INSTALL_DIR)/packages;$(BIOS_INSTALL_DIR)/packages;$(CE_INSTALL_DIR)/packages; # Conditionally, you can create verbose build output XDCOPTIONS=v # Select the combo build type , either eval(evaluation) or prod( Production) XDCARGS="eval" export XDCOPTIONS export XDCPATH export XDCARGS ######################################################## ## Shouldn't have to modify anything be low this line ## ######################################################## SERVERNAME = "" all: .all-packages # This recursively locates all packages in the specified directory, builds # and releases them .all-packages: .check-BIOS $(XDC) -PR . # This recursively cleans all packages in the specified directory clean: clean-packages clean-packages: $(XDC) clean -PR . # This recursively cleans all packages that were delivered via an 'xdc release' relclean: relclean-packages relclean-packages: $(XDC) .make -PR . $(XDC) clean -PR . # This recursively releases all packages in the specified directory release: release-packages release-packages: $(XDC) release -PD . # Just a shortcut to launch the RTSC Package wizard genpackage: $(XDC_INSTALL_DIR)/xs ti.sdo.codecutils.genpackage # Just a shortcut to launch the CE RTSC Combo wizard genserver: $(XDC_INSTALL_DIR)/xs ti.sdo.ce.wizards.genserver # This ensures that the BIOS you're using has been patched for SDSCM00004525. # Specifically, the fix is to rename # $(BIOS_INSTALL_DIR)/packages/ti/rtdx/package_export.xdc to package.xdc .check-BIOS : $(BIOS_INSTALL_DIR)/packages/ti/rtdx/package.xdc $(BIOS_INSTALL_DIR)/packages/ti/rtdx/package.xdc : $(warning Your BIOS needs to be patched for SDSCM00004525!) $(error Please copy $(BIOS_INSTALL_DIR)/packages/ti/rtdx/package_export.xdc to $@)
And the corresponding Rules.make: -
# # ======== Rules.make ======== # This file specified defines used by the top-level makefile. # Define target platform. PLATFORM=omap3530 # Where the Codec Engine package is installed. CE_INSTALL_DIR=C:\codec_engine_2_22\packages;C:\codec_engine_2_22\cetools # Where the codec servers are installed. CODEC_INSTALL_DIR=C:\win_codec_combos\dm6446_aachedec_1_30_002_evaluation\packages;C:\win_codec_combos\omap3530_mpeg4dec_2_00_008_evaluation # Where the RTSC tools package is installed. XDC_INSTALL_DIR=C:\xdctools_3_10_03 # Where DSP/BIOS is installed. BIOS_INSTALL_DIR=C:\bios_5_33_03
We then simply run: -
gmake clean gmake CODEGEN_INSTALL_DIR=c:\CCStudio_v3.3\C6000\cgtools
Known Issues
See Codec_Engine_Known_Issues - in particular note the issues highlighted on the genserver wizard.