Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Cryptography Users Guide

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:


NOTE: This page is isolated, it was for AMASK6.0 or older. Please refer to Linux_Core_Crypto_User_Guide for Cryptography support in Processor Linux SDK.

Return to the Sitara Linux Software Developer's Guide

TIBanner.png

Overview

This article provides a description of the example applications under the cryptography page of the Matrix application that comes with the Sitara SDK.  This page is labled "Cryptos" in the top-level Matrix GUI.



MatrixMain.PNG



Devices Supported

All Sitara SDK's provide cryptography through OpenSSL, but the following devices have cryptographic hardware accelerators and drivers:

  • AM3517 - AES, DES, 3DES, SHA, MD5
  • AM37x - AES, DES, 3DES, SHA, MD5
  • AM335x - AES, SHA, MD5, RNG



The example applications have been designed to use hardware accelerators when they are available and fall back to a pure software implementation when hardware accelerators are not available.


 

Cryptography Examples

All of the examples under the Cryptos page use the OpenSSL command line application to perform cryptographic functions.  A comprehensive list of cryptographic functionality using OpenSSL is beyond the scope of the out-of-box experience intended with the Matrix GUI.  However, the examples present a nice variety of cryptographic functions that are available with OpenSSL on the Sitara platform.

MatrixCryptos.PNG


OpenSSL Performance

This example executes the OpenSSL built-in speed test for a variety of cryptographic algorithms.  The results of the test are displayed on the screen and also written to the file OpenSSLspeedResults.txt in the top level directory of the target filesystem.


Certificate Generation

This example generates a web page certificate for use with a secure web server.  The certificate is held in the file matrixcert.pem.  This file will appear in the top level directory of the target file system.  If the certificate already exists, then the example will fail and prompt the user to delete the existing certificate (matrixcert.pem) before generating a new one.


Public Key Generation

This example generates a public key based on the certificate (matrixcert.pem) generated in the previous example.  If the certificate does not exist the example will fail and pronpt the user to first generate the certificate before trying to generate the public key.  The public key will be saved to a file pubkey.pem in the top level directory of the target file system.


Secure Server

Once the web certificate (matrixcert.pem) has been generated, the secure web server can be started on the target board.  Pointing a modern web browser at the target should generate a warning that the certificate is self-signed.  This means that the certificate has not been verified by a trusted third party such as Verisign.  Depending on the browser, you can view details of the certificate.  In the example below the target board has an IP address of 128.247.106.217.  When Internet Explorer is pointed to the URL https://128.247.106.247:4433 , it first warns the user that there is a problem with the website's security certificate.  Make sure that you use https:// and the port number :4433 with the IP address in the URL of the browser.  Clicking the link to continue anyway provides the page below.  And clicking the "Certificate Error" button at the top of the page will provide details of the certificate.


SecureServer.PNG

NOTE

OpenSSL 1.0.0j contains a bug in the secure client code that will crash the secure server. AMSDK 6.0 is affected by this bug. That patch and build instructions are [[1]].


Certificate Info

This example simply prints out details of the generated certificate (matrixcert.pem).

AES 256

This example will perform an encrypt/decrypt cycle on a 10M file of random data with the AES 256 algorithm.  The 10M file called rnddata will be generated if it doesn't already exist.  The result of the decryption is compared to the original file and the results are displayed to the screen.

SHA Hash

This example will perform a SHA1 hash function on the 10M file of random data (rnddata).  If the file doesn't exist, it is generated.  The result of the hash is displayed to the screen.


 

Building the Driver

For devices with available cryptographic hardware accelerators, a Linux driver and additionally an OCF kernel module (for OpenSSL) is needed to access them.  Other devices use the pure software implementation of OpenSSL for the crypto demos.

NOTE

{{{1}}}

AM35x/37x, AM335x - AES, SHA/MD5 Drivers

Starting with SDK 5.05.00.00, the driver for AM335x is completely integrated into the kernel source.  The pre-built kernel that comes with the SDK already has the AES and SHA/MD5 drivers built-in to the kernel.  The kernel configuration has already been set up in the SDK and no further configuration is needed for the drivers to be built-in to the kernel.  The configuration of the random number generator does require an extra step and this is detailedd in the next section.

For reference, the configuration details are shown below.  The configuration of the AES and SHA/MD5 driver is done under the Hardware crypto devices sub-menu of the Cryptographic API menu in the kernel configuration. 

--- Cryptographic API
    [*] Hardware crypto devices --->
        --- Hardware crypto devices
            <*> Support for OMAP4 AES hw engine
            <*> Support for OMAP4 SHA/MD5 hw engine

Messages printed during bootup will indicate that initialization of the crypto modules has taken place.

[ 1.695495] omap4_aes_mod_init: loading AM33X AES driver
[ 1.701202] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.707733] omap4_aes_probe: probe() done
[ 1.712402] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.718536] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.733276] omap4_sham_probe: probe() done

Build the OCF kernel module using SDK

For using OpenSSL to access the Crypto Hardware Accelerator Drivers above, the Open Cryptographic Framework (OCF) is required (can be built as module). The framework is not officially in the kernel and was ported to Linux under the name "ocf-linux".  As long as the OCF pieces are enabled in menuconfig whenever the kernel is built the OCF components are built during that process.


Using Cryptographic Hardware Accelerators

Using the TRNG Hardware Accelerator

For the True Random Number Generator (TRNG) in the AM335x there is an extra step needed in the Linux kernel configuration that needs to be performed to get the driver included in the kernel.

Use the menuconfig command accroding to the "Customizing the Configuration" section to get into the configuration menu for the kernel.

processors.wiki.ti.com/index.php/AMSDK_Linux_User%27s_Guide#Customizing_the_Configuration

In the configuration menu, scroll down to Device Drivers and hit enter.  Now scroll to Character devices and hit enter.  

 Device Drivers --->
    Character devices --->
        < > Hardware Random Number Generator Core support

Use the spacebar to select the Hardware Random Number Generator support and also select OMAP4 Random Number Generator support.  The screen should look like below.

        <*> Hardware Random Number Generator Core support
           < > Timer IOMEM HW Random Number Generator support (NEW) 
           <*> OMAP4 Random Number Generator support (NEW) 

Now rebuild the kernel accoring to the User's Guide and boot up the board with the resulting kernel.  The following message should be part of the boot-up messages.

[ 0.944152] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00


Once the system is booted up, the hwrng device should now show up in the filesystem.

root@am335x-evm:~# ls -l /dev/hwrng
crw------- 1 root root 10, 183 Jan 1 2000 /dev/hwrng
root@am335x-evm:~#


Use cat on this device to generate random numbers.

root@am335x-evm:~# cat /dev/hwrng | od -x
0000000 b2bd ae08 4477 be48 4836 bf64 5d92 01c9
0000020 0cb6 7ac5 16f9 8616 a483 7dfd 6bf4 3aa5
0000040 d693 db24 d917 5ee7 feb7 34c3 34e9 e7a5
0000060 36b7 ea85 fc17 0e66 555c 0934 7a0c 4c69
0000100 523b 9f21 1546 fddb d58b e5ed 142a 6712
0000120 8d76 8f80 a6d2 30d8 d107 32bc 7f45 f997
0000140 9d5d 0d0c f1f0 64f9 a77f 408f b0c1 f5a0
0000160 39c6 f0ae 4b59 1a76 84a7 a364 8964 f557
root@am335x-evm:~#

AES, SHA, TRNG Hardware Accelerators using OpenSSL (requires OCF-linux kernel support)

The device drivers for AES and SHA/MD5 hardware acceleration is configured and built into the kernel by default in SDK 5.05.00.00. No other special setup is needed for OpenSSL to access the crypto modules.

First, the kernel from the SDK must be configured and built according to the SDK User's Guide.

processors.wiki.ti.com/index.php/AMSDK_Linux_User%27s_Guide

The General Purpose (GP) EVMs on TI SoCs allows access to built in cryptographic accelerators. Inorder to use these drivers from OpenSSL, the drivers on their own have no contact with userspace. For this, a special driver is available which abstracts the access to these accelerators through the Open Cryptographic Framework for Linux (OCF-Linux).

The demo application under the crypto menu of Matrix will load and use the OCF driver kernel modules automatically to perform hardware accelerated crypto functions. The process of manually loading the kernel modules and using the driver is explained below.

OCF-Linux is itself a special device driver which provides a general interface for higher level applications such as OpenSSL to access hardware accelerators.

Kernel modules are required for OCF-linux, OCF cryptosoft and OCF cryptodev. All these 3 modules are a part of the OCF-linux package.

The filesystem which comes with the SDK comes built with the OCF-Linux kernel modules and the TI driver which directly accesses the hardware accelerators is built into the kernel.

From the target boards perspective the drivers are located in the following directories:

/lib/modules/3.8.4-01427-g1eb3bbb-dirty/kernel/crypto/ocf/cryptosoft.ko
/lib/modules/3.8.4-01427-g1eb3bbb-dirty/kernel/crypto/ocf/cryptodev.ko
/lib/modules/3.8.4-01427-g1eb3bbb-dirty/kernel/crypto/ocf/ocf.ko

To use the drivers they must first be installed. Use the insmod command to install the drivers.  The TI crypto driver allows a parameter to be passed in to indicate if DMA should be used.  The following log shows the commands used to install the modules and query the system for the state of all system modules.

root@am37x-evm:~# lsmod
Module                  Size  Used by
cryptosoft             14350  0 
cryptodev              11962  0 
ocf                    25277  2 cryptosoft,cryptodev
root@am37x-evm:~#

After the modules are installed, OpenSSL commands may be executed which take advantage of the hardware accelerators through the OCF-Linux driver.  The following example demonstrates the OpenSSL built-in speed test to demonstrate performance.  The addition of the parameter -engine cryptodev tells OpenSSL to use the OCF-Linux driver if it exists.

root@am37x-evm:~# openssl speed -evp aes-128-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-128-cbc for 3s on 16 size blocks: 108107 aes-128-cbc's in 0.16s
Doing aes-128-cbc for 3s on 64 size blocks: 103730 aes-128-cbc's in 0.20s
Doing aes-128-cbc for 3s on 256 size blocks: 15181 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 1024 size blocks: 15879 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 8192 size blocks: 4879 aes-128-cbc's in 0.02s
OpenSSL 1.0.0b 16 Nov 2010
built on: Thu Jan 20 10:23:44 CST 2011
options:bn(64,32) rc4(ptr,int) des(idx,risc1,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp -mthumb-interwork -mno-thumb -fPS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 10810.70k 33193.60k 129544.53k 542003.20k 1998438.40k
root@am37x-evm:~#
root@am37x-evm:~#
root@am37x-evm:~#

Using the Linux time -v function gives more information about CPU usage during the test.

root@am37x-evm:~# time -v openssl speed -evp aes-128-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-128-cbc for 3s on 16 size blocks: 108799 aes-128-cbc's in 0.17s
Doing aes-128-cbc for 3s on 64 size blocks: 102699 aes-128-cbc's in 0.18s
Doing aes-128-cbc for 3s on 256 size blocks: 16166 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 1024 size blocks: 15080 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 8192 size blocks: 4838 aes-128-cbc's in 0.03s
OpenSSL 1.0.0b 16 Nov 2010
built on: Thu Jan 20 10:23:44 CST 2011
options:bn(64,32) rc4(ptr,int) des(idx,risc1,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp -mthumb-interwork -mno-thumb -fPS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 10239.91k 36515.20k 137949.87k 514730.67k 1321096.53k
Command being timed: "openssl speed -evp aes-128-cbc -engine cryptodev"
User time (seconds): 0.46
System time (seconds): 5.89
Percent of CPU this job got: 42%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.06s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 7104
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 479
Voluntary context switches: 36143
Involuntary context switches: 211570
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0

When the cryptodev driver is removed, OpenSSL reverts to the software implementation of the crypto algorithm.  The performance using the software only implementation can be compared to the previous test.

root@am37x-evm:~# rmmod cryptodev
root@am37x-evm:~# time -v openssl speed -evp aes-128-cbc
Doing aes-128-cbc for 3s on 16 size blocks: 697674 aes-128-cbc's in 2.99s
Doing aes-128-cbc for 3s on 64 size blocks: 187556 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 256 size blocks: 47922 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 1024 size blocks: 12049 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 8192 size blocks: 1509 aes-128-cbc's in 3.00s
OpenSSL 1.0.0b 16 Nov 2010
built on: Thu Jan 20 10:23:44 CST 2011
options:bn(64,32) rc4(ptr,int) des(idx,risc1,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp -mthumb-interwork -mno-thumb -fPS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 3733.37k 4001.19k 4089.34k 4112.73k 4120.58k
Command being timed: "openssl speed -evp aes-128-cbc"
User time (seconds): 15.03
System time (seconds): 0.00
Percent of CPU this job got: 99%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.07s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 7216
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 1
Minor (reclaiming a frame) page faults: 484
Voluntary context switches: 13
Involuntary context switches: 35
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0

Crypto Performance

Read AM3517 performance tests using cryptotest

Archived Versions