DIO Library

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

DIO Library ( DIOlib )


Purpose and Scope

This DIO library aims at providing a CSL-like Serial RapidIO "functional layer" for the directIO mode of Texas Instruments' TMS320C645x/7x DSP platform. The I/O operations supported by this library are defined in RapidIO Interconnect Specification rev1.2 - Chapter 2. The DIO library is built on top of TMS320C645x/7x Chip Support Library.

Note: DIO Library is available for download at TI's Gforge: https://gforge.ti.com/gf/project/sriodirectiolib/
[At the gforge site, click on the top or most recent Activity Type, then on the zip filename, then on the (download) link for the HEAD entry.]

DIO library modules

This DIO library contains 5 different modules:

RIO module : The RIO module is dedicated to the definition of generic elements for the TMS320C645x/7x SRIO module (independent to the directIO or message passing protocols) and dedicated to the H/W initialization of the SRIO module.

DIO module : This DIO module is dedicated to the handling of Serial RapidIO directIO operations supported by the TMS320C645x/7x SRIO module. DIO differentiates three types of operations: data request packets (nread, nwrite, nwrite_r, swrite and atomic), maintenance request packets, and doorbell signals. The DIO module also supports one-shot long (>4KBytes) read and write I/O operations with EDMA-initiated "streaming" requests. Finally, the DIO module offers "raw" IDMA or EDMA directIO fast request. It assumes the application has pre-configured directIO operations at initialization time. This functionality gives the application a way to bypass the configuration calls of higher level DIO lib APIs, by re-using pre-set LSU command sets.

COM module : This COM module contains benchmarking APIs, the library error handler and callback set, and a random bit generator. Please note that the COM module is not documented.

BRU module : The BRU module is dedicated to the support of system bring up. Initial scope is to enable static system configuration, where one end point has knowledge about the topology of the system.

TST module : "$(DirectIODir)/test" contains all tests used to validate the library.

Leave a Comment

Comments

Comments on DIO Library


Ringel said ...

Hi,

What SW should I install (under win - xp/vista) for checkout?

Many Thanks, Haim

--Ringel 14:26, 19 October 2009 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox