Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

DM355 Getting Started Guide

From Texas Instruments Wiki
Jump to: navigation, search

Purpose

The purpose of this Getting Started Guide (GSG) is to walk you through setting up a development system for the DM355. You should proceed through this guide in the order given for best results. By the end of this Getting Started Guide you will have the DM355 DVEVM hardware setup, a Linux host development environment configured, and a Linux target booting to run some provided demonstration software. You should also bookmark the DM355 category since new articles will continue to appear here.

DVEVM Overview

For an overview of the DVEVM please see the GSG: DVEVM Overview page.

Hardware Setup

For information on setting up the DM355 DVEVM hardware please see the GSG: DM355 DVEVM Hardware Setup page.

Software Setup

The Software Setup page covers how to install the Linux tools, (DV)SDK software, and Linux Product Support Package for the DM355 DVEVM.

For Community Linux based DVSDKs (i.e. DVSDK 3.10) see GSG: DM3XX DVEVM Software Setup.

The latest DVSDK release can be downloaded from here.

Note: For Monta Vista Linux 5 based DVSDKs (i.e. DVSDK 2.00) see the Getting Started Guide included in the software package for a Red Hat Enterprise v4 based install, or for an alternative set of installation steps for a Ubuntu 9.04 (or similar) distribution please see GSG: DVSDK 2.0 Software Setup in Ubuntu.

Running Demos

The GSG: DM355 DVEVM Running the Demos page describes how to set up, execute, and shut down the demos.

Additional Procedures

This section covers additional useful procedures that are not necessarily part of the getting started process.

Creating JFFS2 DVSDK 3.10 demo filesystem

For information on creating JFFS2 demo filesystem from DVSDK release please see DM3xx filesystem restore procedure in DVSDK 3.10 page.

Setting Up a TFTP Server

For information on setting up a TFTP server please see the Setting up a TFTP Server page.

Example TeraTerm Scripts

For example TeraTerm scripts that can be used with the platform board please see the TeraTerm Scripts page.

Digital Video Test Bench

For more information on the Digital Video Test Bench (DVTB) and how to install it, see the Digital Video Test Bench page.

Linux Performance Test Bench

For more information on the Linux Performance Test Bench (LPTB) and how to install it, see the Linux Performance Test Bench page.

DVSDK Makefile Usage

For more information on the main DVSDK Makefile usage, see the DVSDK Makefile Usage page.

Integrate New Codec

For more information on how to add a new codec, see the Integrate a New Codec for DM3xx page.

Additional Information