Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

GStreamer

From Texas Instruments Wiki
(Redirected from DM3xx Gstreamer Solution)
Jump to: navigation, search

Abstract

GStreamer is a pipeline-based multimedia framework that allows you to create a variety of media-handling software components, including simple audio playback, audio and video playback, recording, streaming, and editing. The pipeline design allows you to easily write any type of streaming multimedia application. GStreamer also provides existing libraries and plugins for features such as A/V synchronization, muxing/demuxing, etc. Using GStreamer allows you to leverage all of this existing code in your product.

However, existing open source plugins do not leverage the DSP and accelerator modules on TI hardware. Leveraging these resources allows the system to perform labor-intensive operations while consuming fewer ARM cycles. This leaves the ARM processor free to perform other tasks in parallel. In order to enable full use of the hardware we do not need to significantly modify GStreamer to support TI platforms, we just need to write a plugin.

By providing a plugin that provides access to the hardware we are enabling the user to:

  1. Focus development efforts on "WOW" features of an application rather than spending time on base functionality.
  2. Enable DaVinci and OMAP devices to use existing applications built on top of GStreamer.
  3. Leverage the modular design to decrease the time required to develop new applications and enable more re-use of existing code.

GStreamer Plug-ins for TI hardware

There are several approaches that have been used to develop GStreamer plug-ins that utilize the DSP and accelerator modules in TI hardware.