DSPLink Overview

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

What is DSP/BIOSTM Link?

DSP/BIOS™ LINK is foundation software for the inter-processor communication across the GPP-DSP boundary. It provides a generic API that abstracts the characteristics of the physical link connecting GPP and DSP from the applications. It eliminates the need for customers to develop such link from scratch and allows them to focus more on application development.
This software can be used across platforms:

As the name suggests, DSP/BIOS™ is expected to be running on the DSP. No specific operating system is mandated to be running on the GPP. It is released on a reference platform for a set of reference operating systems. The release package contains full source code to enable the customers to port it to their specific platforms and/ or operating systems.
Depending on the supported platform, OS and DSPLink version, DSP/BIOS™ LINK provides a subset of the following services to its clients:

Why use DSP/BIOSTM Link?

DSPLink provides several features and capabilities that make it easier and more convenient for developers using a multi-core system:

Trainings

DSPLink overview streaming webex training is available at this page.

Other information

DSPLink is also available as part of the Codec Engine product available from TI.
DSPLink FAQs are available here.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox