Java Scripting with DSS
From Texas Instruments Embedded Processors Wiki
Contents |
Overview
JavaScript is the default scripting language supported by DSS. But because DSS is implemented as a set of Java APIs, it works quite nicely out of the box with Java. While the provided DSS examples are mostly for JavaScript, the DSS Java API documentation shows examples of API calls with Java code.
Prerequisites
At minimum, a Java compiler (javac) and a Java Runtime Environment (JRE) are needed to build and run the DSS Java application. While CCSv4 comes with a JRE, it does not come with a JDK (which provides a Java compiler). The JDK can be downloaded from the Sun Java SE download site. If a Java IDE (such as Eclipse) will be used to develop the DSS Java application, then a java compiler will already be available.
Creating DSS Java Source
To create a new DSS Java source file, simply create a new Java source file in an editor. If a Java IDE is being used, create a new Java project and add your new Java source file to the project. Refer to the documentation for the available APIs.
Example
Let's take a look at some example code snippets. They are from a straight Java port of the 'Breakpoints.js' JavaScript example that ships with DSS.
First thing that is needed is to import all the necessary DSS packages. the 'Breakpoints' example uses APIs for the Debug Server and the below will import all the necessary packages:
// Import all DSS packages for the Debug Server import com.ti.ccstudio.scripting.environment.*; import com.ti.debug.engine.scripting.*;
The first action done my the main() method is to create a scripting instance:
... public class DssBreakpointsExample { public static void main(String[] args) { // Create our scripting environment object - which is the main entry point into any script and // the factory for creating other Scriptable ervers and Sessions ScriptingEnvironment env = ScriptingEnvironment.instance(); ...
Let's look at how the a debug server instance is created and a debug session is started. Since most DSS APIs can throw exceptions, note how the calls are in a 'try-catch' block;
...
DebugServer debugServer = null;
DebugSession debugSession = null;
try
{
// Get the Debug Server and start a Debug Session
debugServer = (DebugServer) env.getServer("DebugServer.1");
debugServer.setConfig("C:/Program Files/Texas Instruments/ccsv4/scripting/examples/C64/tisim_c64xple.ccxml");
debugSession = debugServer.openSession(".*");
// Load a program
debugSession.memory.loadProgram("C:/Program Files/Texas Instruments/ccsv4/scripting/examples/C64/modem/Debug/modem.out");
}
catch (Exception e)
{
...Let's look at one more snippet, somewhere in the middle, of breakpoints being set:
... try { // Set a breakpoint at "main" main = debugSession.symbol.getAddress("main"); bp1 = debugSession.breakpoint.add(main); // Set another breakpoint address = debugSession.symbol.getAddress("ReadNextData"); bp2 = debugSession.breakpoint.add(address); ...
And so forth. To see what the rest of the functionality of the example is, refer to the 'Breakpoints.js' JavaScript example that ships with DSS. As an exercise, try to do a complete port of it yourself! The file should be saved as 'DssBreakpointsExample.java'.
Compiling
Once all the code has been written, next is to build it. When calling the java compiler, the following JAR files must be passed in with the '-classpath' (or '-cp') option:
- com.ti.ccstudio.scripting.environment_3.1.0.jar
- com.ti.debug.engine_1.0.0.jar
- dss.jar
The JAR files can be found in '<INSTALL DIR>\ccsv4\DebugServer\packages\ti\dss\java'. If building from a JAVA IDE, add the above JAR files to the list of external JAR in the project settings.
Below is an example of building the 'DssBreakpointsExample.java' file from the command line:
> javac -cp "C:\Program Files\Texas Instruments\ccsv4\DebugServer\packages\ti\dss\java\com.ti.ccstudio.scripting.environment_3.1.0.jar";"C:\Program Files\Texas Instruments\ccsv4\DebugServer\packages\ti\dss\java\com.ti.debug.engine_1.0.0.jar";"C:\Program Files\Texas Instruments\ccsv4\DebugServer\packages\ti\dss\java\dss.jar" DssBreakpointsExample.java
This will generate the 'DssBreakpointsExample.class' file. Note that the above example has '<JDK INSTALL>\bin' added to the system PATH so 'javac.exe' can be called from anywhere.
Running
Once the *.class file has been generated, the application can be run. Before running, two paths must be added to the system PATH:
- <INSTALL DIR>\ccsv4\common\bin
- <INSTALL DIR>\ccsv4\common\uscif
Ex:
> set PATH=%PATH%;C:\Program Files\Texas Instruments\ccsv4\common\bin;C:\Program Files\Texas Instruments\ccsv4\common\uscif
Now the application can be run. When calling 'java.exe':
- set the 'XPCOM.RUNTIME' system property needs to '<INSTALL DIR>\ccsv4\DebugServer\win32' with the '-D' option
- pass in the 'dss.jar' file and the path to the *.class file being run with the '-cp' option.
The following will run the example DSS Java 'DssBreakpointsExample' application:
> java -DXPCOM.RUNTIME="C:\Program Files\Texas Instruments\ccsv4\DebugServer\win32" -cp C:\DSS_Java_Example;"C:\Program Files\Texas Instruments\ccsv4\DebugServer\packages\ti\dss\java\dss.jar" DssBreakpointsExample
Using DVT APIs
When using DVT API calls:
- Add an additional line to the list of imported packages in your code:
import com.ti.dvt.engine.scripting.*;
- Add the following DVT JAR files to the classpath (along with the other JAR files) that is passed to the Java compiler:
- com.ti.dvt.scripting.engine_1.0.0.jar
- dvt.jar
- The DVT JAR files can be found in '<INSTALL DIR>\ccsv4\dvt\scripting'
- When running the application, add the 'dvt.jar' file to the classpath that is passed to 'java.exe'.
- Ex:
> java -DXPCOM.RUNTIME="C:\Program Files\Texas Instruments\ccsv4\DebugServer\win32" -cp .;"C:\Program Files\Texas Instruments\ccsv4\DebugServer\packages\ti\dss\java\dss.jar";"C:\Program Files\Texas Instruments\ccsv4\dvt\scripting\dvt.jar" DssDvtExample
References
TBD
Leave a CommentComments
Comments on DSS from Java


Hi, could the author provide the full java source code?
--AppleCat 02:57, 11 June 2009 (CDT)