ELDK usage
From Texas Instruments Embedded Processors Wiki
There are various ARM toolchains available which can be used for DaVinci U-Boot and Linux development on ARM side. One of these is ELDK - the Embedded Linux Development Kit - from DENX Software Engineering (the people behind U-Boot). If you like to test/use ELDK for DaVinci development, this article may help you.
Note: This article only gives you some rough ELDK quick start instructions and DaVinci specials. For more and general information about ELDK see ELDK overview.
Download
Go to
and download 4.1/arm-linux-x86/iso/ arm-2007-01-21.iso (~210MB) from one of the various mirrors.
Note: We use the ELDK with standard GLibc. If you like a smaller system, consider using the UCLibc version arm-2007-01-22-uclibc.iso
Installation
Put downloaded arm-2007-01-21.iso to directory where you like to install ELDK. Then, create two directories, one temporary we mount the *.iso image to and one where we install ELDK into:
host > mkdir eldk host > mkdir install_mount
Change into ELDK installation directory and mount iso image in top directory. Most probably (depends on your system configuration), this has to be done as root:
host > cd eldk/ host/eldk > su host/eldk # mount -o loop,exec ../arm-2007-01-21.iso ../install_mount/ host/eldk # exit
Exit to do installation as normal user. Then, content of iso image should be visible:
host/eldk > ls ../install_mount/ . arm ELDK_FIXOWNER etc install RPMS tools .. common ELDK_MAKEDEV icons README.html sys version
If you like more info about ELDK and what we are doing here, open README.html above in web browser. Now we install ARM development environment (usable for DaVinci) in current (host/eldk) directory:
host/eldk > ../install_mount/install arm
This installs ELDK in eldk directory. Use install option -d <dir> to select an other installation directory.
... take some time
If installation finished, make eldk_init script executable...
host/eldk > chmod u+x eldk_init
... and unmount install ISO image, we don't need it any more:
host/eldk > su host/eldk # umount ../install_mount/ host/eldk # exit
If you like, delete arm-2007-01-21.iso now if you need the space. And download again, if you need it later again ;)
Usage
Usage is simple. Every time you like to use ELDK tools, go to ELDK installation directory (e.g. host/eldk) and execute there
host/eldk > ./eldk_init arm
This sets some environment variables necessary for ELDK usage:
ARCH=arm CROSS_COMPILE=arm-linux- DEPMOD=host/eldk/usr/bin/depmod.pl PATH=host/eldk/usr/bin:host/eldk/bin:...
and then you can use ELDK tools. E.g. change to directories where U-Boot or DaVinci Linux kernel is stored and compile it.
Note: If you don't like to execute eldk_init everytime manually, put the environment variables set by this script into some global configuration files, e.g. .bashrc.
Leave a CommentComments
Comments on ELDK usage

i understand..what u have written above...but cn u tell me is dis tool-chain has included all the necessery componants like"uboot,gcc adn glibc for ARM"..plz tell me one more thing,,that..what are the tools and things which will be port to our board from this tool chain or from outside...??...
i am waiting for ur ans...
--Mpchap 06:12, 29 January 2011 (CST)