Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

EVMK2E Hardware Setup

From Texas Instruments Wiki
Jump to: navigation, search

Last updated: 01/12/2016


Hardware Setup

NoteNote: The EVM board is sensitive to electrostatic discharges (ESD). Use a grounding strap or other device to prevent damaging the board. Be sure to connect communication cables before applying power to any equipment.

Attach the Ethernet cable

Using the Ethernet cable supplied, connect one end of the cable to the Ethernet Port 0 (At bottom one) on the EVM and the other end to your PC. The below picture shows which Ethernet Port is port 0:

Evmk2e-image001.jpg

Connect the JTAG interface

Use the USB to USB mini-B cable provided. Connect the USB mini-B connector to the USB mini-B interface near to the RST_PWR1 (Red color) button on the EVM, and the USB connector to your PC. This enables XDS-2xx emulation and is directly useable by CCS. If you are using a different JTAG, you can connect it at MIPI60 connector (EMU1).

Set the boot mode switch SW1

SPI Little Endian Boot mode (Default factory setting)

 MSB                         LSB
 SW1 - 1(OFF) 2(OFF) 3(ON) 4(OFF)

Evmk2e-image002.jpg

NoteNote: Here a switch on “ON” position should be considered as “1”.

No Boot/JTAG DSP Little Endian Boot mode

 MSB                      LSB
 SW1 - 1(ON) 2(ON) 3(ON) 4(ON)

Evmk2e-image003.jpg

Attach the serial port cable to the SoC UART port

Connect the SoC UART port to PC using the serial cable provided with the EVM. The SoC UART port is the 4-pin white connector COM1 of the EVM.

Start TeraTerm or HyperTerminal and set configuration to

  • Baud Rate or Bits per second: 115200
  • Data Bits: 8
  • Parity: None
  • Stop Bits: 1
  • Flow Control: None

Connect the power cable

Connect the power cable to the EVM power jack on the board. To be ESD safe, plug in the other end of the power cable only after you have connected the power cord to the board. Then turn on the board.

DIP Switch and Bootmode Configurations

EVM SW1 switch Bootmode Configuration

The table below shows the bootmode combinations for the BMC v1.1.0.x. and value selected from internal flash memory of LM3s2d93.

DIP Switch settings Selected

High_value of that bootmode

Low_value of that bootmode

Selected bootmode

0000

0x00000000

0x00010067

ARM NAND

0001

0X00000000

0x00100001

DSP No Boot

0010

0x00000000

0x00008005

ARM SPI

0011

0x00000000

0x00100003

ARM I2C Master

0100

0x00000000

0x0000006F

ARM UART Master

0101

0x00000000

0x0001506B

ARM RBL EthNet

0110

0x00000000

0x00001061

Sleep with Max PLL and ARM Bypass

0111

0x00000000

0x00001061

Sleep with Max PLL

1000

0x00000000

0x00010167

DSP NAND

1001

0x00000000

0x00001061

Sleep with Slow PLL and ARM Bypass

1010

0x00000000

0x00008105

DSP SPI-boot

1011

0x00000000

0x00100103

ARM I2C Master

1100

0x00000000

0x0000016F

DSP UART boot

1101

0x00000000

0x0001516B

DSP RBL ENET

1110

0x00000000

0x00003661

Sleep with Slow PLL and Slow ARM PLL

1111

0x00000000

0x00100001

DSP No-Boot


How To Guides

Host driver for on-board mini-USB connector

The K2E EVM has a CP2105 device on-board. A driver must be installed on the host PC in order to be able to communicate with the EVM using the CP2105 mini-USB connector located at the corner edge of the EVM. The driver can be downloaded from CP2105 driver download.

Both Linux and Windows host machine drivers can be downloaded from this page. For Linux host machine, please follow the instructions given in the release notes. There are two versions of drivers for Linux kernel version 3.x.x and 2.6.x. Please download appropriate drivers after identifying the correct kernel version of the user’s host machine.

NoteNote: Before testing the USB connection, make sure that the mini-USB cable is plugged into the port on the base board.

After installing the driver and connecting the USB cable, two COM ports should be visible in the list of COM ports available to connect to in the PC Host terminal console. The lower COM port (Enhanced) corresponds to the SoC UART and the higher (Standard) one corresponds to the MCU UART.

BMC Version Check and Update

BMC, or Board Management Controller, takes care of the power, clocks, resets, bootmodes, etc. of the EVM.

You can check the version by:

  1. Opening a hyperterminal or another similar type of console application.
  2. Set COM Port to higher value.
    • When you connect to CP2105 mini-USB on the EVM it will provide two COM port connections, one to the SOC UART and one to BMC UART.
    • The SOC UART will always be the “Enhanced” COM port, for example COM6 (actual COM PORT values will vary.)
  3. Set COM port properties appropriately:
    • Baud Rate or Bits per second: 115200
    • Data Bits: 8
    • Parity: None
    • Stop Bits: 1
    • Flow Control: None
  4. At BMC prompt type 'ver' (no quotes).
  5. Check BMC version

Evmk2e-image005.jpg

If an in-field update is needed, downloaded the latest version here (labeled “BMC”) and follow instructions below.

Prepare EVM for in-field update

  1. Remove power to the EVM.
  2. Set boot mode to "No Boot mode” (see above).
  3. Remove the MCU_BOOTSELECT (CN4) jumper (see picture below for location of jumper.)
  4. Make sure your
    • USB cable is connected to CP2105 mini-USB (not XDS200 Emulator USB) or
    • Connect 4pin UART cable to COM1: MCU UART connector
  5. Make sure no HyperTerminal/Console connected to BMC COM port are open or active.
  6. Use the LM Flash Programmer (available here) to update the firmware, as detailed in the steps below.

CN 4

Perform in-field update

  1. Apply power to the EVM. No LED's will be illuminated and no LCD backlight or characters will be on because the BMC is waiting for a command rather than executing from Flash.
  2. Open the LM Flash programmer utility. (Default location Start Menu -> All Programs -> Texas Instruments -> Stellaris -> LM Flash Programmer -> LM Flash Programmer )
  3. In the LM Flash Programmer Utility ‘Configuration’ tab, in the interface section, select ‘Serial (UART)’ from the drop-down box on the left.
  4. Select the BMC COM Port (the same COM port used to issue the ver command earlier), and set the ‘Baud Rate’ to 115200.
  5. Set ‘Transfer Size’ to 60, and make sure ‘Disable Auto Baud Support’ is unchecked. See image below.
  6. In the ‘Program’ tab, Browse to the location of the binary file containing the firmware update, and select it.
  7. Leave all other options as default, and press the ‘Program’ button.
  8. After the programming is complete, power off the board.
  9. Reconnect the jumper.
  10. Open the HyperTerminal/Console for the BMC COM port.
  11. Apply power to the EVM. When BMC completes initialization of board it will show latest version of BMC in Console.
  12. If step 9 was done after power was applied, just type "ver" at BMC prompt.

Evmk2e-image007.jpg

UCD Power Management Update

There is one power management module (a.k.a. UCD) located on the EVM. It can be identified by its address: 104(68h). Each module contains non-volatile registers that determine its operation. It may be necessary to update these registers in the field after the board has been shipped.

This update can be performed through the BMC, which can issue commands to the UCD modules to update the register settings. The Power Management Configuration Update Tool performs the task of sending commands to the BMC to get the current module versions, and perform updates using configuration files.

The latest version of the tool is available from here along with instructions on using the tool, and the latest configuration files (txt files). Please follow the instructions provided to check the current module versions, and update them accordingly.

NoteNote: The DIP switch configuration of the board when running the update is irrelevant.