Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

EZ-FET lite

From Texas Instruments Wiki
Jump to: navigation, search

The eZ-FET lite is a low cost USB-based on-board emulation solution for MSP430 microcontrollers. It allows direct interfacing to a PC for easy programming, debugging, and evaluation and provides a USB-to-UART bridge for serial connection to the target microcontroller.

The eZ-FET lite on-board emulation is supported by the MSP430 DLL and can be used with IAR Embedded Workbench™ for MSP430 Integrated Development Environment (IDE) or Code Composer Studio™ (CCS) IDE to write, download, and debug applications.

The debugger is unobtrusive, allowing the user to run an application at full speed with hardware breakpoints and single stepping available while consuming no extra hardware resources.

The following picture shows an example of the eZ-FET lite on-board emulation. The emulation components are placed within the red highlighted areas.


eZ-Fet lite


Features

  • USB debugging and programming interface featuring a driverless installation
  • Application UART serial communication with up to 1MBaud
  • Green and red LED for visual feedback
  • Field-updateable firmware
  • Supports all MSP430 devices compatible with SBW programming
  • Schematic, reference layout and production test software available as open source package

Hardware and Software Requirements

The following hardware and software is required to use the eZ-FET on-board emulation

  • Personal computer with Windows O/S or Linux
  • MSP430 Debug Stack (MSP430.DLL 3.3.0.6 or higher)
  • Texas Instruments Code Composer Studio 5.4 or higher
  • IAR Embedded Workbench 5.50 or higher


Please Note

  • Do not change eZ-FET Lite layout. Changes could cause functional failures. In case of failures Texas Instruments will not give any support.
  • Make sure that you use the correct firmware and tests images matching you eZ-FET Lite firmware.