Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

EZ430-RF256x

From Texas Instruments Wiki
Jump to: navigation, search

Return to CC256x EVM Platform

Introduction

The EZ430-RF256x is a complete TI Bluetooth evaluation and demonstration tool for the MSP430 and CC256x that includes all the necessary hardware and software in a convenient USB stick.

  • You can follow this link to see Step by Step out of box instructions.
  • We also have a short FAQ for troubleshooting the EZ430-RF256x Kit.
  • The EZ430-RF256x can be used as a stand-alone development tool. Additionally, the RF256xT target board also may be detached from the debugging interface and integrated into another design by removing the plastic enclosure.

This platform is composed of the CC256x Bluetooth device and the msp430f5438A microcontroller. Additional key terms. The tool also comes with a sample PC game that you can play using the CC256x target board as a remote controller.
The table below depicts briefly the hardware and software partition of this platform.


Device Hardware Software

msp430f5438A

  • Host TI’s Bluetooth Stack
  • Classic BT and BLE Sample Demos
  • UART


cc256x.jpg
CC256x
  • BT Firmware
  • MAC/PHY




Please Note:

  • The EZ430-RF256x is intended as a software and end design evaluation platform. It is not intended for hardware evaluation purposes and does not contitute a reference hardware design. As such, TI does not provide schematics and/or layout information. Customers wishing to leverage TI's Bluetooth connectivity should design using Panasonic's Bluetooth modules.
  • The EZ430-RF256x SDK license requires that the MSP430BT5190 must be used only in combination with TI Bluetooth solutions such as the CC256x for end product production.

Reference Schematic


The target board features an MSP430F5438A and most of its pins are routed out. Please refer to the PAN1323ETU Design Guide for more information.




Kit Content

The EZ430-RF256x kit can be ordered here in order to evaluate the solution. The kit content is listed below:

  • 2 target boards with MSP430BT5190 and PAN1323 Bluetooth module
  • 1 Battery pack with 2 AAA batteries
  • 1 USB emulator
  • plastic case for emulator + target board
  • CD and Quick Start Guide
Exclamation-icon.jpg This device is granted for use in mobile only configurations in which the antennas used for this transmitter must be installed to provide a separation distance of at least 20cm from all persons (as specified in Panasonics’s grant T7V1315A) and not be co-located with any other transmitters except in accordance with FCC and/or Industry Canada multi-transmitter product procedures as applicable”



Key Features

  • USB debugging and programming interface (emulator board) featuring a driverless installation and application backchannel
  • PAN1323 which contains TI's CC256x – TI single-chip Bluetooth v4.0 solution
  • MSP430F5438A – 25MHz, 256KB Flash, 16KB RAM, 12Bit ADC, 4-USCIs, 32-bit HW Multi
  • Interactive sample PC game for demonstration of Bluetooth use in a remote control application
  • VTI's 3-axis accelerometer with user selectable 2g and 8g measurement range and capable of sub-11uA current consumption at 40/10Hz sample rate.
  • Temperature sensor with accuracy as low as +/-2 degrees celsius from -40C to +85C.
  • Supports software development with the MSP430BT5190 microcontroller
  • Two application LEDs, one power LED
  • Two application buttons, one reset button
  • Multiple debug headers
  • Removable USB stick enclosure


         EZ430RF256xkit.jpg

 

HW Architecture 

                                                Ez430 unit arch.png

 

NOTES:

  • EZ430U supports maximum UART baudrate of 9.6kbps (please note that this is an EZ430U HW limitation).
  • uEVM debug header is not populated.

 

RF256xT Target Board Architecture & Pinout  



EZ430-RF256xT Arch.PNG



MSP430BT5190 Interfaces
Ez430rfpan1315 headers.jpg

MSP430BT5190 IF 2.png

                             

Debug Headers

RF256xT_Debug_Headers_2.png

EZ430U USB Debugging I/F Connector Pinout

  
USB Debug IF Pinout 2.png
      

uEVM connector

This connector is present on the backside of the target board and provides access to more pins of the MSP430BT5190 on board.
The footprint of the connector can be populated with a DF40C-40DS-0.4V connector, readily available at  distributors such as Digikey and Mouser.
The connector's functionality is as follows:

Ez430rfpan1315 p1 uevm desc.png

SW Architecture

Bluetooth SW Arch 2.jpg


  • FreeRTOS is ported on the MSP430BT5190 device to support the Bluetooth stack for read and write tasks.
  • Users can develop their own application and interact with the Bluetooth stack APIs to enable Bluetooth connectivity on their end products.
  • MSP430BT5190-CC256x Developers Guide contains detailed information on the software architecture and Bluetooth stack APIs.



Suggested Reading


Support

FAQ