EZ430 Emulator Upgrade

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

The firmware on the eZ430 emulator can be manually upgraded in order to add new functionality such as the Application UART and to support additional MSP430 devices. The latest version of the eZ430 emulator is included with the eZ430-Chronos. It supports the broadest range of MSP430 devices including the MSP430F2xx, 5xx, and CC430 devices. It's recommended to use the Chronos emulator firmware in order to have the latest device support.

Note: The original eZ430-F2013 emulator with the 4-pin header cannot be upgraded using this method because it contains unique functionality for both the MSP430F1612 and the TUSB3410 which doesn't support the new firmware.

This procedure is NOT supported by TI. Do so at your own risk.

Contents

Hardware Requirements

  1. eZ430 Rev 2 Emulator.  Available on eZ430-RF2500
  2. MSP-FET430UIF
  3. 0.1" Pin headers
  4. Short wire or an alligator clip (preferred)

EZ430 Firmware Download

eZ430 Firmware V30394216 Release Date: 11/09/2011

Download eZ430 Firmware

Release Notes

Supported Features:


Supported Devices:


Supported Tools:

Instructions

  1. Modify the MSP-FET430UIF’s JTAG Cable to connect to eZ430. The easiest way consists of:
    1. 4x1 0.1” header starting on pin 1 (all of the signals are on the same side of the header)
    2. Wire on pin 9 (GND)
      Connections on the FET
  2. Connect the eZ430 emulator to the FET. (Ignore TP2 on the eZ430). Connect external power via the USB port.
    eZ430 JTAG Connections
  3. Update the eZ430 firmware using the Elprotronic FET-Pro430 software.

    Configure the following FET-Pro430 settings:
    1. Select “Open Code File” > Browse to new firmware image. (Download the eZ430 Emulator Firmware)
    2. Select Microcontroller Type: MSP430F1612
    3. Under Setup > Connection / Device Reset ensure the following:
      1. “JTAG (4 wires)” is selected
      2. The COM port corresponds to your FET tool (says something like “COM111”)
    4. Select “AUTO PROG.”
      1. If the upgrade fails, double check your settings and your hardware connections.
FETPro-430 Configuration Screenshot
Leave a Comment

Comments

Comments on EZ430 Emulator Upgrade


Caolang said ...

I have done all the steps, the program announced that the flashing is done. The PC still recognizes the ez430 emulator as MSP-FET430UIF-VCP but now I cannot use it to debug the F2013 board any more. What happened to my emulator?

--Caolang 07:25, 7 April 2011 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox