Example GStreamer Pipelines
From Texas Instruments Embedded Processors Wiki
Purpose
This page provides example pipelines that can be copied to the command line to demonstrate various GStreamer operations. Some of the pipelines may need modification for things such as file names, ip addresses, etc.
It is our hope that people using this page will add new interesting pipelines that they themselves are using. For example, on DM6467 if you are decoding a 1080 video and outputing to component please include your pipeline for others to use as a reference.
Refer to this Gstreamer article for more information on downloading and building TI Gstreamer elements. The project is hosted at http://gstreamer.ti.com. If you are interested in understanding the design details then watch video presentation http://software-dl.ti.com/sdo/sdo_apps_public_sw/GStreamer_On_TI/FLV1/GStreamer_On_TI.htm
Testing
Currently these pipelines have not undergone any extensive testing. If you find an error in a pipeline please correct it.
Media files
You should be able to use any audio and video media file that conforms to the appropriate standard.
Creating an AVI file
The following ffmpeg command takes a .mov file (say from the Apple movie trailers site) and make an AVI file. Run the command on your host computer.
ffmpeg -i tropic_thunder-tlr1a_720p.mov -r 60 -b 6000000 -vcodec mpeg2video -ab 48000000 -acodec libmp3lame -s 1280x544 tropic.avi
Supported Platforms
Following are a list of supported platforms, with links that jump directly to pipeline examples for each platform.
DM355
This section covers pipelines for common use cases for the DM355 processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/dm355/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
cat /dev/zero > /dev/fb2 2> /dev/null
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
Loopback: Video
v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite contiguousInputFrame=TRUE sync=false
videotestsrc (generated video test-bars):
gst-launch -v videotestsrc ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite accelFrameCopy=FALSE sync=false
Loopback: Audio
No pipelines here yet. Please feel free to add your own.
Loopback: Audio + Video
No pipelines here yet. Please feel free to add your own.
Decode Video Files
NTSC:
gst-launch -v filesrc location=sample.m4v ! TIViddec2 codecName=mpeg4dec engineName=codecServer ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
PAL:
gst-launch -v filesrc location=sample.m4v ! TIViddec2 codecName=mpeg4dec engineName=codecServer ! TIDmaiVideoSink videoStd=D1_PAL videoOutput=composite sync=false
Decode Audio Files
This platform does not have an accelerated audio decoder element. You can use the ARM based audio decoders "mad", "ffdec_mp3" or "faad"
MP3 pipelines:
gst-launch filesrc location=sample.mp3 ! mad ! alsasink gst-launch filesrc location=sample.mp3 ! mp3parse ! ffdec_mp3 ! alsasink
AAC pipeline:
gst-launch filesrc location=sample.aac ! faad ! alsasink
Decode .AVI Files
The following pipeline assumes you have an AVI file with MPEG-4 Video and MP1L2 or MP3 Audio. Note that not all MPEG-4 video streams can be played using the DM355 MPEG-4 decoder -- make sure the MPEG-4 stream was encoded with the DM355 MPEG-4 encoder or another compatible encoder.
gst-launch -v filesrc location=sample.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite
Encode Video Files
videotestsrc (generated video test-bars):
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer ! filesink location=output.m4v
v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer contiguousInputFrame=TRUE ! filesink location=output.m4v
Encode Audio Files
This platform does not have an accelerated audio encoder element. You can use the ARM based audio encoders "lame" or "faac"
No pipelines here yet. Please feel free to add your own.
Image Encode
A simple pipeline that converts a UYVY image into JPEG format.
gst-launch -v filesrc location=sample.yuv ! TIImgenc1 resolution=720x480 iColorSpace=UYVY oColorSpace=YUV420P qValue=75 ! filesink location=output.jpg
Image Decode
A simple pipeline that converts a JPEG image into UYVY format.
gst-launch -v filesrc location=sample.jpg ! TIImgdec1 resolution=720x480 ! filesink location=sample.yuv
Resize
A simple pipeline capturing from v4l2src and resizing to CIF.
gst-launch v4l2src always-copy=FALSE ! TIVidResize contiguousInputFrame=TRUE ! 'video/x-raw-yuv,width=352,height=288' ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
Network Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
MPEG-4 Encode/Stream/Decode:
A simple RTP server to encode and transmit MPEG-4
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc1 codecName=mpeg4enc engineName=encode contiguousInputFrame=TRUE ! rtpmp4vpay pt=96 ! udpsink host=<HOST IP ADDRESS> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)1, config=(string)000001010000012000845d4c28b421e0a21f, payload=(int)96, ssrc=(guint)3412089386, clock-base=(guint)945410414, seqnum-base=(guint)27711
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to decode MPEG-4 and display on HOST machine
gst-launch -v udpsrc port=5000 caps="<PASS_CAPS_FROM_SERVER>" ! rtpmp4vdepay ! ffdec_mpeg4 ! xvimagesink
For sending and receiving MPEG-4 with DM355 EVM you can use these 2 pipelines :
RTP server side :
gst-launch -v videotestsrc ! TIVidenc1 codecName=mpeg4enc engineName=encode ! rtpmp4vpay send-config=true ! udpsink host=<HOST IP ADDRESS> port=5000
Don't forget to set the "send-config" property to true
RTP client side :
gst-launch -v udpsrc port=5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)1, config=(string)000001010000012000845d4c285020f0a21f, payload=(int)96, ssrc=(guint)3319524202, clock-base=(guint)4012564513, seqnum-base=(guint)25833" ! rtpmp4vdepay ! TIViddec2 codecName=mpeg4dec engineName=decode ! TIDmaiVideoSink videoStd=D1_PAL videoOutput=composite sync=false
Note that client should be started before server
DM357
This section covers pipelines for common use cases for the DM357 processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/dm357/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
cat /dev/zero > /dev/fb2 2> /dev/null
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
Notes on DM357 Performance: There is a known issue on DM357 where there are intermittent freezes in video and audio playback in some cases. If you experience this, nicing your gst-launch command to 15 as follows may resolve the issue:
nice -n 15 gst-launch .... (rest of gst-launch command)
Loopback: Video
v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite contiguousInputFrame=TRUE sync=false
videotestsrc (generated video test-bars):
gst-launch -v videotestsrc ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite accelFrameCopy=FALSE sync=false
Loopback: Audio
No pipelines here yet. Please feel free to add your own.
Loopback: Audio + Video
No pipelines here yet. Please feel free to add your own.
Decode Video Files
H.264/NTSC:
gst-launch -v filesrc location=sample.264 ! TIViddec codecName=h264dec engineName=hmjcp ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
MPEG-4/NTSC:
gst-launch -v filesrc location=sample.m4v ! TIViddec codecName=mpeg4dec engineName=hmjcp ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
Decode Audio Files
This platform does not have an accelerated audio decoder element. You can use the ARM based audio decoders "mad" or "faac"
No pipelines here yet. Please feel free to add your own.
Decode .MP4 Files
No pipelines here yet. Please feel free to add your own.
Decode .AVI Files
The following pipeline assumes you have an AVI file with MPEG-2 or MPEG-4 Video and MP1L2 or MP3 Audio.
gst-launch -v filesrc location=sample.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! queue ! TIViddec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite
Encode Video Files
H.264/v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc codecName=h264enc engineName=hmjcp contiguousInputFrame=TRUE ! filesink location=sample.264
MPEG-4/v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc codecName=mpeg4enc engineName=hmjcp contiguousInputFrame=TRUE ! filesink location=sample.m4v
H.264/videotestsrc (generated video test-bars):
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc codecName=h264enc engineName=hmjcp ! filesink location=sample.264
MPEG-4/videotestsrc (generated video test-bars):
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc codecName=mpeg4enc engineName=hmjcp ! filesink location=sample.m4v
Encode Video in Container
Encode H.264 in quicktime container (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc codecName=h264enc engineName=hmjcp contiguousInputFrame=TRUE byteStream=FALSE ! qtmux ! filesink location=sample.mp4
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc codecName=h264enc engineName=hmjcp byteStream=FALSE ! qtmux ! filesink location=sample.mp4
Image Encode
A simple pipeline that converts a YUV422P image into JPEG format.
gst-launch filesrc location=sample.yuv ! TIImgenc resolution=720x480 iColorSpace=UYVY oColorSpace=YUV422P qValue=75 ! filesink location=sample.jpg
Image Decode
A simple pipeline that converts a JPEG image into UYVY format.
gst-launch filesrc location=sample.jpg ! TIImgdec resolution=720x480 ! filesink location=sample.yuv
Resize
A simple pipeline capturing from v4l2src and resizing to CIF.
gst-launch v4l2src always-copy=FALSE ! TIVidResize contiguousInputFrame=TRUE ! 'video/x-raw-yuv,width=352,height=288' ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite accelFrameCopy=FALSE sync=false
Network Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
H.264 Encode/Stream/Decode:
A simple RTP server to be run on EVM.
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc codecName=h264enc engineName=hmjcp contiguousInputFrame=TRUE ! rtph264pay pt=96 ! udpsink host=<HOST_PC_IP> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstRtpH264Pay:rtph264pay0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)42801e, sprop-parameter-sets=(string)\"Z0KAHtoC0PRA\\,aM48gA\\=\\=\", payload=(int)96, ssrc=(guint)895989858, clock-base=(guint)3971488929, seqnum-base=(guint)34821
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to be run on Host PC (Linux).
gst-launch -v udpsrc port=5000 caps="<CAPS_FROM_SERVER>" ! rtph264depay ! ffdec_h264 ! xvimagesink
DM644x
This section covers pipelines for common use cases for the DM644x processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/dm6446/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
cat /dev/zero > /dev/fb2 2> /dev/null
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
Loopback: Video
v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite contiguousInputFrame=TRUE sync=false
videotestsrc (generated video test-bars):
gst-launch -v videotestsrc ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite accelFrameCopy=FALSE sync=false
Loopback: Audio
No pipelines here yet. Please feel free to add your own.
Loopback: Audio + Video
No pipelines here yet. Please feel free to add your own.
Decode Video Files
H.264/NTSC:
gst-launch -v filesrc location=sample.264 ! TIViddec2 codecName=h264dec engineName=decode ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
MPEG-2/NTSC:
gst-launch -v filesrc location=sample.m2v ! TIViddec2 codecName=mpeg2dec engineName=decode ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
MPEG-4/NTSC:
gst-launch -v filesrc location=sample.m4v ! TIViddec2 codecName=mpeg4dec engineName=decode ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
Decode Audio Files
AAC:
gst-launch -v filesrc location=sample.aac ! TIAuddec1 codecName=aachedec engineName=decode ! alsasink sync=false
Decode .MP4 Files
The following pipeline assumes you have an .MP4 file with H.264 Video and AAC Audio.
gst-launch -v filesrc location=sample.mp4 ! qtdemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! TIAuddec1 ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite
Decode .AVI Files
The following pipeline assumes you have an .AVI file with MPEG-2 or MPEG-4 Video and MP1L2 or MP3 Audio.
gst-launch -v filesrc location=sample.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite
Decode .TS Files
The following pipeline assumes you have an transport stream file with H.264 Video and MP1L2 or MP3 Audio.
gst-launch filesrc location=sample.ts ! typefind ! mpegtsdemux name=demux demux. ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! typefind ! mad ! alsasink demux. ! typefind ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPOSITE
Encode Video Files
H.264/v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE ! filesink location=sample.264
MPEG-4/v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=mpeg4enc engineName=encode contiguousInputFrame=TRUE ! filesink location=sample.m4v
H.264/videotestsrc (generated video test-bars):
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=encode ! filesink location=sample.264
MPEG-4/videotestsrc (generated video test-bars):
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=mpeg4enc engineName=encode ! filesink location=sample.m4v
Encode Video in Container
Encode H.264 in quicktime container (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE byteStream=FALSE ! qtmux ! filesink location=sample.mp4
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=encode byteStream=FALSE ! qtmux ! filesink location=sample.mp4
Resize
A simple pipeline capturing from v4l2src and resizing to CIF.
gst-launch v4l2src always-copy=FALSE ! TIVidResize contiguousInputFrame=TRUE ! 'video/x-raw-yuv,width=352,height=288' ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false accelFrameCopy=FALSE
Network Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
H.264 Encode/Stream/Decode:
A simple RTP server to be run on EVM.
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE ! rtph264pay pt=96 ! udpsink host=<HOST_PC_IP> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstRtpH264Pay:rtph264pay0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)42801e, sprop-parameter-sets=(string)\"Z0KAHtoC0PRA\\,aM48gA\\=\\=\", payload=(int)96, ssrc=(guint)895989858, clock-base=(guint)3971488929, seqnum-base=(guint)34821
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to be run on Host PC (Linux).
gst-launch -v udpsrc port=5000 caps="<PASS_CAPS_FROM_SERVER>" ! rtph264depay ! ffdec_h264 ! xvimagesink
MPEG-4 Encode/Stream/Decode:
A simple RTP server to encode and transmit MPEG-4
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc1 codecName=mpeg4enc engineName=encode contiguousInputFrame=TRUE ! rtpmp4vpay pt=96 ! udpsink host=128.247.105.80 port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)5, config=(string)000001b005000001b509000001000000012000847a9828b421e0a31f, payload=(int)96, ssrc=(guint)302303174, clock-base=(guint)347576712, seqnum-base=(guint)48616
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to decodes MPEG-4 and display on HOST machine
gst-launch -v udpsrc port=5000 caps="<PASS_CAPS_FROM_SERVER>" ! rtpmp4vdepay ! ffdec_mpeg4 ! xvimagesink
MPEG-4 Receive/Decode/Display:
This section gives example where EVM acts as RTP client, which receives encoded stream via udp then decodes and display output. Host PC can be used as server to transmit encoded stream.
A simple RTP server which encodes and transmits MPEG-4 on DM6446 EVM.
gst-launch-0.10 videotestsrc ! 'video/x-raw-yuv,width=720,height=480' ! ffenc_mpeg4 ! rtpmp4vpay ! udpsink host=<EVM_IP_ADDR> port=5000 -v
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to receive and decode the MPEG-4 encoded stream.
gst-launch -v udpsrc port=5000 caps="<CAPS_FROM_SERVER>" ! rtpmp4vdepay ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
DM365
This section covers pipelines for common use cases for the DM365 processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/dm365/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
cat /dev/zero > /dev/fb2 2> /dev/null
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
Please see some special notes while playing 720P clip here
Loopback: Video
Generated_D1, composte out (videotestsrc):
gst-launch -v videotestsrc ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite accelFrameCopy=FALSE sync=false
Generated_720p60, component out (videotestsrc):
gst-launch -v videotestsrc !video/x-raw-yuv,width=1280,height=720 ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component accelFrameCopy=FALSE sync=false
Capture_D1 (v4l2src):
gst-launch -v v4l2src always-copy=FALSE input-src=composite ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite contiguousInputFrame=TRUE sync=false
Capture_720P (v4l2src):
gst-launch -v v4l2src always-copy=FALSE ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component contiguousInputFrame=TRUE sync=false
Loopback: Audio
Generated audio tone (audiotestsrc):
gst-launch audiotestsrc num-buffers=1000 ! alsasink
Captured audio (alsasrc):
gst-launch -v alsasrc ! alsasink sync=false
Loopback: Audio + Video
No pipelines here yet. Please feel free to add your own.
Decode Video Files
MPEG-4 -> NTSC_D1:
gst-launch -v filesrc location=sample_ntsc_D1.mpeg4 ! TIViddec2 engineName=codecServer codecName=mpeg4dec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPOSITE sync=FALSE
MPEG-4 -> PAL_D1:
gst-launch -v filesrc location=sample_pal_D1.mpeg4 ! TIViddec2 engineName=codecServer codecName=mpeg4dec ! TIDmaiVideoSink videoStd=D1_PAL videoOutput=COMPOSITE sync=FALSE
MPEG-4 -> NTSC_720P:
gst-launch -v filesrc location=sample_720p.mpeg4 ! TIViddec2 codecName=mpeg4dec engineName=codecServer ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 !TIDmaiVideoSink videoStd=720P_60 videoOutput=COMPONENT sync=FALSE hideOSD=TRUE
H.264 -> NTSC_D1:
gst-launch -v filesrc location=sample_D1.264 ! TIViddec2 engineName=codecServer codecName=h264dec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPOSITE sync=FALSE
H.264 -> NTSC_720P:
gst-launch -v filesrc location=sample_720P.264 ! TIViddec2 codecName=h264dec engineName=codecServer ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component sync=false hideOSD=TRUE
MPEG-2 -> NTSC_D1:
gst-launch filesrc location=sample_D1.m2v ! TIViddec2 engineName=codecServer codecName=mpeg2dec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPOSITE sync=FALSE
MPEG-2 -> NTSC_720P:
gst-launch filesrc location=sample_720p.m2v ! TIViddec2 engineName=codecServer codecName=mpeg2dec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component sync=false hideOSD=TRUE
Decode Audio Files
AAC:
gst-launch -v filesrc location=sample.aac ! TIAuddec1 codecName=aacdec engineName=codecServer ! alsasink sync=false
Decode Container Files
AVI (MPEG-4 / MP3):
gst-launch filesrc location=sample.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! TIViddec2 engineName=codecServer codecName=mpeg4dec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPOSITE sync=FALSE
Encode Video Files
Generated_D1 (videotestsrc) -> MPEG-4:
gst-launch videotestsrc num-buffers=1000 ! video/x-raw-yuv, format=(fourcc)NV12 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer ! filesink location=output_gen_D1.m4v
YUV_D1 -> MPEG-4:
gst-launch filesrc location=sample_nv12.yuv ! video/x-raw-yuv, format=(fourcc)NV12, width=320, height=240, framerate=(fraction)30/1 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer ! filesink location=output_yuv_D1.m4v
Captured_D1 (v4l2src) -> MPEG-4:
gst-launch -v v4l2src always-copy=FALSE num-buffers=800 input-src=composite ! video/x-raw-yuv,format=(fourcc)NV12,width=720,height=480 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer ! filesink location=output_cap_D1.m4v
Captured_720P (v4l2src) -> MPEG-4:
gst-launch -v v4l2src always-copy=FALSE num-buffers=800 input-src=COMPONENT ! video/x-raw-yuv,format=(fourcc)NV12,width=1280,height=720 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer contiguousInputFrame=TRUE ! filesink location=output_cap_720P.m4v
Generated_D1 (videotestsrc) -> H.264:
gst-launch videotestsrc num-buffers=1000 ! video/x-raw-yuv, format=(fourcc)NV12 ! TIVidenc1 codecName=h264enc engineName=codecServer ! filesink location=output_gen_D1.264
YUV_D1 -> H.264:
gst-launch filesrc location=sample_nv12.yuv ! video/x-raw-yuv, format=(fourcc)NV12, width=320, height=240, framerate=(fraction)30/1 ! TIVidenc1 codecName=h264enc engineName=codecServer ! filesink location=output_yuv_D1.264
Captured_D1 (v4l2src) -> H.264:
gst-launch -v v4l2src always-copy=FALSE num-buffers=800 input-src=composite ! video/x-raw-yuv,format=(fourcc)NV12,width=720,height=480 ! TIVidenc1 codecName=h264enc engineName=codecServer ! filesink location=output_cap_D1.264
Captured_720P (v4l2src) -> H.264:
gst-launch -v v4l2src always-copy=FALSE num-buffers=800 input-src=COMPONENT ! video/x-raw-yuv,format=(fourcc)NV12,width=1280,height=720 ! TIVidenc1 codecName=h264enc engineName=codecServer contiguousInputFrame=TRUE ! filesink location=output_cap_720P.264
Generated_D1 (videotestsrc) -> MPEG-2:
gst-launch videotestsrc num-buffers=1000 ! video/x-raw-yuv, format=(fourcc)NV12 ! TIVidenc1 codecName=mpeg2enc engineName=codecServer ! filesink location=output_gen_D1.m2v
YUV_D1 -> MPEG-2:
gst-launch filesrc location=sample_nv12.yuv ! video/x-raw-yuv, format=(fourcc)NV12, width=320, height=240, framerate=(fraction)30/1 ! TIVidenc1 codecName=mpeg2enc engineName=codecServer ! filesink location=output_yuv_D1.m2v
Captured_D1 (v4l2src) -> MPEG-2:
gst-launch -v v4l2src always-copy=FALSE num-buffers=800 input-src=composite ! video/x-raw-yuv,format=(fourcc)NV12,width=720,height=480 ! TIVidenc1 codecName=mpeg2enc engineName=codecServer ! filesink location=output_cap_D1.m2v
Captured_720P (v4l2src) -> MPEG-2:
gst-launch -v v4l2src always-copy=FALSE num-buffers=800 input-src=COMPONENT ! video/x-raw-yuv,format=(fourcc)NV12,width=1280,height=720 ! TIVidenc1 codecName=mpeg2enc engineName=codecServer contiguousInputFrame=TRUE ! filesink location=output_cap_720P.m2v
Encode Audio Files
Captured (alsasrc) -> AAC:
gst-launch -v alsasrc num-buffers=1000 ! TIAudenc1 codecName=aaclcenc engineName=codecServer ! filesink location=output.aac
Captured (alsasrc) -> AAC + PlayBack:
gst-launch -v alsasrc num-buffers=1000 ! audio/x-raw-int, endianness=1234, signed=true, width=16, depth=16, rate=44100, channels=2 ! tee name=t ! queue ! TIAudenc1 bitrate=64000 engineName=codecServer codecName=aaclcenc ! filesink location=output.aac t. ! queue ! alsasink sync=false
PCM File -> AAC + PlayBack:
gst-launch filesrc location=sample.pcm ! audio/x-raw-int, endianness=1234, signed=true, width=16, depth=16, rate=44100, channels=2 ! tee name=t ! queue ! TIAudenc1 bitrate=64000 engineName=codecServer codecName=aaclcenc ! filesink location=output.aac t. ! queue ! alsasink sync=false
Encode Video in Container
Generated_D1 (videotestsrc) -> H.264 -> Quicktime container:
gst-launch -v videotestsrc num-buffers=2000 ! 'video/x-raw-yuv,format=(fourcc)NV12' ! TIVidenc1 codecName=h264enc engineName=codecServer byteStream=FALSE ! qtmux ! filesink location=output_gen_.mp4
Captured_D1 (v4l2src) -> H.264 -> Quicktime container:
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 input-src=composite ! video/x-raw-yuv,format=(fourcc)NV12,width=720,height=480 ! TIVidenc1 codecName=h264enc engineName=codecServer byteStream=FALSE ! qtmux ! filesink location=output_cap_.mp4
Image Encode
UYVY -> JPEG:
gst-launch filesrc location=sample_720x480.yuv ! TIImgenc1 resolution=720x480 iColorSpace=UYVY oColorSpace=YUV420P qValue=75 engineName=codecServer ! filesink location=output.jpg
Image Decode
JPEG -> UYVY:
gst-launch filesrc location=sample_720x480.jpg ! TIImgdec1 resolution=720x480 engineName=codecServer ! filesink location=output.yuv
Resize
Generated_CIF (videotestsrc) -> D1:
gst-launch videotestsrc ! video/x-raw-yuv, width=352, height=288, framerate=(fraction)30/1 ! TIVidResize ! video/x-raw-yuv,width=640,height=480, framerate=(fraction)30/1 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPOSITE sync=false
Captured_D1 (v4l2src) -> CIF:
gst-launch v4l2src always-copy=FALSE input-src=composite ! TIVidResize contiguousInputFrame=TRUE ! 'video/x-raw-yuv,width=352,height=288' ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
Note: To use the resize element as shown above, the IPIPE module must be configured in single-shot modeby setting "dm365_imp.oper_mode=1" in the kernel bootargs.
Network Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
MPEG-4 Encode/Stream/Decode:
A simple RTP server to encode and transmit MPEG-4
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc1 codecName=mpeg4enc engineName=encode contiguousInputFrame=TRUE ! rtpmp4vpay pt=96 ! udpsink host=<HOST_PC_IP> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)1, config=(string)000001010000012000845d4c28b42240a21f, payload=(int)96, ssrc=(guint)543171998, clock-base=(guint)1153531416, seqnum-base=(guint)45441
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to decodes MPEG-4 and display on HOST machine
gst-launch-0.10 -v udpsrc port=5000 caps="<CAP_FROM_SERVER>" ! rtpmp4vdepay ! ffdec_mpeg4 ! xvimagesink
H.264 Receive/Decode/Display:
This section gives example where EVM acts as RTP client, which receives encoded stream via udp then decodes and display output. Host PC can be used as server to transmit encoded stream.
A simple RTP client to recieve and decode the H.264 encoded stream.
gst-launch -v udpsrc port=5000 ! 'application/x-rtp, media=video, payload=96, clock-rate=90000, encoding-name=H264' ! rtph264depay ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
A simple RTP server which encodes and transmits H.264 to the DM365 EVM (Note: this is a command for a host Linux PC).
gst-launch-0.10 -vvv videotestsrc ! x264enc byte-stream=true bitrate=300 ! rtph264pay ! udpsink port=5000 host=<EVM_IP_ADDR> sync=false
Note: first run the client then server
DM6467
This section covers pipelines for common use cases for the DM6467 processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/dm6467/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
Loopback: Video
v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component contiguousInputFrame=TRUE sync=false
videotestsrc (generated video test-bars):
TIDmaiVideoSink does not support videotestsrc for DM6467.
Loopback: Audio
alsasrc (Capture):
gst-launch alsasrc ! alsasink
audiotestsrc (generated audio tone):
gst-launch audiotestsrc num-buffers=1000 ! alsasink
Loopback: Audio + Video
No pipelines here yet. Please feel free to add your own.
Decode Video Files
H.264/1080i30:
gst-launch filesrc use-mmap=true blocksize=40960 location=sample.264 ! queue max-size-buffers=0 max-size-time=0 max-size-bytes=2097152 ! TIViddec2 genTimeStamps=FALSE engineName=decode codecName=h264dec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=1080I_30
MPEG-2/1080i30:
gst-launch filesrc use-mmap=true blocksize=40960 location=sample.m2v ! queue max-size-buffers=0 max-size-time=0 max-size-bytes=2097152 ! TIViddec2 genTimeStamps=FALSE engineName=decode codecName=mpeg2dec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=1080I_30
Decode Audio Files
AAC:
gst-launch -v filesrc location=sample.aac ! TIAuddec1 codecName=aachedec engineName=decode ! alsasink sync=false
Decode .MP4 Files
The following pipeline assumes you have an .MP4 file with H.264 Video and AAC Audio.
gst-launch -v filesrc location=sample.mp4 ! qtdemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! TIAuddec1 ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=1080P_30
Decode .AVI Files
The following pipeline assumes you have an .AVI file with MPEG-2 Video and MP1L2 or MP3 Audio.
gst-launch -v filesrc location=sample.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=1080P_30
Decode .TS Files
The following pipeline assumes you have an transport stream file with H.264 Video and MP1L2 or MP3 Audio.
gst-launch -v filesrc location=sample.ts ! typefind ! mpegtsdemux name=demux demux. ! audio/mpeg ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! typefind ! mad ! alsasink demux. ! video/x-h264 ! typefind ! TIViddec2 ! TIDmaiVideoSink videoStd=1080P_30
Encode Video Files
H.264/v4l2src (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE ! filesink location=sample.264
H.264/videotestsrc (generated video test-bars):
gst-launch -v videotestsrc num-buffers=2000 ! 'video/x-raw-yuv,format=(fourcc)NV12' ! TIVidenc1 codecName=h264enc engineName=encode ! filesink location=sample.264
Encode Video in Container
Encode H.264 in quicktime container (Capture):
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE byteStream=FALSE ! qtmux ! filesink location=sample.mp4
gst-launch -v videotestsrc num-buffers=2000 ! 'video/x-raw-yuv,format=(fourcc)NV12' ! TIVidenc1 codecName=h264enc engineName=encode byteStream=FALSE ! qtmux ! filesink location=sample.mp4
Encode Audio Files
AAC/alsasrc (Capture):
gst-launch -v alsasrc ! TIAudenc1 codecName=aacheenc engineName=encode ! filesink location=sample.aac
AAC/alsasrc (Capture+Playback): This pipeline encodes 2000 buffers of audio data before exiting.
gst-launch -v alsasrc num-buffers=2000 ! audio/x-raw-int, endianness=1234, signed=true, width=16, depth=16, rate=44100, channels=2 ! tee name=t ! queue ! TIAudenc1 bitrate=64000 engineName=encode codecName=aacheenc ! filesink location=sample.aac t. ! queue ! alsasink sync=false
AAC/filesrc (PCM input file): This pipeline encodes 2000 buffers of audio data before exiting. You will need to create a PCM file. You can do so by decoding an audio file and sending the output to the filesink.
gst-launch filesrc location=sample.pcm ! audio/x-raw-int, endianness=1234, signed=true, width=16, depth=16, rate=44100, channels=2 ! tee name=t ! queue ! TIAudenc1 bitrate=64000 engineName=encode codecName=aacheenc ! filesink location=sample.aac t. ! queue ! alsasink sync=false
Resize
A simple pipeline capturing from v4l2src and resizing to CIF.
gst-launch v4l2src always-copy=FALSE ! TIVidResize contiguousInputFrame=TRUE ! 'video/x-raw-yuv,width=352,height=288,format=(fourcc)Y8C8' ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=composite sync=false
Network Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
H.264 Encode/Stream/Decode:
A simple RTP server to be run on EVM.
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE ! rtph264pay pt=96 ! udpsink host=<HOST_PC_IP> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)42801f, sprop-parameter-sets=(string)\"Z0KAH/QFoeiA\\,aN48gA\\=\\=\", payload=(int)96, ssrc=(guint)521259813, clock-base=(guint)1231006457, seqnum-base=(guint)2761
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to be run on Host PC (Linux).
gst-launch-0.10 -v udpsrc port=5000 caps="<CAP_FROM_SERVER>" ! rtph264depay ! ffdec_h264 ! xvimagesink
DM6467T
This section covers pipelines for common use cases for the DM6467T processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/dm6467/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
Loopback: Video
Generated (videotestsrc):
TIDmaiVideoSink does not support videotestsrc for DM6467T.
Capture_720P (v4l2src):
gst-launch -v v4l2src always-copy=FALSE ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component contiguousInputFrame=TRUE sync=false
Loopback: Audio
Generated audio tone (audiotestsrc):
gst-launch audiotestsrc num-buffers=1000 ! alsasink
Captured audio (alsasrc):
gst-launch -v alsasrc ! alsasink sync=FALSE
Loopback: Audio + Video
No pipelines here yet. Please feel free to add your own.
Decode Video Files
H.264 -> NTSC_D1:
gst-launch -v filesrc location=sample_D1.264 ! TIViddec2 engineName=codecServer codecName=h264dec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPONENT sync=FALSE
H.264 -> NTSC_720P:
gst-launch -v filesrc location=sample_720P.264 ! TIViddec2 codecName=h264dec engineName=codecServer ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component sync=false hideOSD=TRUE
H.264 -> NTSC_1080I30:
gst-launch -v filesrc use-mmap=true blocksize=40960 location=sample_1080i_30.264 ! queue max-size-buffers=0 max-size-time=0 max-size-bytes=2097152 ! TIViddec2 genTimeStamps=FALSE engineName=codecServer codecName=h264dec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=1080I_30
H.264 -> NTSC_1080P60:
gst-launch -v filesrc use-mmap=true blocksize=40960 location=sample_1080p_60.264 ! queue max-size-buffers=0 max-size-time=0 max-size-bytes=2097152 ! video/x-h264, framerate=60/1, width=1920, height=1080 ! TIViddec2 genTimeStamps=FALSE codecName=h2641080p60vdec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=1080P_60 sync=false
MPEG-2 -> NTSC_D1:
gst-launch filesrc location=sample_D1.m2v ! TIViddec2 engineName=codecServer codecName=mpeg2dec ! TIDmaiVideoSink videoStd=D1_NTSC videoOutput=COMPONENT sync=FALSE
MPEG-2 -> NTSC_720P:
gst-launch filesrc location=sample_720p.m2v ! TIViddec2 engineName=codecServer codecName=mpeg2dec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=720P_60 videoOutput=component sync=false hideOSD=TRUE
MPEG-2 -> NTSC_1080I30:
gst-launch filesrc use-mmap=true blocksize=40960 location=sample_1080i_30.m2v ! queue max-size-buffers=0 max-size-time=0 max-size-bytes=2097152 ! TIViddec2 genTimeStamps=FALSE engineName=codecServer codecName=mpeg2dec ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=1080I_30
Decode Audio Files
AAC:
gst-launch -v filesrc location=sample.aac ! TIAuddec1 codecName=aachedec engineName=codecServer ! alsasink sync=false
Decode Container Files
AVI (MPEG-2 / MP3) -> NTSC_1080I30:
gst-launch -v filesrc location=sample_1080i.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=1080I_30
MP4 (H.264 / AAC) -> NTSC_1080I30:
gst-launch -v filesrc location=sample_1080i.mp4 ! qtdemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! TIAuddec1 ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=1080I_30
TS (H.264 / MP3) -> NTSC_1080I30:
gst-launch -v filesrc location=sample_1080i.ts ! typefind ! mpegtsdemux name=demux demux. ! audio/mpeg ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! typefind ! mad ! alsasink demux. ! video/x-h264 ! typefind ! TIViddec2 TIDmaiVideoSink videoStd=1080I_30
Encode Video Files
Generated_D1 (videotestsrc) -> H.264:
gst-launch -v videotestsrc num-buffers=1000 ! video/x-raw-yuv,format=(fourcc)NV12 ! TIVidenc1 codecName=h264enc engineName=codecServer ! filesink location=output_gen_D1.264
Captured_720P (v4l2src) -> H.264:
gst-launch -v v4l2src always-copy=FALSE num-buffers=1000 ! TIVidenc1 codecName=h264enc engineName=codecServer contiguousInputFrame=TRUE ! filesink location=output_cap_720p.264
Encode Video in Container
Generated_D1 (videotestsrc) -> H.264 -> Quicktime container:
gst-launch -v videotestsrc num-buffers=2000 ! 'video/x-raw-yuv,format=(fourcc)NV12' ! TIVidenc1 codecName=h264enc engineName=codecServer byteStream=FALSE ! qtmux ! filesink location=output_gen_.mp4
Captured_720P (v4l2src) -> H.264 -> Quicktime container:
gst-launch -v v4l2src always-copy=FALSE num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=codecServer ! qtmux ! filesink location=output_cap_.mp4
Encode Audio Files
There's no AAC encoder included in DVSDK 3.10 due to licensing restrictions.
Resize
Captured_D1 (v4l2src) -> CIF:
gst-launch v4l2src always-copy=FALSE ! TIVidResize contiguousInputFrame=TRUE ! video/x-raw-yuv,width=352,height=288,format=(fourcc)Y8C8 ! TIDmaiVideoSink
Network Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
H.264 Encode/Stream/Decode:
A simple RTP server to be run on EVM.
gst-launch -v v4l2src always-copy=FALSE ! TIVidenc1 codecName=h264enc engineName=encode contiguousInputFrame=TRUE ! rtph264pay pt=96 ! udpsink host=<HOST_PC_IP> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)42801f, sprop-parameter-sets=(string)\"Z0KAH/QFoeiA\\,aN48gA\\=\\=\", payload=(int)96, ssrc=(guint)521259813, clock-base=(guint)1231006457, seqnum-base=(guint)2761
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to be run on Host PC (Linux).
gst-launch-0.10 -v udpsrc port=5000 caps="<CAP_FROM_SERVER>" ! rtph264depay ! ffdec_h264 ! xvimagesink
OMAP35x
This section covers pipelines for common use cases for the OMAP3530 processor.
Environment Requirements
Before executing the pipeline you need to set couple of environment variables, load kernel modules and activate video planes as follows:
cd /opt/gstreamer_demo/omap3530/
./loadmodules.sh
export GST_REGISTRY=/tmp/gst_registry.bin
export LD_LIBRARY_PATH=/opt/gstreamer/lib
export GST_PLUGIN_PATH=/opt/gstreamer/lib/gstreamer-0.10
export PATH=/opt/gstreamer/bin:$PATH
cat /dev/zero > /dev/fb2 2> /dev/null
The above command assumes that gstreamer is installed in /opt/gstreamer directory.
If you are using Angstrom distribution on beagleboard then you can use "omapdmaifbsink" instead of "TIDmaiVideoSink" to display the video inside the X windowing system.
Loopback: Video
gst-launch -v videotestsrc ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD accelFrameCopy=FALSE sync=false
Loopback: Audio
gst-launch audiotestsrc freq=1000 num-buffers=100 ! alsasink
If you want to route audio in to audio out (your very own P.A. system), try:
gst-launch alsasrc num-buffers=1000 ! alsasink
If you get a Could not open audio device for recording. error, likely your ALSA configuration is incorrect. I fixed it with
mv /etc/asound.conf /etc/asound.conf.orig
to move the ALSA configuration file out of the way.
Loopback: Audio+Video
No pipelines here yet. Please feel free to add your own.
Decode Video files
H.264/VGA:
gst-launch -v filesrc location=sample.264 ! TIViddec2 codecName=h264dec engineName=codecServer ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD sync=false
MPEG-4/VGA:
gst-launch -v filesrc location=sample.m4v ! TIViddec2 codecName=mpeg4dec engineName=codecServer ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD sync=false
MPEG-2/VGA:
gst-launch -v filesrc location=sample.m2v ! TIViddec2 codecName=mpeg2dec engineName=codecServer ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD sync=false
Decode Audio Files
AAC:
gst-launch -v filesrc location=sample.aac ! TIAuddec1 codecName=aachedec engineName=codecServer ! alsasink sync=false
Decode .MP4 Files
The following pipeline assumes you have a VGA .MP4 file with H.264 Video and AAC Audio.
gst-launch -v filesrc location=sample.mp4 ! qtdemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! TIAuddec1 ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD
Decode .AVI Files
The following pipeline assumes you have VGA .AVI file with MPEG-2 or MPEG-4 Video and MP1L2 or MP3 Audio.
gst-launch -v filesrc location=sample.avi ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! mad ! alsasink demux.video_00 ! queue ! TIViddec2 ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD
Decode .TS Files
The following pipeline assumes you have VGA .TS file with H.264 Video and MP1L2 or MP3 Audio.
gst-launch filesrc location=sample.ts ! typefind ! mpegtsdemux name=demux demux. ! queue max-size-buffers=1200 max-size-time=0 max-size-bytes=0 ! typefind ! mad ! alsasink demux. ! typefind ! TIViddec2 ! queue max-size-buffers=2 max-size-time=0 max-size-bytes=0 ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD
Encode Video Files
H.264/QVGA:
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=codecServer ! filesink location=sample.264
MPEG-4/QVGA:
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=mpeg4enc engineName=codecServer ! filesink location=sample.m4v
Encode Video in Container
Encode H.264 in quicktime container (Capture):
gst-launch -v videotestsrc num-buffers=2000 ! TIVidenc1 codecName=h264enc engineName=codecServer byteStream=FALSE ! qtmux ! filesink location=sample.mp4
Image Encode
A simple pipeline to encode YUV420P image
gst-launch filesrc location=sample.yuv ! TIImgenc1 resolution=720x480 iColorSpace=UYVY oColorSpace=YUV420P qValue=75 ! filesink location=sample.jpeg
Image Decode
A simple pipeline that converts a JPEG image into UYVY format.
gst-launch filesrc location=sample.jpeg ! TIImgdec1 codecName=jpegdec engineName=codecServer ! filesink location=sample.uyvy
Resize
A simple pipeline receiving CIF from videotestsrc and resizing to VGA.
gst-launch videotestsrc ! 'video/x-raw-yuv,width=352,height=288' ! TIVidResize ! 'video/x-raw-yuv,width=640,height=480' ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD sync=false
Network Streaming
Audio RTP Streaming
Although these examples are using a target device and a host PC, you could use two target devices as well.
Case 1: sending audio from target (BeagleBoard in my case) to Ubuntu host:
On target:
gst-launch audiotestsrc freq=1000 ! mulawenc ! rtppcmupay ! udpsink host=<HOST_PC_IP> port=5555
On host:
gst-launch udpsrc port=5555 caps="application/x-rtp" ! queue ! rtppcmudepay ! mulawdec ! audioconvert ! alsasink
The above example experienced dropped audio, please update pipeline when you get it working properly.
Case 2: sending audio from Ubuntu host to target (BeagleBoard)
On host:
gst-launch audiotestsrc freq=1000 ! mulawenc ! rtppcmupay ! udpsink host=<TARGET_PC_IP> port=5555
On target
gst-launch udpsrc port=5555 caps="application/x-rtp" ! queue ! rtppcmudepay ! mulawdec ! audioconvert ! alsasink
H.264 RTP Streaming
This section gives example where EVM acts as streaming server, which captures, encodes and transmit via udp. Host PC can be used as client to decode.
H.264 Encode/Stream/Decode A simple RTP server to encode and transmit H.264.
gst-launch -v videotestsrc ! TIVidenc1 codecName=h264enc engineName=codecServer ! rtph264pay pt=96 ! udpsink host=<HOST_PC_IP> port=5000
When the pipeline starts to run, you'll see something that looks like this:
/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, profile-level-id=(string)42801e, sprop-parameter-sets=(string)\"Z0KAHukCg+QgAAB9AAAdTACA\\,aM48gA\\=\\=\", payload=(int)96, ssrc=(guint)3417130276, clock-base=(guint)2297521617, seqnum-base=(guint)48503
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to decodes H.264 and display on HOST machine
gst-launch -v udpsrc port=5000 caps="<CAPS_FROM_SERVER>" ! rtph264depay ! ffdec_h264 ! xvimagesink
MPEG-4 Receive/Decode/Display:
This section gives example where EVM acts as RTP client, which receives encoded stream via udp then decodes and display output. Host PC can be used as server to transmit encoded stream.
A simple RTP server which encodes and transmits MPEG-4 on OMAP3530 EVM.
gst-launch-0.10 videotestsrc ! 'video/x-raw-yuv,width=640,height=480' ! ffenc_mpeg4 ! rtpmp4vpay ! udpsink host=<EVM_IP_ADDR> port=5000 -v
Make a note of caps="application/x-rtp, media=(string)video ................" string and pass this string in client below
A simple RTP client to receive and decode the MPEG-4 encoded stream.
gst-launch -v udpsrc port=5000 caps="<CAPS_FROM_SERVER>" ! rtpmp4vdepay ! TIViddec2 ! TIDmaiVideoSink videoStd=VGA videoOutput=LCD sync=false
All
This section covers pipelines that should work for all processors. These pipelines should work on any other platform too (such as your desktop Linux machine). They are included because we have been asked for these examples previously.
Debugging
Verbose output
If you want to see what capabilities are being used or are expected, add -v.
gst-launch -v alsasrc ! alsasink
Element debug output
To enable debug output for a specific element:
gst-launch --gst-debug=audiotestsrc:4 audiotestsrc ! alsasink
Adjust the element name and debug level until you get the data you are looking for.
To enable debug output for a more than one element:
gst-launch --gst-debug=audio*:3 audiotestsrc ! audioconvert ! alsasink
or for all elements
gst-launch --gst-debug=*:3 alsasrc ! alsasink
You can see the list of element names that support debug output using
gst-launch --gst-debug-help
Audio pipelines
Controlling the sample rate and bit depth
Find the default audio capabilities:
gst-launch -v alsasrc ! alsasink
The output will be similar to
caps = audio/x-raw-int, endianness=(int)1234, signed=(boolean)true, width=(int)32, depth=(int)32, rate=(int)44100, channels=(int)2
Using that pattern (minus the data type indication, which is not needed with gst-launch):
gst-launch -v alsasrc ! audio/x-raw-int, endianness=1234, signed=true, width=32, depth=32, rate=44100, channels=2 ! alsasink
Adjust the capabilities as needed.
Generic network audio streaming example
These pipelines do not depend on the TI DMAI GSteamer plug-in.
Sender (host):
TARGET_IP=10.111.0.194 gst-launch audiotestsrc freq=1000 ! mulawenc ! rtppcmupay ! queue ! udpsink host=$TARGET_IP port=5555
Receiver (target):
gst-launch udpsrc port=5555 caps="application/x-rtp" ! queue ! rtppcmudepay ! mulawdec ! alsasinkLeave a Comment