Find Source of Code Size Increase

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Problem Statement

You are compiling your code with two different options sets, or two different compiler versions, and you want to find the functions which have the largest code size increase between the builds.

Presumptions

Collect Code Size Data

Collect code size data by using the --func_info option of the Object File Display (OFD) utility. OFD is described in the Assembly Language Tools Guide for your device family. The executable is named something like ofd6x, ofd55, or ofd470. Only fairly recent versions of OFD support the --func_info option.

Target Version
C6000 v6.1.0
ARM v4.5.0
C5500 v4.2.0
MSP430 v3.0.0
C2000 v5.1.0

Note, however, that since OFD is a purely diagnostic tool, it is OK to use a newer OFD on code built with an older compiler. The topic Compiler Releases tells you where to get compiler updates.

So, to collect code size data on your two builds ...

% ofd55 --func_info file1.out > size_data1.csv
% ofd55 --func_info file2.out > size_data2.csv

View Code Size Data with Excel

The output from using --func_info is in CSV format. CSV stands for comma separated values. It is a very simple format. For example ...

C:\dir>ofd6x --func_info file.out | more
"HOSTclose","SHARED/trgdrv.c",0x00004ee0,0x00004f7c,156
"HOSTlseek","SHARED/trgdrv.c",0x000042a0,0x00004374,212
...

Each row represents data for one function. The data is separated by commas. The data on one row is: function name, file name, starting address, ending address, size.

The details of the format don't matter much in this article. Just let Excel deal with that. On a typically configured Windows system, you can "execute" a .csv file to bring it up in Excel ...

% size_data1.csv

Compare Code Size Data with Excel

  1. Bring up both .csv files in Excel
  2. Delete the file name, starting address, and ending address columns
  3. Sort both files by function name
  4. Copy the columns from one file into the other
  5. Put the name columns next to each other and visually inspect one last time to make sure they are exactly the same
  6. Delete one name column
  7. Add a formula to subtract the two size columns, called the delta
  8. Sort by the delta

The functions with the largest delta are now at the top of the spreadsheet. Here is an example, with column headings added for clarity.

Codesize compare.jpg

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox