Flash configuration in the Kernel
From Texas Instruments Embedded Processors Wiki
Contents |
Introduction
What is the MTD Subsystem
The Memory Technology Devices (MTD) subsystem allows for support for a wide variety of Flash devices. It abstracts the details of the device interaction and provides an interface for communication with Flash devices. The details of how to actually communicate with the Flash device are left to individual device drivers which conform to the MTD API. This enables users to program their Flash chips without worrying about the specifics of how to communicate with the Flash device.
Flash Types supported
In the TI DaVinci kernel there are MTD compatible drivers that allow the user to interact with NOR Flash (both AMD and Intel) as well as NAND flash. Not all EVMs have both types of Flash. For example the DM644x has both NOR and NAND Flash, whereas the DM355 has only NAND Flash. For details about the Flash devices on your EVM please refer to the Technical Reference documentation for your EVM.
Enabling NOR Support
This section covers enabling NOR Flash support in the MontaVista TI DaVinci kernel. For open source git kernel see NOR configuration.
For devices such as the DM644x EVM the NOR Flash may be an AMD or Intel chip depending on the hardware revision of your EVM.
You can use the flinfo command from the u-boot prompt to determine your Flash type. For AMD chips you should see output similar to the following:
dvevm# flinfo Bank # 1: MY AMD 29LV256M (256 Mbit)
AMD NOR Chip
To enable support in the kernel for AMD NOR chips you must enable:
- MTD support
- DaVinci NOR Flash (AMD Flash)
- AMD compatible flash chip support (non-CFI)
For example to enable MTD support you should have the following selected in "Memory Technology Devices (MTD)" when running xconfig
To enable AMD Flash support you should have the following selected in the "RAM/ROM/Flash chip drivers" section of the "Memory Technology Devices (MTD)" section
Intel NOR Chip
To enable support in the kernel for Intel NOR chips you must enable:
- MTD support
- DaVinci NOR Flash (Intel Flash)
- Support for Intel/Sharp flash chips
For example to enable MTD support you should have the following selected in "Memory Technology Devices (MTD)" when running xconfig
To enable Intel Flash support you should have the following selected in the "RAM/ROM/Flash chip drivers" section of the "Memory Technology Devices (MTD)" section
Enabling NAND Support
For open source git kernel see NAND configuration. To enable support in the MontaVista TI kernel for NAND Flash you must enable:
- MTD support
- NAND Device Support
- NAND Flash device on DaVinci SoC
For example to enable MTD support you should have the following selected in "Memory Technology Devices (MTD)" when running xconfig
To enable NAND Flash support you should have the following selected in the "NAND Flash Device Drivers" section of the "Memory Technology Devices (MTD)" section
Conclusion
You should now have a kernel with Flash support enabled. You can now compile this kernel and use it to access your Flash devices. For more information on compiling the kernel please refer to the Building a New Linux Kernel section of the Getting Started Guide for you product.
Leave a Comment