GEL Launcher
From Texas Instruments Embedded Processors Wiki
Contents |
About GEL Launcher
The GEL Launcher is a CCStudio plug-in toolbar that allows you to launch custom GEL functions with the press of a button.
NOTE: This plug-in is not an 'official' product, thus it is unsupported (i.e. - use at your own risk).
Installation
For CCStudio v3.x
To install the GEL Launcher plug-in:
- Download and execute GEL_Launcher-1.0-Setup.exe
- Install GEL Launcher in the root CCStudio installation directory (ex. C:\CCStudio_v3.3)
- Launch CCStudio. It will inform you that new plugins have been dectected and asks if you wish to enable them. Select 'YES'
- The GEL Launcher plug-in is now available for use. The GEL Launcher Toolbar with 5 configurable buttons will appear in the upper left side of the CCStudio IDE:
Uninstallation: Control Panel->Add or Remove Programs->GEL Launcher
For CCStudio v4
Download the GEL Launcher Toolbar for CCStudio v4. Copy the jar file into <Install dir>\Eclipse\plugins.
Usage
To associate a button in the GEL Launcher Toolbar with a GEL action, simply define a GEL function called 'GEL_ToolbarN()' where 'N' is the button number you wish to associate with the function.
Example:
// mygelfile.gel
GEL_Toolbar1()
{
// enter GEL expressions to be performed when button 1 is pressed
}
GEL_Toolbar2()
{
// enter GEL expressions to be performed when button 2 is pressed
}
etc...
Hovering your mouse pointer over a button will bring up a tooltip that will state the name of the GEL function that button will call when pressed (The prior screenshot in the Installation section shows a tooltip for button 1 with shows that it will call GEL_Toolbar1() ).
Leave a Comment