GSG: OMAP35x DVEVM Additional Procedures

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

^ Up to main OMAP35x DVEVM Getting Started Guide Table of Contents

Contents


Updating/Restoring the Flash Image (From DVSDK version 3.01.00.01)

GSG:_AM35x_EVM_Additional_Procedures#Updating.2FRestoring_the_Flash_Image

Updating/Restoring the Flash Image

This section describes how to install software images onto the flash memory on the EVM. This procedure can be used to install an updated version of the software from TI, to install a customized version built by the customer or to restore the flash image if it is destroyed or damaged. This procedure will work even if the flash is completely erased.

Requirements

Preparing to Install

If the EVM has an active u-boot, please disable it from booting the kernel by following the steps given below.

  1. Ensure that the host PC is connected to the board via UART as mentioned in Section UART1
  2. Power On the board. Once you power on the board, the following will be printed on the hyperterminal or teraterm.
    Texas Instruments X-Loader 1.41
    Detected Samsung MuxOneNAND1G Flash
    Starting OS Bootloader...
    U-Boot 1.1.4 (Jun 5 2008 - 17:53:37)
    OMAP3-GP rev 2, CPU-OPP2 L3-165MHz
    OMAP3EVM 1.0 Version + mPOP (Boot ONND)
    DRAM: 128 MB
    OneNAND Manufacturer: Samsung (0xec)
    Muxed OneNAND 128MB 1.8V 16-bit (0x30)
    OneNAND version = 0x0221
    Scanning device for bad blocks
    num of blocks = 2048
    In: serial
    Out: serial
    Err: serial
    Resetting CHIP... Done
    LAN9x18 (0x01150002) detected.
    Setting mac address: 00:50:c2:7e:85:66
    start Auto negotiation... (take ~2sec)
    Auto negotiation complete, 100BaseTX, full duplex
    
  3. Stop the boot process by pressing the Enter key on the development PC keyboard. The u-boot prompt will appear.
  4. Disable the u-boot from booting the kernel by using the following commands at the u-boot prompt.
    OMAP3EVM # setenv bootcmd echo no boot command configured
    OMAP3EVM # setenv bootdelay 99
    OMAP3EVM # saveenv
    

    NOTE: Make sure you follow this step. The download will not work and button S2 on the EVM will not operate if the Linux kernel begins to boot.

Downloading U-boot via the UART Downloader

  1. Turn off the EVM by unplugging the power adapter.
  2. Close any open terminal programs.
  3. Move the serial port cable to UART3.
  4. Ensure SW4 is set as described in Section Main Board SW4
  5. Start the DownloadUtility.exe program in AM35x-OMAP35x-PSP-SDK-##.##.##.##/host-tools/windows/utilities
  6. Select the correct COM port
  7. Press the “open” button and select the following file:
    • AM35x-OMAP35x-PSP-SDK-##.##.##.##/images/omap3530/u-boot/u-boot.bin
  8. Press the Download button, Press OK on the dialog that say “Press OK and reset the target”
  9. Power on the EVM
  10. If the download does not immediately start, Press S2 on the EVM
  11. The download utility (DownloadUtility.exe) should show progress and eventually will show “Main Image has been sent”
  12. Close Download Utility (DownloadUtility.exe) and restart your terminal program. Do not power cycle the EVM.
  13. Move the serial cable to UART1 and press enter to get a U-boot prompt
    OMAP3530 EVM GSG Additional information 01.JPG
    OMAP3530 EVM GSG Additional information 02.JPG

    NOTE: If you do not get the uboot prompt on pressing "Enter" after connecting the serial port cable to UART1, check if you have followed all the above steps properly. If the problem persists, your NAND could be corrupted. In the event of NAND corruption, perform SD/MMC card boot using the steps mentioned in OMAP35x_DVEVM_Boot_from_SD/MMC_card and erase the NAND using the following command

    For Micron NAND, 
    OMAP3EVM# nand erase
    For Samsung OneNAND, 
    OMAP3EVM# onenand erase

Using U-boot to Update the Flash Memory

Now that U-boot is running on the target, you can use it to update any or all of the software in flash. The steps provided here will use the Ethernet connection with the TFTP protocol to transfer the files.

Setup the TFTP Server

This section will describe setting up the TFTP server using a Windows host. You may also use a Linux TFTP server but that process is not described here.

The OMAP35x SDK comes with the PumpKIN TFTP server. This program is easy to setup and can be started and stopped easily.

To setup PumpKIN follow these steps:

  1. Start the PumpKIN executable. The first time it is started it should show a Window. Subsequent starts may only show in the system tray. You may open the window from the right click menu of the system tray icon.
  2. Hit the Options button and configure the path to the base of the SDK directory structure.
  3. Select “Allow Access to sub-directories” and “Give all files”
  4. Hit OK
OMAP3530 EVM GSG Additional information 03.JPG
OMAP3530 EVM GSG Additional information 04.JPG
OMAP3530 EVM GSG Additional information 05.JPG

Running the Re-flash Procedure

  1. Ensure that the terminal program is configured with ~ 100 ms of delay after sending each line as described in Section Setup Terminal Program
  2. Ensure the environment is set as appropriate for your EVM and network setup
    OMAP3EVM # setenv ethaddr   00:50:c2:XX:XX:XX	(see sticker on EVM)
    OMAP3EVM # setenv ipaddr    192.168.1.10		(as appropriate)
    OMAP3EVM # setenv serverip  192.168.1.100		(PumpKIN PC’s addr)
    OMAP3EVM # setenv netmask   255.255.255.0		(as appropriate)
    OMAP3EVM # setenv gatewayip 192.168.1.1		(if needed)
    OMAP3EVM # nand unlock					(ONLY MICRON!)
    OMAP3EVM # saveenv
  3. The windows IP address can be obtained using the following steps
    1. Go to Start->Run
    2. Type cmd to open the command window
    3. Type ipconfig on command prompt to get the IP address of the Windows host PC
  4. Check the IP settings
    OMAP3EVM # ping $(serverip)				(expect “x.x.x.x is alive”)
  5. Use the terminal program to send the text file reflash.txt file to the EVM
    1. Make sure you know if your board has Samsung or Micron memory parts
    2. path: AM35x-OMAP35x-PSP-SDK-##.##.##.##/scripts/omap3530
      • reflash-micron.txt (for Micron memory boards)
      • reflash-samsung.txt (for Samsung memory boards)
      Note:The scripts are saved in Unix format.If you want to run from windows please convert it to dos format using unix2dos command in the scripts directory.Usage as given below:
      unix2dos *
    3. If you need to use these scripts for re-flashing the demos that come along with the OMAP3530 DVSDK, the following changes are required to be modified in the re-flash scripts. The changes are marked in bold. The example is shown for only reflash-samsung.txt. Performing similar changes for reflash-micron.txt is needed if Micron-NAND OMAP35x EVM is being used.
      setenv rf_unlock      onenand unlock 0x0 0x8000000
      setenv rf_blank_ram   mw.b 0x81600000 0xff 0x1400000
      setenv rf_er_xloader  onenand erase block 0-3
      setenv rf_er_uboot    onenand erase block 4-18
      setenv rf_er_env      onenand erase block 19-19
      setenv rf_er_kernel   onenand erase block 20-59
      setenv rf_er_ramdisk  onenand erase block 60-1023
      setenv rf_er_fs       onenand erase block 60-1023
      setenv rf_get_xloader tftpboot 0x81600000 images/boot-strap/x-load.bin.ift
      setenv rf_get_uboot   tftpboot 0x81600000 images/u-boot/u-boot.bin
      setenv rf_get_kernel  tftpboot 0x81600000 images/kernel/uImage
      setenv rf_get_ramdisk tftpboot 0x81600000 images/fs/ramdisk.gz
      setenv rf_get_min_rd  tftpboot 0x81600000 images/fs/ramdisk-base.gz
      setenv rf_get_fs      tftpboot 0x81600000 images/fs/rootfs.jffs2
      setenv rf_wr_xloader  onenand write 0x81600000 0x000000 0x0020000
      setenv rf_wr_uboot    onenand write 0x81600000 0x080000 0x0040000
      setenv rf_wr_kernel   onenand write 0x81600000 0x280000 0x0220000
      setenv rf_wr_ramdisk  onenand write 0x81600000 0x780000 0x1000000
      setenv rf_wr_fs       onenand write 0x81600000 0x780000 0x1400000
      setenv rf_ev          run rf_unlock\; run rf_er_env
      setenv rf_xl          run rf_unlock\; run rf_blank_ram\; run rf_er_xloader\; run rf_get_xloader\; run rf_wr_xloader
      setenv rf_ub          run rf_unlock\; run rf_blank_ram\; run rf_er_uboot\; run rf_get_uboot\; run rf_wr_uboot
      setenv rf_kn          run rf_unlock\; run rf_blank_ram\; run rf_er_kernel\; run rf_get_kernel\; run rf_wr_kernel
      setenv rf_rd          run rf_unlock\; run rf_blank_ram\; run rf_er_ramdisk\; run rf_get_ramdisk\; run rf_wr_ramdisk
      setenv rf_min_rd      run rf_unlock\; run rf_blank_ram\; run rf_er_ramdisk\; run rf_get_min_rd\; run rf_wr_ramdisk
      setenv rf_fs          run rf_unlock\; run rf_blank_ram\; run rf_er_fs\; run rf_get_fs\; run rf_wr_fs
      setenv rf_all_rd      run rf_xl\; run rf_ub\; run rf_kn\; run rf_rd
      setenv rf_all_min_rd  run rf_xl\; run rf_ub\; run rf_kn\; run rf_min_rd
      setenv rf_all_fs      run rf_xl\; run rf_ub\; run rf_kn\; run rf_fs
      printenv
      echo done 
      echo Make sure to set MAC address
      

      If you need to re-flash the target file systems that contains the demos that come along with the OMAP3530 DVSDK, or your own target file systems, refer section Flashing the Pre-built/rebuilt NAND Flash File System

    4. For HyperTerm use Transfer / Send Text File …
    5. For TeraTerm use File / Send file …
    6. For minicom use the paste file command (Ctrl-A Y)
  6. Run the reflash command sequence
    OMAP3EVM # run rf_all_fs (for jffs file-system)
    OMAP3EVM # run rf_all_rd (for ramdisk)

    (Individual components can be reflashed by using commands like rf_ub, rf_kn, etc)

    Note: For reflashing choices for Micron nand please select the commands which are marked by _new.(For example 'rf_all_fs_new' for using JFFS filesystem and 'rf_all_rd_new' for using full ramdisk).

    Note: Ramdisk should be used for Micron boards as JFFS produces warnings and very long boot times.

    Note: If the flashed rootfs.jffs2 or the NFS setup uses the target file system which is present in the CD , or uses the NFS setup, which has demos that have dependency on the CMEM module, then the bootargs within the initenv-xxx.txt scripts need to be modified as follows. The changes are reflected in bold.

    The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

    setenv bootargs_rd     mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

    setenv bootargs_rd     mem=100M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_fs     mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y 
    setenv bootargs_nfs    mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK release 3.00.02.44 is as given below

    setenv bootargs_rd     mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y 

    The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

    setenv bootargs_rd     mem=88M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_fs     mem=88M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
    setenv bootargs_nfs    mem=88M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y 

    If the script is not used, use the above appropriate command (depending on ramdisk, NAND flash or NFS file system) to set the bootargs by using the following command

    For Ramdisk:
    setenv bootargs ‘bootargs_rd’
    For NFS:
    setenv bootargs ‘bootargs_nfs’
    For NAND Flash:
    setenv bootargs ‘bootargs_fs’

    Even if the script is not being used, it is important to set the bootargs in u-boot params to use mem=88M (in case of DVSDK releases from v3.00.00.33 to 3.00.01.42),mem=99M (in case of DVSDK release 3.00.02.44 onwards), mem=100M (in case of DVSDK v3.01 release) or the appropriate value that is equal to the (size of DDR used in OMAP35x EVM – size allocated for CMEM).

  7. Reset the board Note: The current U-boot only allows 40 environment variables. Do not saveenv after the reflash script has been submitted. Instead complete the reflash and reboot before making env changes.
  8. Use the terminal program to send the text file initenv.txt to the EVM
    1. path: AM35x-OMAP35x-PSP-SDK-##.##.##.##/scripts/omap3530/…
    • initenv-micron.txt (for Micron memory boards)
    • initenv-samsung.txt (for Samsung memory boards)
  9. Save the environment
    OMAP3EVM # nand unlock					(ONLY MICRON!)
    OMAP3EVM # saveenv
    
  10. Reset the board and it should boot into the kernel and file-system

Using Telnet

The initialization file (/etc/init.d/rcS) starts a telnet server. If your development host is in the same sub-net as the EVM, you can telnet to it using the IP address assigned in the U-boot environment.  The following is an example from a Linux host.

$ telnet 192.168.1.10

You will be prompted for a user name and password. The user name should be root and the password should be left blank (just hit Enter).


From a Windows XP host, click the Start button, then click Run... Type telnet and click OK. This will open a telnet window.

Type "o < ip-addr >" and hit enter.  Example:

Microsoft Telnet> o 128.247.107.12 

Type root for the password and leave the password blank (just hit Enter)

Booting the New Linux Kernel

After building the new kernel, in order to use it to boot the OMAP35x EVM, you must transfer it to the board via TFTP. Once you transfer the kernel image to the board via TFTP, you could either perform a TFTP kernel boot or flash the kernel image to the NAND and subsequently use the NAND boot. It is assumed you have completed the steps under Rebuilding the Linux Kernel, and the boot file, uImage has been copied to /tftpboot (or some other site-specific TFTP accessible location).

Checking the TFTP server setup in the Linux development PC

You can check to see if a TFTP server is set up with this command

# rpm -q tftp-server
    If it is not set up, you can follow these steps:
  1. To install TFTP, use this command, where -#.#-# is the version number portion of the filename:
    # rpm -ivh /db/ztree/useracct/tftp-server-#.#-#.rpm
  2. Confirm that TFTP is installed with this command:
    # /sbin/chkconfig --list | grep tftp

    You should see the following output:

    tftp: off

    If you need to turn on the TFTP server, use this command:

    # /sbin/chkconfig tftp on

    The default root location for servicing TFTP files is /tftpboot.

Using TFTP to boot the New Linux Kernel

  1. Power on the EVM board, and abort the automatic boot sequence by pressing the “Enter key” in the console window.
  2. Set the following environment variables to ensure that you are starting from a default, clean U-Boot environment.
    OMAP3EVM # setenv serverip <tftp server ip address>
    OMAP3EVM # setenv bootfile uImage

    The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

    setenv bootargs mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

    setenv bootargs mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK release 3.00.02.44 is as given below

    OMAP3EVM # setenv bootargs mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

    The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

    OMAP3EVM # setenv bootargs mem=88M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
    OMAP3EVM # setenv bootcmd ‘tftpboot 0x80000000 uImage;bootm’

    This configuration boots a new Linux kernel via TFTP with a NAND flash based file system

  3. The initenv-samsung.txt and initenv-micron scripts provide the options for setting the bootargs for the appropriate target file system that is being used for the boot. Kindly refer to the appropriate script files for the flash parts that is being used on the board for more details. In case of use of ramdisk file system use the following commands:
    The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below
    setenv bootargs mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

    setenv bootargs mem=100M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK release 3.00.02.44 is as given below

    OMAP3EVM # setenv bootargs mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M mpurate=600 ramdisk_size=40960 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

    The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

    OMAP3EVM # setenv bootargs mem=88M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

    You could use TFTP to transfer the ramdisk image from the development PC or flash it on the NAND flash. Refer section 5.4.2, Running the Re-flash Procedure for more details on flashing the file systems on the target

    NOTE: Currently there is no full ramdisk image that includes OMAP3530 DVSDK demonstrations.

    In case of use of NFS, use the following commands:

    The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

    setenv bootargs mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y

    The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

    setenv bootargs mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y
    

    The bootargs for DVSDK release 3.00.02.44 is as given below

    OMAP3EVM # setenv bootargs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs  nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

    The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

    OMAP3EVM # setenv bootargs    mem=88M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs  nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

Flashing the New Linux Kernel

The Linux kernel can also be flashed on the NAND and then could be used for the boot. Perform the following steps for flashing the new or rebuilt Linux Kernel

  1. Make sure that the environment variables are properly set
    OMAP3EVM # setenv serverip <tftp server ip address>
    OMAP3EVM # setenv bootfile uImage
    
  2. Flash the Kernel Image onto the Samsung NAND flash using the following commands.
    OMAP3EVM # mw.b 0x81600000 0xff 0x1400000
    OMAP3EVM # onenand erase block 20-59
    OMAP3EVM # tftpboot 0x81600000 uImage
    OMAP3EVM # onenand write 0x81600000 0x280000 0x0300000
    
  3. Flash the Kernel Image onto the Micron NAND flash using the following commands.
    OMAP3EVM # nand unlock
    OMAP3EVM # mw.b 0x81600000 0xff 0x1400000
    OMAP3EVM # nand erase 280000 300000
    OMAP3EVM # tftpboot 0x81600000 uImage
    OMAP3EVM # nandecc sw
    OMAP3EVM # nand write.i 0x81600000 280000 300000
    
  4. Once the image is flashed, refer to Booting From Flash using Board’s NAND Flash File System or Booting from Flash Using NFS File System for booting using the kernel image in NAND flash.

Flashing the Pre-built/rebuilt NAND Flash File System

Perform the following steps to program the flash for pre-built or a rebuilt NAND flash file system. The pre-built NAND flash file system (rootfs.jffs2) for OMAP3530 DVSDK is available under /home/<useracct>/dvsdk/dvsdk_#_##_##_##/targetfs folder. Copy it to the default location for servicing the tftp files on the host PC. (refer to section TFTP server setup on Linux PC or section Setup the TFTP Server)

  1. Make sure that the environment variables are properly set
    OMAP3EVM # setenv serverip <tftp server ip address>
    OMAP3EVM # setenv bootfile uImage
    
  2. Flash the NAND flash file system Image onto the Samsung NAND flash using the following commands.
    OMAP3EVM # mw.b 0x81600000 0xff 0x6000000
    OMAP3EVM # onenand erase block 60-1023
    OMAP3EVM # tftpboot 0x81600000 rootfs.jffs2
    OMAP3EVM # onenand write 0x81600000 0x780000 0x6000000
    
  3. Flash the NAND flash file system Image onto the Micron NAND flash using the following commands.
    OMAP3EVM # nand unlock
    OMAP3EVM # mw.b 0x81600000 0xff 0x6000000
    OMAP3EVM # nand erase 780000 6000000
    OMAP3EVM # tftpboot 0x81600000 rootfs.jffs2
    OMAP3EVM # nandecc sw
    OMAP3EVM # nand write.i 0x81600000 780000 6000000
    

    Once the image is flashed, refer to section Booting From Flash using Board’s NAND Flash File System or section Booting via TFTP Using Board’s NAND Flash File System for booting using the NAND flash file system

Changing Options in U-boot

If you use the environment provided by the initenv.txt script you have several choices for boot options. Most of the boilerplate has been provided; you just need to set your choices.

Note: Refer Section Running the Re-flash Procedure for modifications in the initenv.txt script files required to be able to run the dvsdk demos that comes OMAP3530 DVSDK. Also Refer Alternate Boot Methods

Kernel choices:

OMAP3EVM # setenv get_kernel run nand_kernel	(get kernel from flash)
OMAP3EVM # setenv get_kernel run tftp_kernel	(get custom kernel from TFTP)

Initrd choices:

OMAP3EVM # setenv get_initrd run nand_initrd	(get kernel from flash)
OMAP3EVM # setenv get_initrd run tftp_initrd	(get custom image from TFTP)

File-system choices:

OMAP3EVM # setenv bootcmd    run bootargs_rd      	(use an initrd ramdisk)
OMAP3EVM # setenv bootcmd    run bootargs_fs		(use a JFFS file-system in flash)
OMAP3EVM # setenv bootcmd    run bootargs_nfs		(use an NFS root directory)

Save your choices:

OMAP3EVM # nand unlock					(only MICRON!)
OMAP3EVM # saveenv					(save to flash)

To run a JFFS file-system or a ramdisk image from flash you need to make sure the appropriate image is in flash. You can use the reflash.txt script to load the appropriate image.

Re-flash choices:

OMAP3EVM # run rf_all_rd				(update all using full ramdisk)
OMAP3EVM # run rf_all_min_rd				(update all using minimal ramdisk)
OMAP3EVM # run rf_all_fs				(update all using JFFS image)
OMAP3EVM # run rf_rd					(update just the full ramdisk)
OMAP3EVM # run rf_min_rd				(update just the full ramdisk)
OMAP3EVM # run rf_fs					(update just the JFFS image)

Note 1: The two ramdisk images and JFFS are all mutually exclusive in Flash as they occupy the same partition. (Running ramdisk from tftp does not require flash space).

Note 2: The current U-boot only allows 40 environment variables. Do not saveenv after the reflash script has been submitted. Instead complete the reflash and reboot before making env changes.

Note 3: For reflashing choices for Micron nand please select the commands which are marked by _new.(For example 'rf_all_fs_new' for using JFFS filesystem and 'rf_all_rd_new' for using full ramdisk).

Alternate Boot Methods

Booting From Flash using Board’s NAND Flash File System

This is the default, out-of-the-box boot configuration Make sure that the kernel image and the JFFS2 root file system is flashed To boot in this mode, set the following parameters after you abort the automatic boot sequence:

For Micron NAND EVM:

 OMAP3EVM # setenv nand_kernel nand read.i 0x80000000 280000 300000 

For Samsung NAND EVM:

 OMAP3EVM # setenv nand_kernel onenand read 0x80000000 0x280000 0x0300000 

Set the following environment variables, irrespective of Micron NAND or Samsung NAND EVM:

OMAP3EVM # setenv get_kernel run nand_kernel
OMAP3EVM # setenv bootcmd ‘run get_kernel;bootm 0x80000000’

The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

OMAP3EVM # setenv bootargs mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2
           mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

OMAP3EVM # setenv bootargs mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2
                          mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK release 3.00.02.44 is as given below

OMAP3EVM # setenv bootargs mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600
                           omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
OMAP3EVM # boot

The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

OMAP3EVM # setenv bootargs mem=88M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 
                           omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

NOTE: All setenv commands should be entered on a single line. They are shown on multiple lines here for ease of reading.

Booting from Flash Using NFS File System

Make sure that the kernel image is flashed. To boot in this mode, set the following parameters after you abort the automatic boot sequence:

For Micron NAND EVM:

 OMAP3EVM # setenv nand_kernel nand read.i 0x80000000 280000 300000 

For Samsung NAND EVM:

 OMAP3EVM # setenv nand_kernel onenand read 0x80000000 0x280000 0x0300000 

Set the following environment variables, irrespective of Micron NAND sor Samsung NAND EVM:

OMAP3EVM # setenv get_kernel      run nand_kernel
OMAP3EVM # setenv bootcmd ‘run get_kernel;bootm 0x80000000’

The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

OMAP3EVM # setenv bootargs_nfs mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs
                           nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 
                           omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

OMAP3EVM # setenv bootargs_nfs mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs
                           nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 
                           omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK release 3.00.02.44 is as given below

OMAP3EVM # setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp  root=/dev/nfs nfsroot=<nfshost>:<rootpath>,nolock 
                           mem=99M mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

OMAP3EVM # setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp  root=/dev/nfs nfsroot=<nfshost>:<rootpath>,nolock 
                           mem=88M omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
OMAP3EVM # boot

NOTE: All setenv commands should be entered on a single line. They are shown on multiple lines here for ease of reading.

The <nfshost> shall be set to the ip address of the NFS host machine. The <rootpath> must match the filesystem that you set up on your workstation. For example, /home/<useracct>/workdir/filesys

Booting via TFTP Using Board’s NAND Flash File System

To boot in this mode, set the following parameters after you abort the automatic boot sequence:

NOTE: You can find a pre-build kernel image (uImage) in the OMAP35x-PSP-SDK-##.##.##.##/images/kernel directory.

Make sure to check the tftp server setup on the Linux development host (Refer Checking the TFTP server setup in the Linux development PC)

OMAP3EVM # setenv serverip <tftp server ip address>
OMAP3EVM # setenv bootfile  <kernel image>
OMAP3EVM # setenv bootcmd ‘tftpboot 0x80000000 uImage;bootm 0x80000000’ 

The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

setenv bootargs_fs     mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK release 3.00.02.44 is as given below

OMAP3EVM # setenv bootargs   mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp root=/dev/mtdblock4 rw rootfstype=jffs2 
                             mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

OMAP3EVM # setenv bootargs   mem=88M console=ttyS0,115200n8 noinitrd ip=dhcp root=/dev/mtdblock4 rw rootfstype=jffs2 
                             omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
OMAP3EVM # boot

NOTE: All setenv commands should be entered on a single line. They are shown on multiple lines here for ease of reading.

Booting via TFTP using NFS file system

To boot in this mode, set the following parameters after you abort the automatic boot sequence:

NOTE: You can find a pre-build kernel image (uImage) in the OMAP35x-PSP-SDK-##.##.##.##/images/kernel directory.

OMAP3EVM # setenv bootcmd 'dhcp;bootm'
OMAP3EVM # setenv serverip <ip addr of tftp server>
OMAP3EVM # setenv bootfile <name of kernel image>
OMAP3EVM # setenv rootpath <root directory to mount>
OMAP3EVM # setenv nfshost <ip addr of nfs host>

The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs
                       nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 
                       omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

setenv bootargs_nfs    mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs
                       nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 
                       omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.00.02.44 onwards are as given below

OMAP3EVM # setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp  root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock
                           mem=99M mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y

The bootargs for DVSDK releases from 3.00.00.36 up to and including 3.00.01.42 are as given below

OMAP3EVM # setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp  root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock
                           mem=88M omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
OMAP3EVM # boot

NOTE: All setenv commands should be entered on a single line. They are shown on multiple lines here for ease of reading.

The <root directory to mount> must match the file system that you set up on your workstation. For example, /home/<useracct>/workdir/filesys.

Working With 256MB Micron mDDR Memory

In case the EVM that you have has ES3.1 silicon and 256MB Micron memory part, and you wish to utilize the entire 256MB, the bootargs need to be changed to create a memory hole.

In case of DVSDK release 3.01.00.09, perform the following steps

Replace

insmod cmemk.ko phys_start=0x86300000 phys_end=0x87200000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 

with

insmod cmemk.ko phys_start=0x86300000 phys_end=0x87200000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 allowOverlap=1 


In case of DVSDK release 3.01.00.02, perform the following steps

Replace

insmod cmemk.ko phys_start=0x86400000 phys_end=0x87300000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 

with

insmod cmemk.ko phys_start=0x86400000 phys_end=0x87300000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 allowOverlap=1 


In case of DVSDK release 3.00.02.44, perform the following steps

Replace

insmod cmemk.ko phys_start=0x86300000 phys_end=0x87300000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 

with

insmod cmemk.ko phys_start=0x86300000 phys_end=0x87300000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 allowOverlap=1 


In case of DVSDK releases from 3.00.00.33 to 3.00.01.42, perform the following steps

Replace

insmod cmemk.ko phys_start=0x85800000 phys_end=0x86800000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440

with

insmod cmemk.ko phys_start=0x85800000 phys_end=0x86800000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440 allowOverlap=1


Putting Demo Applications in the Third-Party Menu

You can add your own demos to the Third-Party Menu by following the steps in this section. Only four demos can be shown at once in the user-interface. If you add more than four demos, the first four in alphabetical order are shown.

  1. Create the following files for your demo:
    • logo.jpg. This is the logo of the third party company which will be showed next to the demo description. The picture needs to be in JPEG format and of size 50x50.
    • readme.txt. This is a text file. The first 40 characters of the file should briefly describe the demo. The demo interface displays up to 40 characters, but stops if it encounters a new line character. For example, the file might contain "Video Phone demo" or "Network Audio demo".
    • app.sh. This is an executable that launches your demo. It can either be the demo executable itself or a shell script that executes the executable. (If this is a shell script, make sure its executable bit is set for all). A script could look something like:
    #!/bin/sh
    exec ./mydemoname
    • other files. If app.sh is a shell script, your demo executable will have some other name. You may also need to include data files or other files used by the executable.

    Note: The demo application must use relative paths to access any files it needs at runtime. This because the archive is extracted to another location from which the demo is executed.

  2. Create a gzipped tar file (ends with .tar.gz) that archives all the files in the previous list. For example, if your files are logo.jpg, readme.txt, and app.sh, you could use the following command:
    tar cvzf ti_videophone.tar.gz logo.jpg readme.txt app.sh

    Name the tar file using <company>_<demoname>.tar.gz (with no spaces in the file name) as the convention. For example, a video phone demo created by Texas Instruments would be named ti_videophone.tar.gz. The name must be unique since all demos are installed in the same directory.

    The three required files must be in the top-level directory of the archive. Other files may be in subdirectories, so long as the demo uses relative references to access them. For example, the following directory structure might be used in the archive:

    |-- app.sh
    |-- data
    |    |-- datafile1
    |    `-- datafile2
    |-- logo.jpg
    `-- readme.txt

    To check the format of the file you create, execute the following command in Linux. The result should say "gzip compressed data".

    file <filename>.tar.gz
  3. Put your archive in the "thirdpartydemos" subdirectory of the target installation directory. This is where the DVEVM software was installed on the target file system. The default target installation directory is /opt/dvsdk/omap3530, so the default location for demo archives is /opt/dvsdk/omap3530/thirdpartydemos. Do not extract the contents of the archive in this location. Extraction is performed behind-the-scenes each time the demo is run.

Changing the Output Display to DVI

The output display is set by default as LCD.You can change it to DVI either through Boot Mode Argument for the kernel or command line arguments once the kernel has booted.

Boot Mode Arguments for DVI

Please add the following commands to the bootargs 'omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"'

Please note that some versions of the EVM may require a hardware modification for DVI output to work. You can find information on the hardware modification required in the EVM Modifications for DVI-D output section.

The bootargs mentioned in section Running the Re-flash Procedure can be modified as below for running the pre-built Nand filesystem or NFS filesystem which is part of the download page.

The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

setenv bootargs_rd     mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp="dvi"
setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp="dvi"
setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp="dvi"

The bootargs for DVSDK releases from 3.01.00.02 onwards are as given below

setenv bootargs_rd     mem=100M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp="dvi"
setenv bootargs_fs     mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp="dvi"
setenv bootargs_nfs    mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp="dvi"

The bootargs for DVSDK release 3.00.02.44 is as given below

setenv bootargs_rd     mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"
setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"
setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"

The bootargs for DVSDK releases from 3.00.00.36 to 3.00.01.42 are as given below

setenv bootargs_rd     mem=88M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"
setenv bootargs_fs     mem=88M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"
setenv bootargs_nfs    mem=88M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"

Command Line Arguments

Once the EVM is booted, you can change the output display from LCD to DVI from the Linux shell in a terminal window connected to the EVM board’s serial port.

Note:The bootargs for DVSDK releases from 3.01.00.09 onwards requires modifications for switching from LCD to DVI using the command line at run-time

Add the following command omapfb.mode=dvi:720x480MR-16@60 to the bootargs if you intend to switch the display from LCD to DVI during run time. This is required for the DVSDK decode demos not to return errors at the end of playback or when it returns to the interface application.

For Example,

setenv bootargs_rd     mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60
setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60
setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60

Note:The bootargs for DVSDK releases from 3.01.00.02 onwards requires modifications for switching from LCD to DVI using the command line at run-time

Add the following command omapfb.mode=dvi:720x480MR-16@60 to the bootargs if you intend to switch the display from LCD to DVI during run time. This is required for the DVSDK decode demos not to return errors at the end of playback or when it returns to the interface application.

For Example,

setenv bootargs_rd     mem=100M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omapfb.mode=dvi:720x480MR-16@60
setenv bootargs_fs     mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omapfb.mode=dvi:720x480MR-16@60
setenv bootargs_nfs    mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 omapfb.rotate=1 omapfb.vrfb=y vram=10M omapfb.vram=0:10M omapfb.mode=dvi:720x480MR-16@60

The Commands for DVSDK releases since 3.01.00.02 are to be given as below for switching from command line at Run Time

target $ echo 0 > /sys/devices/platform/omapdss/display0/enabled
target $ echo "" > /sys/devices/platform/omapdss/manager0/display
target $ fbset -fb /dev/fb0 -xres 720 -yres 480 -vxres 720 -vyres 480
target $ echo "dvi" > /sys/devices/platform/omapdss/manager0/display
target $ echo 1 > /sys/devices/platform/omapdss/display2/enabled
target $ fbset -fb /dev/fb0 -xres 720 -yres 480 -vxres 720 -vyres 480

The Commands for DVSDK releases till 3.00.02.44 are to be given as below for switching from command line at Run Time

target $ echo "gfx e:0" > /sys/devices/platform/omapfb/overlays
target $ echo "lcd e:0" > /sys/devices/platform/omapfb/displays
target $ echo "lcd t:none" > /sys/devices/platform/omapfb/managers
target $ echo "dvi e:1" > /sys/devices/platform/omapfb/displays
target $ echo "lcd t:dvi" > /sys/devices/platform/omapfb/managers
/* Set the Frame buffer parameters like xres, xres_virtual, y_res, yres_virtualagain before running below command. For example for 720P as DVI resolution setxres=1280 yres=720 xres_virtual=1280 yres_virtual=1440.*/
target $ echo "gfx e:1" > /sys/devices/platform/omapfb/overlays 

Enabling Audio Capture for Speech encode

Audio Capture for speech encode is not enabled by default.You can use amixer utilty which is present by default enable the Audio Capture.

Once the EVM is booted issue following commands to enable Audio Capture.

target $amixer controls
target $amixer cset name='Analog Left Capture Route AUXL' 1
target $amixer cset name='Analog Right Capture Route AUXR' 1
target $amixer controls
amixer cset name='Analog Left AUXL Capture Switch' 1
amixer cset name='Analog Right AUXR Capture Switch' 1

Enabling TV Out

For enabling S-Video please issue the following command in bootargs 'omapdss.def_disp="tv" omapfb.mode=tv:pal'
Note : Please change mode for NTSC as omapfb.mode=tv:ntsc The bootargs for DVSDK releases from 3.01.00.09 onwards are as given below

setenv bootargs_rd     mem=99M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 vram=20M omapfb.vram=0:20M omap_vout.vid1_static_vrfb_alloc=y omapdss.def_disp="tv" omapfb.mode=tv:pal
setenv bootargs_fs     mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 vram=20M omapfb.vram=0:20M omap_vout.vid1_static_vrfb_alloc=y omapdss.def_disp="tv" omapfb.mode=tv:pal
setenv bootargs_nfs    mem=99M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 vram=20M omapfb.vram=0:20M omap_vout.vid1_static_vrfb_alloc=y omapdss.def_disp="tv" omapfb.mode=tv:pal

The bootargs for DVSDK releases from 3.01.00.06 onwards are as given below

setenv bootargs_rd     mem=100M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,16M ramdisk_size=40960 mpurate=600 vram=20M omapfb.vram=0:20M omap_vout.vid1_static_vrfb_alloc=y omapdss.def_disp="tv" omapfb.mode=tv:pal
setenv bootargs_fs     mem=100M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 vram=20M omapfb.vram=0:20M omap_vout.vid1_static_vrfb_alloc=y omapdss.def_disp="tv" omapfb.mode=tv:pal
setenv bootargs_nfs    mem=100M console=ttyS0,115200n8 noinitrd ip=dhcp rw root=/dev/nfs nfsroot=<nfsserver_ip>:/home/<useracct>/workdir/filesys,nolock mpurate=600 vram=20M omapfb.vram=0:20M omap_vout.vid1_static_vrfb_alloc=y omapdss.def_disp="tv" omapfb.mode=tv:pal

For Enabling Composite out kernel modification has to be done as follows.
Note: The option to be selected is given in ""

$host: make menuconfig ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-
   ...
   ...
   Kernel Features --->
   Boot options --->
   CPU Power Management --->
   Floating point emulation --->
   Userspace binary formats --->
   Power management options --->
   [*] Networking support --->
   "Device Drivers --->"
   ...
   ...
   ...
   ...
   Sonics Silicon Backplane --->
   Multifunction device drivers --->
   [*] Voltage and Current Regulator Support --->
   <*> Multimedia support --->
   " Graphics support --->"
   <*> Sound card support --->
   [*] HID Devices --->
   [*] USB support --->
   ...
   ...
   ...
   ...
   <M> Lowlevel video output switch controls
   '''<*> Support for frame buffer devices --->'''   < > E-Ink Broadsheet/Epson S1D13521 controller support
   [ ] Check bootloader initialization
   -*- OMAP2/3 Display Subsystem support (EXPERIMENTAL) --->
   [ ] Backlight & LCD device support --->
   ...
   ...
   ...
   ...
   <M> Lowlevel video output switch controls
   <*> Support for frame buffer devices --->
   [ ] Check bootloader initialization
   "-*- OMAP2/3 Display Subsystem support (EXPERIMENTAL) --->"
   [ ] Backlight & LCD device support --->
   ...
   ...
   ...
   ...
   [ ] Debug support
   [ ] RFBI support
   "[*] VENC support"
   "OMAP2_VENC_OUT_TYPE (Use S-Video output interface) --->"
   [ ] SDI support
   ...
   ...

The default TV out interface is S-Video. change the option to Composite.
NOTE:Bootargs are same for S-video and composite out.

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article GSG: OMAP35x DVEVM Additional Procedures here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox