GSG: OMAP35x Graphics SDK Additional Procedures
From Texas Instruments Embedded Processors Wiki
^ Up to main OMAP35x Graphics SDK Getting Started Guide Table of Contents
Contents |
Switching between FrontEGL and FlipEGL Modes
When using FrontEGL, SGX fb updates happen directly on single framebuffer (front buffer). Not really recommended except for SGX benchmarking as it will result tearing artifacts at high resolution and frame rates.
FlipEGL uses ping-pong scheme for graphics updates and this is the default EGL library used if /etc/powervr.ini is not present.
Modify the powervr.ini file under the <your_target_file_system>/etc/init.d to select between the FrontEGL or FlipEGL mode.
Flip support requires increasing the virtual yres size in fb0 plane and allocating appropriate memory for framebuffer.
Use the following command to increase the virtual yres size in fb0 plane. The vyres size needs to be set to three times the height of the screen size for triple buffering. For eg:- OMAP3 EVM LCD fb with dimensions 480x640
target $ fbset -vyres 1920
More solutions for vertical tearing
If you are running on a Linux console frame buffer (/dev/fb0) the following shared object may work better for you to prevent vertical tearing at the center of the screen. This object is often found in /usr/lib or /usr/local/lib. libpvrPVR2D_LINUXFBWSEGL.so.
Switching the display output from LCD to DVI
Switching the display output from LCD to DVI during boot time
This can be done by changing in the bootargs to include the following
For 16bpp :
omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"
For 32bpp :
omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-24@60"
For example, in case of NFS mount
OMAP3EVM # setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=<nfshost>:<rootpath>,nolock mem=128M omapfb.vram="4M" omap-dss.def_disp="dvi" omapfb.video_mode="720x480MR-16@60"
Switching the display output from LCD to DVI during run time after boot
Step 1: Refer here to change the display output from LCD to DVI after boot, from the command line, on target.
Step 2: On target, perform the command "fbset -depth 32 -rgba 8/16,8/8,8/0,8/24"
Step 3: On target, perform "/etc/init.d/rc.pvr stop" followed by "/etc/init.d/rc.pvr start"
After this, the demos should run properly on DVI.
Testing the support for ARGB8888 in Frame Buffer Driver
The bootargs need to be changed as given below.
OMAP3EVM # setenv bootargs 'console=ttyS0,115200n8=noinitrd=rw ip=dhcp root=/dev/nfs nfsroot=<your nfs_path>,nolock, mem=128M omapfb.vram="4M" omapfb.video_mode="640x480MR-24@60" omap-dss.def_disp="dvi"'
Use fbset to configure ARGB8888 mode for framebuffer memory
target $fbset -rgba 8/16,8/8,8/0,8/24
Note that if you are switching to ARGB8888 mode after bootup it is mandatory to reload omaplfb.ko kernel module
Leave a Comment