GSG: OMAP35xx WinCE DVSDK Overview

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

^ Up to main OMAP35xx WinCE DVSDK Getting Started Guide Table of Contents

Contents


The OMAP35xx WinCE 100 DVSDK aims to enable developers to create multimedia-rich applications using the WinCE 6.0 R2/R3 Direct Show multimedia framework APIs along with the capabilities of TI's Digitial Signal Processor embedded in the OMAP3530 SoC. The following functionality is provided:

What's in this kit?

For OMAP35xx you will use the OMAP35x EVM board (Both TMDXEVM3503 and TMDSEVM3530 EVMs are supported)and the OMAP35xx WinCE DVSDK software:

Software components

The following figure shows the software components used for application development with the OMAP35xx WinCE DVSDK:

DVSDK WinCE 100 SW Stack 4.jpg

As shown in the figure, your application can use either the Direct Show multimedia framework APIs or TI's APIs such as DMAI and Codec Engine VISA APIs. DMAI uses VISA APIs provided by the Codec Engine to process video, image, speech, and audio signals. The Codec Engine, in turn, uses services such as DSP/BIOS Link and protocols such as XDAIS and XDM to communicate with a preconfigured Codec Engine Remote Server on the DSP subsystem. The DSP handles signal processing.

What's next?

The next chapter of this Getting Started Guide is GSG: OMAP35xx WinCE DVSDK Hardware Setup.

After you have finished with all the topics in this Getting Started Guide, you can see the following for more information:

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox