GSG C6748: Building Projects

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

^ Up to main Getting Started Guide for C6748 Table of Contents

Contents

Building a project

In order to re-build an example, follow these steps:

  1. Open CCStudio (Code Composer Studio).
  2. Select Project -> Open from the menus.
  3. Browse to the project location and select the project file (.pjt). For example, for the C6748 audio project, the default path is: C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05\packages\ti\pspiom\examples\evm6748\audio\build
  4. After opening the project, select Project -> Build from the menus.


Do not forget to read the documents at:

C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05\docs\C6748\

There you can find the document C6748_BIOSPSP_Userguide.pdf. Look at item 6 in Section 1.4.1.1, page 13, of this document where there is a description of adding the environmental variable EDMA3LLD_BIOS5_INSTALLDIR.

To add the environmental variable, follow these steps:

  1. Open the Windows Control Panel tool called System.
  2. Choose the Advanced tab.
  3. Click the Environment Variables button at the bottom of the tab.
  4. In the System variables area, click on the New button.
  5. Type EDMA3LLD_BIOS5_INSTALLDIR as the Variable Name.
  6. Type C:/C674x_dsp_1_00_00_10/edma3_lld_01_07_00_01 (or the equivalent path on your computer) as the Variable Value.
  7. Click OK.

If you do not add this environmental variable you might get a Compilation failure message.

NOTE: The Userguide is incorrect for 1_30_01 install when is states that you need to have \packages at the end of the installation path. The folder \packages is defined in the Build Options.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox