GStreamer Releases
From Texas Instruments Embedded Processors Wiki
Contents |
GStreamer gst-dmai Releases
Released Source Code
Stable Releases
Stable release are located by clicking on the "Files" panel on the left-hand side of the page. The latest release will be visible under the "TIGStreamerPlugin" package. There are two tarballs in each release:
gst-ti-plugin-full-x.xx.xx.tar.gz:
The TI GStreamer Plugin, sample scripts, and a complete build system for building with the TI DVSDK. Open source libraries needed for the build that are not included with the DVSDK are also included.
gst-ti-plugin-minimal-x.xx.xx.tar.gz:
The TI GStreamer Plugin only. Suitable for building the plugin in other environments such as OpenEmbedded, but some work may need to be done to the build system. See the "BUILDING_STAND_ALONE.txt" file in the release for more information. Creating a Stable Release
A candidate stable release is a branch in SVN while other development can continue on the mainline. The candidate release under goes testing on one or more of the OMAP/DM devices. Any issues that are resolved are merged back into the mainline. A list of the tests run, known issues, tested OMAP/DM device, and other information related to cadidate testing are captured in the release notes. The released software is tagged in SVN.
A step-by-step explanation of the release process can be found on the [CreatingARelease | Creating a Release] page.