Getting Started Guide for Leopard Board DM365 and DM368

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Overview

Leopard Board is an Open Source hardware project, a full featured, ultra low cost, small form factor, high performance development system which includes a TMS320DM365 Processor board. The Leopardboard DM365 is enhanced with more HD Video codecs, Face Detection and HD Video output.

The board is manufactured by Leopard Imaging.

Differences between Leopard Board DM365 and Leopard Board DM355

The following table contains the main differences between Leopard Board DM355 and Leopard Board DM365.


Table 1. Differences between Leopard Board DM355 and Leopard Board DM365
Feature Leopard Board DM355 Leopard Board DM365
Processor TMS320DM355 TMS320DM365
Video output Composite TV Output Composite TV/Component HD TV Output
Video codecs MPEG4, JPEG H.264, VC1, MPEG2, MPEG4, JPEG
Audio codecs MP3, AAC, WMA MP3, AAC, WMA and Audio Echo Canceller
Camera sensors Support wide range of video resolutions from VGA, 1.3M, 2M, 3M to 5 Mega-pixel CMOS Sensors Support wide range of video resolutions from VGA, 1.3M, 2M, 3M to 5 Mega-pixel CMOS Sensors

Hardware

This section shows a brief explanation of the LeopardBoard's hardware, for a little more deep reference you can see the Leopard_Board_DM365_Hardware_Guide.pdf.

Basically the LeopardBoard DM365 is an evaluation board that allows to get access to all the hardware and software capabilities of the TMS320DM365 Texas Instrument's system-on-chip (SoC). This SoC belongs to the DaVinci family oriented principally to multimedia applications.

Components

In the next figures are showed the top and bottom views of the LeopardBoard DM365, over these has been indicated the main hardware components of the LeopardBoard DM365.

Figure 1. LeopardBoard DM365 top view.
Figure 2. LeopardBoard DM365 bottom view.

The following table describes the main hardware components of the LeopardBoard DM365.


Table 2. Basic descriptions of the LeopardBoard DM365 components.
ID Name Description
1 Expansion port Supports SD/MMC, I2C, UART, McBSP, GPIO ans 3.3V power supply.
2 JTAG port Is's a 14 pin JTAG port to allows the software debbuger.
3 Reset Button Resets the system.
4 UART serial output A RS-232 serial port is provided by a 2.5mm stereo audio jack.
5 Microphone input A 2.5mm standard stereo audio jack to receive stereo audio input to the CODEC chip.
6 Network interface A standard RJ-45 connector for 10/100 Ethernet networks.
7 DC Power input The boards provides a 2.1mm power jack for +5VDC power supply with a power consumption less than 2W (see Hardware Guide for more detail). The power also can be supplied by the USB port.
8 SD card slot It is provided as a mean of expansion and also as a interface for this kind of devices.
9 LCD/DVI interface A 50-pin connector fully compatible with DM365EVM expansion connector and with support for LCD or DVI daughter card.
10 Composite video output The LeopardBoard provides a 2-pin video output connector fully compatible with NTSC or PAL format. It's default at NTSC format.
11 Camera module interface This interface supports a wide range of camera modules, from 1.3M to 5 Mega-pixel CMOS sensors.
12 Component video output This port provides access to a component video signal with YPbPr format compatible with TV or other component.
13 Speakers output jack This is a 2.5mm standard stereo jack which provides a stereo audio signal from the CODEC chip.
14 USB OTG port The LeopardBoard DM365 supports both, device and host usb modes. By default the board is working on USB device mode which the capability to be changed on hardware easily (see the LeopardBoard DM365 Hardware User Guide [[1]] for more detail).
15 TMS320DM365 Processor The TMS320DM365 processor is an ARM9-based system-on-chip oriented to basic video processing applications like IP cameras or digital photo frames. For a deep description of the processor characteristics you can see the File:Tms320dm365.pdf.
16 Flash Memory LeopardBoard DM365 includes a Micron Flash Memory with 256M x 8-bit, 2Gb SLC NAND Flash.
17 DDR2 SDRAM This Micron DDR2 SDRAM have 8M x 16 x 8 banks, 1Gb DDR2 SDRAM.
18 Boot up control switch This dip switch allows the user to select the boot mode, that is from where the LeopardBoard will start the system. See the LeopardBoard DM365 Hardware User Guide [[2]] for more information about how to set a specific boot mode.

Camera module

As it was mentioned before, the LeopardBoard DM365 was designed principally for video applications such as IP cameras; is for this reason that there are many camera modules that are compatible with the LeopardBoard DM365. In this section you will find a description table of this camera modules, for more information you can see the [LeopardBoard_DM365_Hardware_User_Guide.pdf].

You can use i2c-tools to read the sensor Chip Version register using the command:

i2cget -f -y 1 0x48 0x0 w # for LI-5M03 / MT9P031

Flip the bytes as i2cget uses anti-Klingon ordering. Different sensors will need different commands (they will be documented as folks with hardware contribute to this page). The table below lists the Chip Version when hardware was available to verify the contents.

Table 3. Camera modules for LeopardBoard DM365.
Name Part Number Description Image
VGA camera board LI-LBCMVGA
  • Sensor: Micron/Aptina 1/11“ CMOS Sensor MT9V113
  • VGA resolution of 648x488 pixels.
  • Output data format: YUV (YCbCr).
  • Sensor part type: SOC with internal color saturation, white balance, noise reduction, dark current management.
  • Infrared Coating filter at 650nm+/-10nm.
  • Focus distance: 40cm+/-2cm.
  • Where to buy: LeopardImaging.com
VGA camera board.jpeg
1.3 Mega-pixel camera board LI-LBCM1M1
  • Sensor: Aptina 1/4“ CMOS Sensor MT9M112
  • Resolution: 1.3 Mega-pixels (1280x1024 pixels).
  • Output data format: YUV (YCbCr).
  • Sensor part type: SOC with internal color saturation, white balance, noise reduction, dark current management.
  • Infrared Coating filter at 650nm+/-10nm.
  • Focus distance: 120cm+/-2cm.
  • Where to buy: LeopardImaging.com
1.3Mpixel camera board.jpeg
2 Mega-pixel camera board LI-LBCM2M1
  • Sensor: Aptina 1/4“ CMOS Sensor MT9D112
  • Resolution: 2 Mega-pixels (1600x1200 pixels).
  • Output data format: YUV (YCbCr).
  • Sensor part type: SOC with internal color saturation, white balance, noise reduction, dark current management.
  • Infrared Coating filter at 650nm+/-10nm.
  • Focus distance: 120cm+/-2cm.
  • Where to buy: LeopardImaging.com
2Mpixel camera board.jpeg
3 Mega-pixel camera board LI-LBCM3M1
  • Sensor: Aptina 1/4“ CMOS Sensor MT9T111
  • Resolution: 3 Mega-pixels (2048x1536 pixels).
  • Output data format: YUV (YCbrCr).
  • Sensor part type: SOC with internal color saturation, white balance, noise reduction, dark current management.
  • Infrared Coating filter at 650nm+/-10nm.
  • Focus distance: 120cm+/-2cm.
  • Where to buy: LeopardImaging.com
3Mpixel camera board.jpeg
5 Mega-pixel camera board LI-LBCM5M1
  • Sensor: Aptina 1/2.5“ CMOS Sensor MT9P011
  • Resolution: 5 Mega-pixels (2592x1944 pixels).
  • Output data format: RGB.
  • Infrared Coating filter at 650nm+/-10nm.
  • Focus distance: 120cm+/-2cm.
  • Where to buy: LeopardImaging.com
5Mpixel camera board.jpeg
5 Mega-pixel camera board LI-5M03
  • Sensor: Aptina 1/2.5“ CMOS Sensor MT9P031
  • Max Resolution: 5 Mega-pixels (2592x1944 pixels, 14 fps)
  • Data output format: RGB
  • Pixel Size: 2.2um x 2.2um
  • Support 720p @ 60 fps and 1080p @ 31 fps
  • Chip Version (I2C address 0x48, register 0 contents): 0x1801
  • Where to buy: LeopardImaging.com
5Mpixel camera board 2.jpeg
WVGA Global Shutter camera board LI-VM34LP
  • Sensor: Aptina 1/3” CMOS Digital Sensor MT9V034
  • Resolution: VGA (752x480 pixels).
  • Pixel size: 6um x 6um.
  • Support 60fps at full resolution.
  • Support either M12 lens or CS-Mount lens.
  • Where to buy: LeopardImaging.com
WVGA camera board.jpeg
Omni Vision 720p camera board LI-OV720
  • Sensor: Omnivision 1/4“ CMOS Sensor OV9712
  • Resolution: WXGA (1280x800).
  • Pixel size: 3um x 3um.
  • Output data format: 10-bit raw RGB.
  • Where to buy: LeopardImaging.com
Omni Vision 720p camera board.jpeg
Omni Vision 1080p camera board LI-OV1080
  • Sensor: Omnivision 1/3“ CMOS Sensor OV2710
  • Resolution: 1920x1080 pixels.
  • Pixel size: 3um x 3um.
  • Output data format: 8-/10-bit raw RGB data.
  • Where to buy: to be released.
Not available.

Video modules

There are also some additional video function modules that can be attached to the LeopardBoard DM365 to increase its capabilities. The following is a table with a basic description of this modules, some other information could be found in the LeopardBoard DM365 Hardware User Guide [[3]] .

Table 4. Additional video function modules for the LeopardBoard DM365.
Name Part Number Description Image
DVI output board LI-DVI1 DVI board.jpg
Video composite input board LI-VI365 Video input board.jpg
Video HD component input board LI-HDI365 HD component video board.jpg

Schematic

You can find the LeopardBoard DM365 (revision 1.3)'s schematic at the following link File:DM365 rev 1.3 Schematic.pdf or you can access to LeopardBoard_Homepage in order to find the latest version.

Besides the above, in the following link is possible to find the camera module schematic for the LeopardBoard DM365:

and in the next link the DVI board schematic:

Layout

You can get the PCB layout for the LeopardBoard DM365 revision 1.3 at the following link: LeopardBoard_DM365_PCB.pdf or get it directly from the LeopardBoard_Homepage, in this page you can find also the Gerber version of the PCB.

Clocking

The ARM9 CPU that includes the TMS320DM365 allows to work at clock speeds of 216MHz, 270MHz and 300MHz. In the figure showed above it is possible to see the different clocking values in the LeopardBoard hardware depending of the CPU main clock speed.

Figure 3. LeopardBoard DM365 hardware speeds according with the CPU speed. (Source: TMS320DM365 Datasheet.)

Availability

Where to purchase your Leopard Board DM365?

Leopard Board DM365 is available from:

What to do in case your country is not on the list of shipping countries?

In case your country is not on the Avnet Express or Leopard Online shopping car, you can follow the next steps:

1. Email purchase order to : sales@leopardimaging.com, listing parts number to buy and QTY.

2. Payment methods: VISA/MasterCard Credit Cards, Paypal or T/T in advance. Please fax the Credit Card information to : 001-510-489-8352 (For security reasons, please do not send credit card information through email).

3. Shipment: UPS, FedEx or USPS.

How to select the shipping method?

Adapters

In this section it will be explained a little about the adapters that you could or must use with the LeopardBoard DM365. For a quite detailed information about the LeopardBoard hardware and its adapters you can refers to the LeopardBoard DM365 Hardware User Guide [[4]].

Serial cable adapter

As it was mentioned at the Hardware section, the LeopardBoard DM365 has a serial interface available through a 2.5mm standard stereo jack. In order to get access to this port through a device with a DB9 serial connector is necessary a serial cable adapter such as the showed in the Figure 4. This adapter converts from 2.5mm stereo plug to female DB9 connector.

Figure 4. Serial cable adapter for the UART interface.

Where to buy: LeopardImaging.com

Power adapter

The power adapter is a +5VDC 2.5A switching power supply with an universal AC input. It works either at 50Hz or at 60Hz frequency. The connector is a conventional 2.1mm AC plug polarized with the positive in the center. In the following figure is shown a power adapter for the LeopardBoard DM365.

Figure 5. Power supply adapter for the LeopardBoard DM365.

Where to buy: LeopardImaging.com

USB adapter

As the LeopardBoard DM365 has a mini-USB port, it is necessary to use a USB cable adapter in order to connect the LeopardBoard to a device with a conventional USB connector. In the Figure 6 is showed this USB adapter used for the LeopardBoard DM365.

Figure 6. USB adapter for the LeopardBoard DM365.

Where to buy: LeopardImaging.com


Composite video adapter

There is a composite video adapter for the LeopardBoard DM365. This adapter converts the LeoardBoard's 2-pin composite output to the standard RCA port in order to conect the video output to a video device. The following figure shows this composite video adapter.

Figure 7. Composite video adapter.

Where to buy: LeopardImaging.com

Component video adapter cable

It is useful to convert the LeopardBoard's composite video stereo jack to Y/Pb/Pr RCA connector. It is shown in the following figure.

Figure 8. Component video adapter.

Where to buy: LeopardImaging.com

BootRom

The LeopardBoard DM365 contains a BootRom characteristic, that is, it is able to boot from either its permanent storage device (NAND) or from another external source like a SD Card or through the serial port.

In order to select the boot method with which the board will start, it includes a dip switch called Boot up control switch (see the section 2.1), this switch allows the user to easily selects the boot source the board will looking for.

The possible boot modes are the following:

Table 5. Boot mode selection.
Switch 1 Switch 2 Switch 3 Boot mode
off off off NAND Boot Mode
off on off SD Card Boot Mode
off on on UART Boot Mode
on off off USB Boot Mode
on on off EMAC Boot Mode

NAND Boot Mode

This is the default boot mode of the LeopardBoard DM365. The board reads its U-Boot from it and starts the system (which can be allocated either on the NAND flash or in a NFS server).

MMC/SD Card Boot Mode

It is possible to start up the LeopardBoard from the MMC/SD Card. At the moment (July, 2010) this is the only way to load the U-Boot on the NAND memory in the LeopardBoard, if you want to know how to do that you can see the following web page How to flash U-Boot using a SD card.

There is also the following link where it is possible to find how to use the boot and flashing tools with the SD Card: SD card boot and flashing tool for DM355 and DM365. These tools and the images needed are available at the LeopardImaging downloads page.

UART Boot Mode

The TMS320DM365 SoC allows to load a small program (UBL) directly from the serial port to its internal RAM. At the moment (July, 2010) this option is not available for the LeopardBoard DM365.

USB Boot Mode

Although the LeopardBoard's TMS320DM365 SoC allows to boot from a USB device charging a second stage of the UBL (User Bootloader) into the LeopardBoard's RAM and then transferring the control to the user software, now (July, 2010) this option is not available for the LeopardBoard DM365.

EMAC Boot Mode

The TMS320DM365 SoC included on the LeopardBoard DM365 also allows an EMAC boot mode, that is, it is possible to transfer the data boot packages through a Ethernet connection in order to start the processor. Although this characteristic is available on the TMS320DM365 SoC, it is unavailable in the LeopardBoard DM365 at the moment that this note was wrote (July, 2010).

Code

Code and binaries for Leopard Board DM365 are available from different sources.

Binaries

Leopard Imaging offers a series of demos for your Leopard Board, you can find the binaries for the following demos here:

Source

RidgeRun Evaluation SDK for Leopard Board DM365

RidgeRun offers an Evaluation SDK for Leopard Board DM365. The Evaluation SDK will allow you to do the following:


Some of the goals behind the Evaluation SDK are:


For further development and requirements, you can purchase a Professional SDK.


The following table shows the available version of the Evaluation SDK.

Table 6. RidgeRun Evaluation SDKs versions
Version Features Information
Beta Release 844703
  • Linux Kernel 2.6.18 (support 2.6.32 coming soon).
  • Uboot 2009.10.
  • RidgeRun u-boot installer technology to simplify firmware deployment.
  • DVSDK 2.10.18 integration into the build system
  • GStreamer support for MJCP codecs
  • Toolchain based on gcc 4
New release coming soon

Some of the main features it will have are:

  • 5M camera support


For information on how to install the Evaluation SDK please visit the Installing RR Evaluation SDK for Leopard Board DM365 page.

Compiler

TMS320DM365 processor on Leopard Board contains an ARM926EJ-S general purpose processor.

ARM

There is broad compiler support including gcc - please see ARM Compilers

Board recovery

If your LeopardBoard DM365 is bricked you can refers to the following links in order to recover it:


Beginners guide

You just received your Leopard Board, what do you have to do now? Please review the Beginners guide for Leopard Board DM365.

FAQ

For Leopard Board frequently asked questions (FAQ) see Leopard Board DM365 FAQ

Links

Leopard Board Community

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Getting Started Guide for Leopard Board DM365 and DM368 here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox