Guidelines when porting NDK to different PHYs
From Texas Instruments Embedded Processors Wiki
This page is intended to provide general guidelines about NDK device drivers' source code and highlight specific points necessary to adapt it to custom EMAC/PHY combinations.
Contents |
Introduction
Since the beginning, NDK was designed to abstract the environment by using two layers of software that require minimum changes depending on the OS and the hardware used. These layers are the Operating System Abstraction Layer (<os.lib>) and the Hardware Abstraction Layer (all the libraries of type <hal_device_name.lib>).
Typically no changes are required to the OSAL, which runs on top of DSP/BIOS. However, the HAL is a source of frequent questions asking to port to specific hardware configurations or different PHYs. Since it is impossible to foresee all the custom hardware implementations or PHY devices available on the marketplace today, the source code for the drivers is available with the NDK distributions since release 1.92.
In addition to the source code availability, the great number of source files in a typical NDK project are usually confusing for anyone that is trying to make modifications to adapt for custom hardware.
Therefore the information below is given to help pinpoint the places where device drivers' code should be carefully examined and modified. Note that several of the PHY manufacturers do not open detailed datasheets or configuration information unless under a non-disclosure agreement, therefore any changes are of entire responsibility of the customer.
Useful information
For NDK 1.9x releases, each Network Support Package (NSP) contains a design document for the Ethernet device driver that covers the basic architecture and file organization. These files are usually installed under %NDK_INSTALL_DIR%\packages\ti\ndk\docs\<device_name>
For NDK 2.00, the NSP Ethernet Driver Design Guide (SPRUFP2) contains the information for all the device drivers and is typically installed under %NDK_INSTALL_DIR%\packages\ti\ndk\docs\stack
The NDK Programmer's Guide for NDK 1.94 and 2.00 contains additional information in the sections A.14 (for NDK 1.94) and A.15 (for NDK 2.00).
Note: The information in these two last references can also be applied to the NSPs for C6455 and DM642 running with NDK 1.94.
Due to performance and added features, it is highly recommended to use the NIMU driver architecture consolidated in NDK release 2.00. Please note that there are also several driver-stack API changes that render it backward incompatible with previous versions.
Tips to modify device drivers
llPacket
The llPacket source code location varies depending on the installation but is typically located at %NDK_INSTALL_DIR%\packages\ti\ndk\src\hal\<device_name>
1) Hardware Independent Low-Level Ethernet Driver. This layer is provided in the file named <llpacket.c> and does not require changes to adapt to different PHYs.
2) Hardware Specific Low-Level Ethernet (mini) Driver. As the name says, this layer contains the hardware dependent information and changes should be done to specific files.
- The EMAC configuration files may require just minimal changes (if any), since they mostly change EMAC-only settings. Some examples of these files are <dm642.c>, <c6455.c>, <c64lc.c>, <cpsw3g_core.c>
- The MDIO configuration files need to be carefully inspected and modified, since they perform the functions of PHY initialization, configuration (MDIO_initPHY() or cpsw_MDIO_Init() functions) and polling (MDIO_timerTick() or cpsw_MDIO_Tic() functions). Some examples of these files are: <c6455_mdio.c>, <64lcmdio.c> and <cpsw_miimdio.c>
For example, the code below starting at line 582 of the file <c6455_mdio.c> might have to be modified to properly initialize a different PHY:
/* Settings for Broadcom phys */ if ( macsel == CSL_DEV_DEVSTAT_MACSEL_RGMII ) { //Put phy in copper mode PHYREG_write( PHYREG_ACCESS, phyAddr, PHYREG_ACCESS_COPPER ); PHYREG_waitResultsAck( i, ack ); /* If the PHY did not ACK the write, return zero */ if( !ack ) return(0); PHYREG_write( 0x10, phyAddr, 0x0000 ); //GMII Interface PHYREG_wait(); // Put phy in RGMII mode/in-band status data for PG 2.0 if (EMAC_REGS->TXIDVER != 0x000C1207) { PHYREG_write(PHYREG_SHADOW, phyAddr, PHYREG_SHADOW_INBAND); PHYREG_waitResultsAck( i, ack ); /* If the PHY did not ACK the write, return zero */ if( !ack ) return(0); } }
Note: If the dsp MII is connected to a switch please make sure that the following lines are not included in MDIO_initPHY():
/* Shutdown all other PHYs */ ltmp1 = MDIO_REGS->ALIVE ; for( i=0; ltmp1; i++,ltmp1>>=1 ) { if( (ltmp1 & 1) && (i != phyAddr) ) { PHYREG_write( PHYREG_CONTROL, i, PHYREG_CONTROL_ISOLATE | PHYREG_CONTROL_POWERDOWN ); PHYREG_wait(); } }
These lines were added for the boards populated with a single PHY (like the dm6437 evm in example), but prevent a switch from working properly.
3) The hardware initialization file in each example project. These files contain functions called before main() and read or configure some initial parameters for the hardware. These files are usually located in the example project directories. For example, at the end of the file <dsk6455init.c> the code below may have to be modified:
void C6455EMAC_linkStatus( uint phy, uint linkStatus ) { Uint16 pData; printf("Link Status: %s on PHY %d\n",LinkStr[linkStatus],phy); MDIO_phyRegRead( phy, 0x2, &pData ); // Program the LEDs for the Intel phy if (pData ==0x13) MDIO_phyRegWrite( phy, 0x14, 0xd5d0 ); // Program the LEDs for the Broadcom phy if (pData ==0x20) MDIO_phyRegWrite( phy, 0x1C, 0xa418 ); }
NIMU
The NIMU source drivers are usually located in the directory %NDK_INSTALL_DIR%\packages\ti\ndk\src\hal\<board_name>\eth_<device_name>
1) Layer 1 – NDK stack interaction layer (NIMU layer). Since it encapsulates all interactions between the stack and the NIMU layer, it has no PHY or hardware dependency. Please check section 2.2 of the NSP Ethernet Design Guide above. Typically the usage example of this layer is shown in the file <nimu_eth.c>
2) Layer 2 – Ethernet mini-driver layer. This layer configures the EMAC using the data structures exposed by underlying CSL layers data structures and APIs. Despite directly communicating with the hardware (cache, interrupts, etc) its code is mostly contained into the DSP itself, thus requiring minor (if any) changes to accomodate a different PHY. This layer is usually shown in the file <ethdriver.c>. For example, check the code below starting at line 401 of the file <ethdriver.c> for C6455; if the use of Jumbo Frames is desired but the PHY supports a MTU value smaller than 10200 bytes, an adjustment is required to the value of ecfg.PktMTU.
#ifndef _INCLUDE_JUMBOFRAME_SUPPORT ecfg.PktMTU = 1514; #else ecfg.PktMTU = 10200; #endif
3) Layer 3 – CSL EMAC / MDIO layer. External hardware dependent layer. Defines data structures and APIs required to configure and control the EMAC and PHY. Changes to this layer can be split in two categories:
- CSL EMAC configuration. Despite the fact that CSL itself directly interacts with the hardware, very little is needed to be changed to the EMAC configuration file since it is tailored for the DSP. Such configuration is usually located in the file named <csl_emac.c>.
- CSL MDIO configuration. Similarly to the MDIO configuration files for llPacket interface, the code requires careful inspection and modification to match the PHY - the names of the functions also match the ones listed for llPacket MDIO configuration. Such configuration is performed by the file <csl_mdio.c>
For example, the code below starting at line 618 of the file <csl_mdio.c> might require modifications to be adjusted to a different PHY.
/* Settings for Broadcom phys */ if ( macsel == RGMII ) { /* Put phy in copper mode */ PHYREG_write( PHYREG_ACCESS, phyAddr, PHYREG_ACCESS_COPPER ); PHYREG_waitResultsAck( i, ack ); /* If the PHY did not ACK the write, return zero */ if( !ack ) return(0); PHYREG_write( 0x10, phyAddr, 0x0000 ); //GMII Interface PHYREG_wait(); // Put phy in RGMII mode/in-band status data if (EMAC_REGS->TXIDVER != 0x000C1207) { PHYREG_write(PHYREG_SHADOW, phyAddr, PHYREG_SHADOW_INBAND); PHYREG_waitResultsAck( i, ack ); } // If the PHY did not ACK the write, return zero if( !ack ) return(0); #if 0 // Override gtxcdly so it's low - it's still needed on EVM PHYREG_write( PHYREG_ACCESS, phyAddr, 0x8C00 ); PHYREG_waitResultsAck( i, ack ); // If the PHY did not ACK the write, return zero if( !ack ) return(0); #endif }
4) At last, verify the hardware initialization files in each example project. Its names, locations and functionality are identical as shown in the llPacket interface above.
Emac layer
C647x specific: verify the phy setup in comparison with the NDK evm configuration. On the on the 6474 evm the connection between the phy and the device has a polarity setting which is specific for a hw workaround.
The schematics of the board can be seen at: http://support.spectrumdigital.com/boards/evmc6474/revb/
When using your own board, assuming you connected the phy properly, you will likely have to rebuild the ethernet driver which is generating the library
NDK_2_0\lib\hal\evm6474\hal_eth_c6474.lib
Basically you will need to edit the file NDK_2_0\src\hal\evm6474\eth_c6474\ethdriver.c at line 601 to make sure you specify the correct polarity for the SGMII connection between the device and the PHY
the value to be edited / checked is:
SgmiiCfg.txConfig = 0x00000ea1;
for the actual meaning of the bit fields, refer to the emac user guide of the device
Leave a Comment