Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

How to Switch Display From Touchscreen to DVIout with Matrix

From Texas Instruments Wiki
Jump to: navigation, search

TIBanner.png

Return to the Sitara Linux Software Developer's Guide

Introduction

A DVI display can be used instead of the LCD touchscreen with the Matrix GUI by following these steps.

Stop Matrix

First stop the matrix application by running the following command.

/etc/init.d/matrix-gui-2.0 stop

A stale output from matrix will still show on the LCD even though the application is now dead.

Run commands to Switch the Display

The following set of commands will switch the display output from the LCD to the DVI port.  The stale output from when matrix was killed will now be sent to the DVI port at 480p resolution.

        echo 0 > /sys/devices/platform/omapdss/display0/enabled
        echo 0 > /sys/devices/platform/omapdss/overlay0/enabled
        echo "" > /sys/devices/platform/omapdss/overlay0/manager
        echo "720,480" > /sys/class/graphics/fb0/virtual_size
        fbset -fb /dev/fb0 -xres 720 -yres 480
        echo "lcd" > /sys/devices/platform/omapdss/overlay0/manager
        echo "dvi" > /sys/devices/platform/omapdss/manager0/display
        echo 1 > /sys/devices/platform/omapdss/display2/enabled
        # DVI out timing can be configured at boottime
        # for 480p, the boot argument is "omapfb.mode=dvi:720x480@60"
        # By default DVI display timings are configured at VGA resolution
        echo "27903,720/24/96/96,480/10/32/3" > /sys/devices/platform/omapdss/display2/timings
        echo 1 > /sys/devices/platform/omapdss/overlay0/enabled

Restart Matrix

Run the script below to start up matrix. It will start matrix without rotation and with a mouse as default input.

/usr/bin/matrix-gui-dvi-2.0.sh start

Matrix will now be displayed to the DVI port.  Depending on the type of display/monitor connected to the DVI port, it may necessary to adjust the setting to get the proper display.  Refer to the instructions for the particular display or monitor that you are using.