Installing CodeSourcery Toolchain
From Texas Instruments Wiki
How to Obtain the CodeSourcery Lite Edition
This section walks through the steps required to install the Code Sourcery Lite toolchain for ARM GNU/Linux EABI processors. The specific toolchain release is 2011.03-42.
NOTE: Download the "IA32 GNU/Linux TAR" tarball. It is significantly smaller and takes less time to download.
When installing please remember the location you installed this toolchain. If your EVM comes with a SDK Installer it will check for a valid toolchain.
Uncompress tar file (About 73.8MB) # tar xvf arm-2009q1-203-arm-none-linux-gnueabi-i686-pc-linux-gnu.tar Move to /opt/CodeSourcery/Sourcery_G++_Lite, /opt/ is the custom software folder in Ubuntu. # mkdir /opt/CodeSourcery # mv arm-2009q1 /opt/CodeSourcery/Sourcery_G++_Lite Add path to existing shell, and apply. # vi ~/.bashrc export PATH=/opt/CodeSourcery/Sourcery_G++_Lite/bin:$PATH # source ~/.bashrc Execute the SDK installer # chmod 755 ./ti-sdk-am180x-evm-4.0.1.0-Linux-x86-Install # ./ti-sdk-am180x-evm-4.0.1.0-Linux-x86-Install
How to Obtain the CodeSourcery Commercial Edition
CodeSourcery also provides commercial edition that contains an IDE, additional tools and support from CodeSourcery. See CodeSourcery offerings for Davinci™, OMAP™ and Sitara™ processors here.
A DVD containing both CodeSourcery G++ Lite and Evaluation version of commercial tools are shipped with the various kits such as the AM37x Evaluation Module.
NOTE - When using the arm_2009q1_203_arm_none_linux_gnueabi.bin instead of the TAR, the toolchain path is /home/user/CodeSourcery/Sourcery_G++_Lite (assumes default). To set path for bash shell, edit .bashrc file by adding the lin:
export PATH=/home/user/CodeSourcery/Sourcery_G++_Lite/bin:$PATH
Comments
Comments on Installing CodeSourcery Toolchain
D-smalley said ...
Baldwinc said ...
CodeSourcery download path appears to be bad, try this:
http://www.codesourcery.com/sgpp/lite/arm/portal/release858
Download the ".bin" file.
To Install, run the UI by typing:
/bin/sh ./arm-2009q1-203-arm-none-linux-gnueabi.bin
--Baldwinc 17:06, 14 September 2011 (CDT)


Executing arm_2009q1_203_arm_none_linux_gnueabi.bin will place the tool chain at /home/user/CodeSourcery/Sourcery_G++_Lite (if using default).
To set path for bash shell, edit .bashrc file by adding thie line
export PATH=/home/user/CodeSourcery/Sourcery_G++_Lite/bin:$PATH
--D-smalley 09:28, 17 August 2010 (CDT)