Interrupt FAQ for C2000

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Introduction

This is an frequently asked question list for C28x interrupts and the Peripheral Interrupt Expansion (PIE) unit.

Electrical Specifications

Electrical specifications can change between devices, peripheral types and device families. Always refer to the data manual and errata for a particular device for Electrical Specifications.

Frequently Asked Questions

Documentation

Q: Where is the CPU's context save and return documented?

Refer to the C28x TMS320C28x CPU and Instruction Set Reference Guide for more information.

Q: Where is the PIE registers and the PIE vector table documented?

Refer to the System Control and Interrupts Reference Guide for your device. All reference guides for each device family are listed in this document: TMS320x28xx, 28xxx DSP Peripherals Reference Guide (SPRU566)

Nesting

Q: Can interrupts be nested?

Absolutely.  Interrupts are automatically disabled when an interrupt begins. That is, the interrupt mask bit, INTM, of the main cpu is automatically set. This will prevent new interrupts from being serviced until software re-enables them or you exit the ISR.
Refer to Interrupt Nesting on C28x for more information

ISR Latency

Consider the following diagram, taken from the C2000 Workshop Material:
C28x Isr Latency.jpg
The actual maximum latency will change, as indicated in the above image. Things that can delay an interrupt:
  • Are interrupts disabled (INTM)? When you take an interrupt this is automatically done - so to allow nested interrupts it has to be cleared.
  • Is the CPU executing a RPT instruction (single repeat). This cannot be interrupted.
  • Multiple cycle instructions - for example, if the CPU was just executing a loop - each time through the loop a branch would be taken which could delay an interrupt for 4 cycles. One way to avoid this is to put the CPU into idle so it will be in the same state each time the interrupt comes in.
  • Is code execution in wait stated memory
  • Is stack in wait stated memory. It is rare to have data memory with a wait state in c2000 but say, just as an example, the stack was in external memory (XINTF).
  • Is the stack and the code in the same physical memory block
  • If the interrupt source is from an external pin, then any qualification on the pin will add to the delay.

Setting up the PIE vector table

Q: How do I link my ISR function to the corresponding interrupt flag bit?

The C/C++ Header Files and Peripheral Examples are a great place to start as they provide peripheral examples with the interrupts already configured. No matter if you are using SPI, SCI, ADC, etc. this software package has interrupt examples.

The ITRAP Interrupt

Q: What causes an illegal (ITRAP) interrupt?

  • An invalid instruction is decoded (this includes invalid addressing modes).
  • The opcode value 0x0000 is decoded. This opcode corresponds to the ITRAP0 instruction.
  • The opcode value 0xFFFF is decoded. This opcode corresponds to the ITRAP1 instruction.
  • A 32-bit operation attempts to use the @SP register addressing mode.
  • Address mode setting AMODE=1 and PAGE0=1which is an illegal combination.

Q: How can I debug an ITRAP?

  • One option is to insert a return instruction into the ISR. Set a breakpoint on this instruction and then step to see where the code came from.
  • Another option is to look at the stack. When you take an illegal instruction trap, registers are automatically pushed on the stack, including the return address. By looking at the return address value on the stack, you can find out where the ITRAP occurred.

Refer to the wiki article C28x Context Save and Restore

T:ST0
ACC
P
AR1:AR0
DP:ST1
DBGSTAT:IER
Return Addr
empty  < SP points here (even or odd address)
E2e.jpg For technical support on the C2000 please post your questions on The C2000 Forum. Please post only comments about the article Interrupt FAQ for C2000 here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox