JTAG Connectors
From Texas Instruments Embedded Processors Wiki
JTAG Connectors
- There are several types of JTAG connectors that are utilized.
- The XDS510 and XDS560 product lines support most of the JTAG_Connectors types. XDS100 also implements JTAG connectors.
- For XDS560 Trace and Trace enabled devices that export through the pins, please see 60 Pin Trace Header. Note that a 60 pin header is not needed for Embedded Trace Buffer useage. This just utilizes JTAG, but is only available for selected devices.
- For MSP430 see JTAG (MSP430) for details.
- You may also want to review XDS Target Connection Guide
Documentation
- Emulation and Trace Headers Technical Reference Manual SPRU655
- The document SPRU641 "Designing for JTAG Emulation Reference Guide" describes the 14-pin JTAG connector and target board electrical requirements for XDS510 JTAG support (despite it's title it is not specific to the TMS320C6000 DSP). Also see your Emulator manufacturer's documentation for emulator specific information.
- The XDS560 header document SPRU589 is available here
- The XDS560 Trace 60 pin header guide is here. For Trace, you may also want to consider reading "Common Trace Transmission Problems and Solutions" here.
- A useful document is SPRA439 here.
Pinout
- For the TI 60 pin connector and the MIPI 60 pin connector, please check here.
- For MSP430 see JTAG (MSP430) for details.
| Pin | TI 14-Pin 0.10" 2 row Molex Target card connector:SAM-TSM-17-DV | Compact TI 20-Pin (CTI) Samtec 0.05" 2 row Molex Target card connector:FTR-110-51-S-D-06 Emulator connector: RSM-110-02-S-D | ARM 20-Pin 0.10" 2 row Molex Target card connector:SAM-TSM-110-DV Emulator connector: SSW-110-22-G-D-VS |
ARM 14-Pin 0.10" 2 row Molex (Not recommended) |
| 1 | TMS | TMS | VTRef | VTRef |
| 2 | TRSTn | TRSTn | VSupply | GND |
| 3 | TDI | TDI | TRST | TRST |
| 4 | TDIS | TDIS | GND | GND |
| 5 | VTRef | VTRef | TDI | TDI |
| 6 | KEY | KEY | GND | GND |
| 7 | TDO | TDO | TMS | TMS |
| 8 | GND | GND | GND | GND |
| 9 | RTCK | RTCK | TCK | TCK |
| 10 | GND | GND | GND | GND |
| 11 | TCK | TCK | RTCK | TDO |
| 12 | GND | GND | GND | SRST |
| 13 | EMU0 | EMU0 | TDO | VTRef |
| 14 | EMU1 | EMU1 | GND | GND |
| 15 | SYSRST# | SRST | ||
| 16 | GND | GND | ||
| 17 | EMU2 | DBGRQ | ||
| 18 | EMU3 | GND | ||
| 19 | EMU4 | DBGACK | ||
| 20 | GND | GND |
Connector Information
TI 14-pin Header Information
- Manufacturer: Samtec USA
- Model Number: TSM-17-DV
- Manufacturer’s Overview: http://samtec.com/technical_specifications/overview.aspx?series=TSM
- Example: TSM-107-01-L-DV-006
- Keyed header for target card: 3M has part number 2514-6002UB. Digikey has the part and the orderable number is MHB14K-ND.(Note this is shrouded, most connections are unshrouded)
TI 20-pin Header Information
- Manufacturer: Samtec USA
- Model Number: FTR-110-51-S-D-06
- Manufacturer’s Overview:
http://www.samtec.com/technical_specifications/overview.aspx?series=FTR
- Recommended Connector: RSM-110-02-S-D
| Manufacturer: | OUPIIN (http://www.oupiin.com/) |
| Model Number: | 2212-2X10G00D/2.8-1P6B (surface mount / mate length is 2.80 mm / 1 pin # 6 pulled Bulk package)
2212-2X10G00D/2.8-1P6U (surface mount / mate length is 2.80 mm / 1 pin # 6 pulled tube package) |
| Manufacturer’s Overview: | http://www.oupiin.com/ |
| Recommended XDS Connector: | 2212-2X10G00D/2.8-1P6B or 2212-2X10G00D/2.8-1P6U |
ARM 20-pin Header Information
- Manufacturer: Samtec USA
- Model Number: TSM-110-DV
- Manufacturer’s Overview:
http://samtec.com/technical_specifications/overview.aspx?series=TSM
- Recommended Connector: SSW-110-22-G-D-VS
Adapters
JTAG Adapter Overview
There are two types of connectors:
- Emulator-This is the connector on the emulator/JTAG ICE/UIF/XDS unit
- Target-This is the connector on the target card
Types of adapters:
- Pin Converters-Passive conversion of one connector type to another
- Adapter-Some active components for different purposes. Ex: Addition of adaptive clocking, buffering of TCK/RTCK signals, Isolation, etc.
JTAG connectors cross reference
TI Part Number, Link to product, or 3rd party product Number
| Target connector | 10-pin ARM | 14-pin TI | 20-pin TI | 20-pin ARM | 60-pin TI | 60-pin MIPI | microSD | |
| Emulator Connector | ||||||||
| 10-pin ARM | N/A | Roadmap | Roadmap | MDL-ADA2 | ||||
| 14-pin TI | TMDSADP1414-ISO1 or TMDSADP1414234 | TMDSADP1420234 or TMDSADPEMU-20T3 | TMDSADPEMU-20A3 | TMDSADP1460 | Roadmap | |||
| 20-pin TI | Usually supplied by manufacturer with emulator. Check manufacturer. | N/A | Usually supplied by manufacturer with emulator. Check manufacturer. | Usually supplied by manufacturer with emulator. Check manufacturer. | Roadmap | Roadmap | ||
| 20-pin ARM | MDL-ADA2 | Lauterbach LA-77485 | TMDSADPEMU-20T3 | TMDSADPEMU-20A3 | Roadmap | |||
| 60-pin TI | Usually supplied by manufacturer with emulator. Check manufacturer. | N/A | Roadmap | |||||
| 60-pin MIPI | Usually supplied by manufacturer with emulator. Check manufacturer. | Usually supplied by manufacturer with emulator. Check manufacturer. | Usually supplied by manufacturer with emulator. Check manufacturer. | Usually supplied by manufacturer with emulator. Check manufacturer. | N/A | |||
1 Isolation adapter
2 Voltage Translation
3 RTCK Signal Boost
4 Adaptive Clocking
5 http://www.lauterbach.com/frames.html?order/ord__7748.html - Code JTAG-ARM-CON-20-TI14
Part numbers:
TMDSADP1414
Product page: http://focus.ti.com/docs/toolsw/folders/print/tmdsadp.html
TMDSADP1414-ISO
Product page: http://focus.ti.com/docs/toolsw/folders/print/tmdsadp.html
TMDSADP1420
Product page: http://focus.ti.com/docs/toolsw/folders/print/tmdsadp.html
TMDSADP1460
Product page: http://focus.ti.com/docs/toolsw/folders/print/tmdsadp.html
TMDSADPEMU-20A
Product page: http://focus.ti.com/docs/toolsw/folders/print/tmdsadp.html
TMDSADPEMU-20T
Product page: http://focus.ti.com/docs/toolsw/folders/print/tmdsadp.html
MDL-ADA2
Product page: http://www.luminarymicro.com/products/mdl-ada2.html
Roadmap
- Various standards organizations have tried to standardize on connectors. TI has several standards already in use. One particular area where significant work has been done is the high speed tracing connectors. This is being driven by technology changes and the changing needs for debug.
- MIPI has a recommendation for a high speed 60 pin trace connector which can provide the flexibility needed for future tracing needs. The recommended connector is the QSH-030-01 (PCB/Target) and QTH-030-01 (Cable/Emulator) connectors from Samtec.
- MIPI Connector recommendation is here. Pin mapping for the 60 pin MIPI connector is in this ocument.
- IEEE 1149.7 does not require a specific connector. Instead, it will simply have the TMS pin become TMSC. When it becomes TMSC, the pin will be bi-directional instead of uni-directional.
FAQ
Q: What are the EMU0/1 pins used for?
- A: The EMU0/1 pins can be used for High Speed RTDX (HSRTDX) or cross-core triggering (ex: one device halts and signals the others to halt, see Advanced Event Triggering). For selected devices, these pins are used for wait-in-reset (ex: TMS320F2808, etc. --> Please see the device datasheet/TRM for details). For selected devices, these pins may also be used to transfer instrumentation and trace information.
Q: What are the EMU2-x pins used for?
- A: These are reserved for high speed instrumentation information and trace information.
Q: What is the difference between the TI 20 pin connector and the ARM 20 pin connector?
- A: The TI 20 pin connector is physically smaller than the ARM 20 pin connector. Becuase it uses a simple "stake" connector, it should also be inexpensive. The TI 20 pin connector has additional EMU2, EMU3, and EMU4 pins, which allow it to carry instrumentation data that are available on selected devices. The TI 20 pin connector also features a System Reset (Emulation) pin.
Q: Do I have to use the ARM 20 pin connector to be able to use Adaptive Clocking?
- A: No. Adaptive clocking has to do with the generation of of the clock signal based on the return clock. Your emulator needs to support this feature, or an adapter is needed. See Adaptive Clocking#Solutions for solutions. The header just needs to have a RTCK and TCK signal.
Q: Which connector should I use?
- A: Use the 60 Pin Trace Header only if your device supports processor trace to the pins. Learn more about XDS560 Trace or from your processor datasheet. If your device is a 24x/28x, you should utilze the TI 14-pin connector. If you do not utilize CCS and XDS560/XDS510 as your toolset (ex: Green Hills, Lauterbach, etc.) and you have existing tools that support the ARM 20 pin connector, you should use the ARM 20 pin connector. For all other situations, the standard, recommended connector is the 20 pin compact TI connector. You should also check what connector your emulator product supports. Emulator vendors such as Spectrum Digital and Blackhawk typically include adapters for the 14 pin TI, 20 pin Compact TI, and the 20 pin ARM configurations.
Q: What do I need to do if I have a device with an ARM 9 or ARM 11?
- A: These ARM devices require adaptive clocking. Please check the section on Adaptive Clocking
Q: What is a Scan Path Linker?
- A: The Scan Path Linker (SPL) is a TI device that is used to configure JTAG scan paths, most often those that connect a motherboard to multiple daughter cards. (This is not the same as the ACT8990 Test-Bus Controller (TBC) device). The scan path linker is used to handle plug-in cards dynamically without breaking the scan path, by reconfiguring the scan path as needed. In general, it is useful whenever your board is in a situation where the scan path can be dynamic, such as during development, when, perhaps not all of the devices on the scan path are populated yet.
The Scan Path Linkers 'ACT8997’, are members of the Texas Instruments SCOPETM testability integrated-circuit family. This family of components facilitates testing of complex circuit-board assemblies. These devices also provide buffering of test signals to reduce the need for external logic. For additional information on the SPL device refer to the following TI site:
Q: Does the TMDSADPEMU-20T, which translates from ARM 20 pin and TI 14 pin emulators to compact 20 pin TI target cards map the reset line from the ARM connector to the compact 20 pin TI target connector? Also, what pins are buffered.
- A: (SRST/SYSRST#) Pin 15 on the compact 20 pin TI target connector is connected to pin 15 of the (SRST/ARM_RSTn) 20 pin ARM target connector. TCK and TCKRET are buffered.
Q: What is the SRST pin for?
- A: SRST is the System Reset (Emulation) signal. If tied to the card or device reset line, it allows the debugger to control the reset of the device. For some devices, when debugging boot code the Wait in Reset may use this signal. See System Reset (Emulation) for details on how to use this feature in Code Composer Studio v4.
Q: What is TDIS used for?
- A: XDS emulators can use this pin to detect when the target is disconnected from the emulator. It is usually a pull-up in the emulator and GND on the target. The emulator senses the removal of GND.
Q: Where can I learn about termination and buffering?
- A: Please check chapter 11 and appendix B of SPRU655
Q: I am using MSP430, where do I look?
- A: Please check: JTAG (MSP430)
Debugging connectivity issues
Please go to the topic Debugging_JTAG_Connectivity_Problems
Leave a Comment