JTAG Scan Chain Length

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

JTAG Scan Chain Lengths for processors:


Core/Controller IR length IR Bypass DR Length DR Bypass
6201/6701 8 bits
621x/671x 46 bits
64x+ 38 bits
672x
674x 38 bits
54x
55x 38 bits
55x+ 38 bits
ARM7 4 bits
ARM9 4 bits
ARM11
ARM Cortex M3
ARM Cortex R4
ARM Cortex A8
ARM Cortex A9
ICEPick-B
ICEPick-C
ICEPick-D

Leave a Comment

Comments

Comments on JTAG Scan Chain Length


Koller said ...

We are testing a DSP board with 4 TMS320C6455 1GHz DSPs. The four DSPs are connected to JTAG chain. We have Spectrum Digital XDS510SUSB emulator cable. The SDConfig program reports no fault, but the JTAG chain length is reported 24 four devices. The 24 probably a wrong number, because one DSP IR Length is 38 bit.

The Code Composer Studio cannot connect to the DSPs.

The TCK signal has been check by scope, seems to be all right.

The board was designed according to the current chip errata.

What could be the problem?


--Koller 12:42, 9 February 2010 (CST)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox