JTAG configuration for CCS and Stellaris

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Introduction

This article will explain how to get started with using Code Composer Studio to debug a Stellaris device. For the latest information on CCS support for Stellaris please visit the Stellaris support in CCS topic.

If using XDS emulators, also refer to the Stellaris Emulator Compatibility page

On-Board Emulation connection

To power the Evaluation Board, use the USB cable supplied in the kit. Connect the mini-b (smaller) end of the USB cable to the connector labeled “P4” on the Evaluation Board. Connect the other end (Type A) to a free USB port on your host PC. The USB is capable of sourcing up to 500 mA for each attached device, which is sufficient for the evaluation board. If connecting the board through a USB hub, it must be a powered hub.

New Hardware Wizard
New Hardware Wizard
New Hardware Wizard
New Hardware Wizard
New Hardware Wizard

You have just installed the drivers for “Stellaris Evaluation Board A.” The USB device built into the EVB is a composite USB device. After you click Finish, a Found New Hardware Wizard appears asking to install drivers for another device. This is for the “Stellaris Evaluation Board B” part of the composite USB device. Follow the same instructions as above to install the drivers for this device.

The Found New Hardware Wizard appears one last time. This is to install the drivers for the “Stellaris Virtual COM Port.” Again, follow the same instructions to install the drivers for this device.

Now all of the hardware drivers for the Evaluation Board have been installed. These drivers give the debugger access to the JTAG interface and the host PC access to the Virtual COM Port.


External Emulator Connection

Jumper wire assembly suggestion


For emulator compatibility please check the page Stellaris_Emulator_Compatibility

CCS Setup

Access_Port_Designator

Stellaris is first supported in CCS with v4.1.0. It is recommended that you follow the instructions in the quickstart guide:

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article JTAG configuration for CCS and Stellaris here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox