LPDDR

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   


Contents

Summary

Micron LPDDR.JPG

Low Power Double Data Rate memory (LPDDR) is also called Mobile DDR (MDDR). This form of memory operates at 1.8 volts as opposed to the more traditional 2.5 volts and is commonly used in portable electronics. As with all DDR memory, the double data rate is achieved by transferring data on both clock edges of the device. The following table describes LPDDR in relation to interfacing with the OMAP3530 device.


Supported devices Any JEDEC 209 compliant device
Supported Size Up to 1 Gigabyte
Max Clock Speed 266 MHz* (see note 1)
Device Count 1 or 2* (see note 2)
Data Width (bits) 16 or 32

Note 1: Higher speed grades are supported due to inherent JEDEC LPDDR backwards compatibility
Note 2: 1 x16 LPDDR device is used for 16 bit LPDDR memory system. 1x32 or 2x16 LPDDR devices are used for a 32 bit LPDDR memory system.


Supported Devices

Any JEDEC 209 compliant device.

Related Documents

Please refer to this section of the OMAP3530 data sheet for more details about LPDDR and OMAP3530.
OMAP3530 SDRC

Block Diagrams

Memories.JPG

Example for interfacing to OMAP SDRC

SDRC MDDR.JPG

The following link describes how to connect an external memory module to the OMAP3530 SDRC and calculate the timing parameters for the device.

Connecting a 512MB module to OMAP3530 SDRC (see section 11.2.6.3 Typical SDRC connection to an External SDRAM Device)


A 512 Mb mobile DDR SDRAM memory with the following characteristics has been chosen:

Type Mobile DDR SDRAM
Size 512 Mbits (8M ´ 16 ´ 4 banks)
Data bus 16-bit width
Speed 133-MHz clock frequency, 7.5-ns clock period
Leave a Comment

Comments

Link at bottom is dead: Connecting a 512MB module to OMAP3530 SDRC

Kevinvap said ...

Link is now fixed.

--Kevin Vap 17:11, 15 February 2011 (CST)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox