LPRF BLE Porting Projects

From Texas Instruments Wiki
Jump to: navigation, search

Bluetooth Low Energy Main Page


This wiki page explains necessary steps to port a BLE-Stack v1.x.x project running on a certain stack version to a newer one, and how to port between CC2540 and CC2541 projects.

Known Issues

This section lists the known issues and anomalies that impact the latest release. Issues that are resolved are listed in the release notes of the respective release and will be deprecated from this list.

  • DMA Initialization of VLEN is not correct in the BIM function DMAExecCrc when supporting OAD. This can result in OAD CRC checksum failures in the BIM. To fix, add the following to line 345 of bim_main.c in BLE-Stack 1.4.2:
HAL_DMA_SET_VLEN( dmaCh0_p, HAL_DMA_VLEN_USE_LEN );
  • Connections may drop after connecting with Android 7+ devices. This issues presents when SNV flash memory has high utilization from either large numbers of pairing / bonding sequences and/or high write usage of customer NV IDs. These operations can lead to large numbers of discarded records and excessive SNV record lookup times which can impact protocol stack realtime operations during a connection. To fix, apply the optimization to the findItem() function as described and attached in this E2E forum post.
  • A Slave initiated L2CAP Connection Parameter Update request via GAP_UpdateLinkParamReq will not be processed by the CC254x's BLE slave stack if the requested connection interval (CI) min/max range does not contain a range value that is a multiple of the current CI. The workaround is for the slave to request a min/max CI range that contains a multiple of the current CI. For example, if the current CI is 11.25ms, the request range should be min=7.5ms to max=X where X is >= than 22.5ms (2x 11.25ms).
  • The configuration of the PICTL register by HalKeyConfig in Components\hal\target\CC2540USB\hal_key.c is incorrect. Change the following within HalKeyConfig:
    PICTL |= 0x01;                 // P1ICONL: Falling edge ints on pins 0-3.

to

    PICTL |= 0x02;                 // P1ICONL: Falling edge ints on pins 0-3.


Porting BLEv1.4.1 Projects to BLEv1.4.2

BLE v1.4.2 is a BLE-Stack maintenance release to the v1.4.1 release with all bug fixes applied in the protocol stack libraries. Refer to the release notes for a detailed list of changes in this release. Compared to the previous BLE v1.4.1 release, there are no API or SDK source code changes in BLE v1.4.2. Therefore, no application or project file porting is required when upgrading a project running BLE v1.4.1 to v1.4.2.
All documentation and examples from BLE v1.4.1 apply to BLE v1.4.2.
1. If the current project is based on a BLE-Stack SDK release prior to BLE v1.4.1 (for example, BLE v1.4.0), then follow the below porting instructions to first port your project to BLE v1.4.1. The following steps apply to projects already running BLE v.1.4.1.
2. Copy all library files from the BLE v1.4.2 SDK to the existing BLE v1.4.1 SDK installation. The libraries are located at: $1.4.2_INSTALL$\Projects\ble\Libraries Where the default $1.4.2_INSTALL$ path is C:\Texas Instruments\BLE-CC254x-1.4.2.2. The entire v1.4.2 'Libraries' folder may be copy / pasted to the v1.4.1 installation.
3. Rebuild the project to link to the updated BLE v1.4.2 protocol stack libraries.

Porting BLEv1.4.0 Projects to BLEv1.4.1

Project Porting Directions


1. Move (or Copy) the project files from $1.4.0_INSTALL$\Projects\ble\$PROJECT$ to $INSTALL\Projects\ble\$PROJECT$ where $1.4.0_INSTALL$ is the top level installation directory of the 1.4.0 stack, $INSTALL$ is the top level installation directory of the 1.4.1 stack, and $PROJECT$ is your project folder.
2. If you modified any files from anywhere outside of the application folder, such as in the profiles at $1.4.0_INSTALL$\Projects\Profiles, you will need to merge your changes with the new 1.4.1 version.
3. Open your project (now in the 1.4.1 folder) with IAR 9.10.3.
4. When prompted, choose yes to convert for use with new version.
5. In the Project options, in the Preprocessor options under the C/C++ Compiler tab, add “CC254x” to the controller include path: $PROJ_DIR$\..\..\..\..\Components\ble\controller\CC254x\include
6. For any profiles, add the CC254x include path. Do not delete the original paths as they are still needed. Using SimpleBLEPeripheral as an example, add the following paths: $PROJ_DIR$\..\..\Profiles\SimpleProfile\CC254x $PROJ_DIR$\..\..\Profiles\Roles\CC254x However, do not delete the original paths: $PROJ_DIR$\..\..\Profiles\SimpleProfile $PROJ_DIR$\..\..\Profiles\Roles
7. Replace the .c files that were affected by the changes in step 6 by deleting the old reference and adding the new file. For example, delete peripheral.c from the SimpleBLEPeripheral project (under the PROFILES group). Then add peripheral.c from $INSTALL$\Projects\ble\Profiles\Roles\CC254x.
8. Compile and save your project.

API Changes

The following API's are now abstracted through gattservapp_util.c:

extern void GATTServApp_InitCharCfg( uint16 connHandle, gattCharCfg_t *charCfgTbl );
extern uint16 GATTServApp_ReadCharCfg( uint16 connHandle, gattCharCfg_t *charCfgTbl );
extern bStatus_t GATTServApp_ProcessCharCfg( gattCharCfg_t *charCfgTbl, uint8 *pValue, uint8 authenticated, gattAttribute_t *attrTbl, uint16 numAttrs, uint8 taskId, pfnGATTReadAttrCB_t pfnReadAttrCB );
extern bStatus_t GATTServApp_ProcessCCCWriteReq( uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint8 len, uint16 offset, uint16 validCfg );

Therefore, the following file should be added to your project (preferably under the PROFILES group for consistency): $INSTALL$\Projects\ble\Profiles\GATT\ gattservapp_util.c

An additional "method" parameter has been added to profiles' read and write callback functions that are registered with GATTServApp_RegisterService() to indicate the type of read / write message.

typedef bStatus_t (*pfnGATTReadAttrCB_t)( uint16 connHandle, gattAttribute_t *pAttr,
                                          uint8 *pValue, uint8 *pLen, uint16 offset,
                                          uint8 maxLen, uint8 method );
 
typedef bStatus_t (*pfnGATTWriteAttrCB_t)( uint16 connHandle, gattAttribute_t *pAttr,
                                           uint8 *pValue, uint8 len, uint16 offset,
                                           uint8 method );

Also, the GAP_RegisterForHCIMsgs( ) command has been changed to GAP_RegisterForMsgs().


Typedef Changes

The Central Event Callback function in the Central GAPRole has changed from:

typedef void (*pfnGapCentralRoleEventCB_t)
(
  gapCentralRoleEvent_t *pEvent         //!< Pointer to event structure.
);

to:

typedef uint8 (*pfnGapCentralRoleEventCB_t)
(
  gapCentralRoleEvent_t *pEvent         //!< Pointer to event structure.
);

Structure Changes

Array Elements Changed to Pointers

In order to prepare for a possible future fragmentation implementation, GATT / ATT payload structures are no longer fixed sized arrays and are now pointers. Therefore, the payload is allocated based on its length. This means that the names of all payload elements in the structures in att.h and gatt.h have changed. A “p” has been added in front of the old array name and the next letter has been capitalized.

typedef struct
{
  uint16 handle;               //!< Handle of the attribute to be written (must be first field)
  uint16 offset;               //!< Offset of the first octet to be written
  uint8 len;                   //!< Length of value
  uint8 value[ATT_MTU_SIZE-5]; //!< Part of the value of the attribute to be written
} attPrepareWriteReq_t

has been changed to:

typedef struct
{
  uint16 handle; //!< Handle of the attribute to be written (must be first field)
  uint16 offset; //!< Offset of the first octet to be written
  uint8 len;     //!< Length of value
  uint8 *pValue; //!< Part of the value of the attribute to be written (0 to ATT_MTU_SIZE-5) - must be allocated
} attPrepareWriteReq_t;


Macro’s have been added which can be used to access offsets from these pointer locations. For example,

typedef struct
    // Service found, store handles
    if ( pMsg->method == ATT_FIND_BY_TYPE_VALUE_RSP &&
         pMsg->msg.findByTypeValueRsp.numInfo > 0 )
    {
      simpleBLESvcStartHdl = pMsg->msg.findByTypeValueRsp.handlesInfo[0].handle;
      simpleBLESvcEndHdl = pMsg->msg.findByTypeValueRsp.handlesInfo[0].grpEndHandle;
    }

has been changed to:

    // Service found, store handles
    if ( pMsg->method == ATT_FIND_BY_TYPE_VALUE_RSP &&
         pMsg->msg.findByTypeValueRsp.numInfo > 0 )
    {
      simpleBLESvcStartHdl = ATT_ATTR_HANDLE(pMsg->msg.findByTypeValueRsp.pHandlesInfo, 0);
      simpleBLESvcEndHdl = ATT_GRP_END_HANDLE(pMsg->msg.findByTypeValueRsp.pHandlesInfo, 0);
    }

where the macro's used are defined as:

#define ATT_ATTR_HANDLE( info, i )         ( BUILD_UINT16( (info)[ATT_ATTR_HANDLE_IDX((i))], \
                                                           (info)[ATT_ATTR_HANDLE_IDX((i))+1] ) )
#define ATT_GRP_END_HANDLE( info, i )      ( BUILD_UINT16( (info)[ATT_GRP_END_HANDLE_IDX((i))], \
                                                	           (info)[ATT_GRP_END_HANDLE_IDX((i))+1] ) )

Additional Fields in Key Distribution Strucutre

The keyDist_t has several added fields which were previously reserved. These are needed for interoperability with Bluetooth 4.1 Security features. See an example of how to use this in the 1.4.1 HostTestRelease project.

typedef struct
{
  unsigned int sEncKey:1;    //!< Set to distribute slave encryption key
  unsigned int sIdKey:1;     //!< Set to distribute slave identity key
  unsigned int sSign:1;      //!< Set to distribute slave signing key
  unsigned int sLinkKey:1;   //!< Set to derive slave link key from slave LTK
  unsigned int sReserved:4;  //!< Reserved for slave - don't use
  unsigned int mEncKey:1;    //!< Set to distribute master encryption key
  unsigned int mIdKey:1;     //!< Set to distribute master identity key
  unsigned int mSign:1;      //!< Set to distribute master signing key
  unsigned int mLinkKey:1;   //!< Set to derive master link key from master LTK
  unsigned int mReserved:4;  //!< Reserved for master - don't use
} keyDist_t;


Default Value of HAL Components

The default values of HAL components, if not defined, have changed. See the hal_board_cfg.h file for a list of the default values. If you need to modify any of these, add a preprocessor definition. For example, HAL_KEY is now set to TRUE if not defined. Therefore, the SimpleBLEPeripheral project has added a new preprocessor definition: HAL_KEY=FALSE.


Allocating Memory for Over-the-Air Messages

As stated above, there have been changes made to prepare for a possible future fragmentation implementation. Therefore, it is now necessary to allocate memory for data sent over-the-air for ATT / GATT commands.
For example, a buffer must be allocated when sending a GATT_Notification. Note that this is done by the stack if the preferred method to send a GATT notification / indication is to used. That is, using a profile’s SetParameter function (i.e. SimpleProfile_SetParameter()) and calling GATTServApp_ProcessCharCfg(). See the simpleGATTProfile.c for an example of this.
If using GATT_Notification() or GATT_Indication() directly, this memory management will need to be added:
1. Attempt to allocate memory for the notification / indication using GATT_bm_alloc().
2. If allocation succeeds, send notification / indication using GATT_Notification() / GATT_Indication().
3. If the return value of the notification / indication is SUCCESS (0x00), this means the memory was freed by the stack. If the return value is something other than SUCCESS (i.e. blePending), free the memory using GATT_bm_free(). There is an example of this in the gattServApp_SendNotiInd() function in gattservapp_util.c:

  noti.pValue = (uint8 *)GATT_bm_alloc( connHandle, ATT_HANDLE_VALUE_NOTI,
                                        GATT_MAX_MTU, &len );
  if ( noti.pValue != NULL )
  {
    status = (*pfnReadAttrCB)( connHandle, pAttr, noti.pValue, &noti.len, 
                               0, len, GATT_LOCAL_READ );
    if ( status == SUCCESS )
    {
      noti.handle = pAttr->handle;
 
      if ( cccValue & GATT_CLIENT_CFG_NOTIFY )
      {
        status = GATT_Notification( connHandle, &noti, authenticated );
      }
      else // GATT_CLIENT_CFG_INDICATE
      {
        status = GATT_Indication( connHandle, (attHandleValueInd_t *)&noti,
                                  authenticated, taskId );
      }
    }
 
    if ( status != SUCCESS )
    {
      GATT_bm_free( (gattMsg_t *)&noti, ATT_HANDLE_VALUE_NOTI );
    }
  }
  else
  {
    status = bleNoResources;
  }

This will need to be done for other GATT messages also.

Allocation of Client Characteristic Configuration Table

The client characteristic configuration descriptors (CCCD's) are now initialized as pointers which must be allocated. For example, the CCCD for simpleProfileCharacteristic 4 is declared as a pointer in simpleGATTprofile.c:

static gattCharCfg_t *simpleProfileChar4Config

This must then be allocated when the profile is added to the application (in SimpleProfile_AddService()):

bStatus_t SimpleProfile_AddService( uint32 services )
{
  uint8 status;
 
  // Allocate Client Characteristic Configuration table
  simpleProfileChar4Config = (gattCharCfg_t *)osal_mem_alloc( sizeof(gattCharCfg_t) *
                                                              linkDBNumConns );
  if ( simpleProfileChar4Config == NULL )
  {     
    return ( bleMemAllocError );
  }



Porting BLEv1.3.2 Projects to BLEv1.4.0

  1. Move (or Copy) the project files from C:\Texas Instruments\BLE-CC254x-1.3.2\Projects\ble\$PROJECT$ to C:\Texas Instruments\BLE-CC254x-1.3\Projects\ble\$PROJECT$ where $PROJECT$ is your project folder.
  2. If you modifed any files from C:\Texas Instruments\BLE-CC254x-1.3.2\Projects\Profiles, you will need to merge your changes with the new 1.4.0 version.
  3. Open your project (now in the 1.4.0 folder) with IAR 8.20.
  4. When prompted, choose yes to convert for use with new version.
  5. Compile and save your project.

You should be aware of two project-specific changes:

  • The functionality of the PLUS_BROADCASTER define has changed so that the peripheralBroadcaster.c and peripheralBraodcaster.h files are no longer needed.  See the modified simpleBLEperipheral project for how to accomodate this.
  • Advertising will now begin again after a connection is dropped by default.  To remove this, comment out line 1021 of peripheral.c (shown below):

                  VOID osal_set_event( gapRole_TaskID, START_ADVERTISING_EVT );

  • All UUID's are now stored in centralized locations: gatt_uuid.h and gatt_profile_uuid.h

Also, the following API's have changed:

  • extern bStatus_t GAP_TerminateLinkReq( uint8 taskID, uint16 connectionHandle, uint8 reason );  
        - the third parameter "reason" has been added to allow the application to indicate the termination reason to the connected device
  • the GAPBondMgr_ProcessGAPMsg( gapEventHdr_t *pMsg ) function is no longer a void-type function. It returns a uint8 which indicates TRUE if safe to deallocate the incoming GAP message and FALSE otherwise




Porting BLEv1.2 Projects to BLEv1.3

  1. Move (or Copy) the project files from C:\Texas Instruments\BLE-CC254x-1.2\Projects\ble to C:\Texas Instruments\BLE-CC254x-1.3\Projects\ble
  2. Move (or Copy) the necessary profiles from C:\Texas Instruments\BLE-CC254x-1.3\Projects\ble\Profiles to C:\Texas Instruments\BLE-CC254x-1.3\Projects\ble\Profiles
  3. Open the project and in the LIB group of the project.
    1. Remove all files
    2. Add CC254x_BLE.lib (or GAP role specific, for a more memory optimized library)
    3. Add CC254x_BLE_HCI_TL_None.lib for SoC solutions
  4. Add NPI group (Right click in the workspace > "Add" > "Add Group..."). Add files npi.h, npi.c (npi_uart.c and npi_spi.c as well if needed)
  5. Go to "Project" > "Options" > "General Options" > "Target" > "Number of virtual registers": Set number to 16
  6. Go to "Project" > "Options" > "C/C++ Compiler" > "Additional include directories": Add the line $PROJ_DIR$\..\..\common\npi\npi_np
  7. Done




Porting from CC2540 to CC2541 Project

This section will describe how to port a CC2540 Project to work on a CC2541. Similar steps can be taken for the reverse direction.
1. Create and select a new CC2540 project configuration based on the CC2541 configuration under Project -> Edit Configurations:
Step1.png

2. In the project options, under general options, in the target tab, change the “Device” to CC2540F256:
Step2 porting.png

3. Under C/C++ Compiler, in the Preprocessor tab, define CC2540 (and make sure CC2541 is not defined):
Step3 porting.png

4. In the Workspace pane, under the TOOLS group, open buildConfig.cfg, and comment out the CC2541 define:
Step4 porting.png

5. In the Workspace pane, under the LIB group, exclude the 2541 library by right clicking on CC2541_BLE_peri.lib and selecting options. Then check “Exclude from build:”
Step5 porting.png

6. Add the CC2540_BLE_peri.lib to the library group:
Step6 porting.png

7. You also have to ensure to exclude the CC2540 library from the other CC2541 configurations.