Leopard Board DM355 Hardware Setup

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Setting up the Hardware

Follow the steps below to setup the hardware and enable communication with the Leopard Board. Verify that the Leopard Board's SW1 (boot from nand flash) switch is correctly set. Both positions to on.


Pin # 1 2
Position 1 1


Leopard-uart.jpg
Leopard-ethernet.jpg
To power through USB: Connect the mini-B USB cable. The mini-B end to the J11 of Leopard Board and the type-A end to a USB port
Or Connect the power cable to the power jack on the board. To be safe, plug in the other end of the power cable only after you have connected the power cord to the board.
Leopard-power.JPG

Connecting to a Console Window

You can open a console window that allows you to watch and interrupt the board's boot messages.

Steps to communicate with the board

1. Connect a serial cable between the serial port on the Leopard Board and the serial port (for example COM1) on a PC.

2. Run a terminal session (such as Minicom on Linux or TeraTerm on Windows) on the workstation and configure it to connect to that serial port with the following characteristics:

Bits per Second: 115200
Data Bits: 8
Parity: None
Stop Bits: 1
Flow Control: None
Transmit delay: 0 msec/char, 100 msec/line
Serial Device : /dev/ttyS0 (the device can change)

3. When you power on the Leopard Board, you will see boot sequence messages (If you have a boot loader in flash. If you do not have a boot loader in flash see the section). You can press a key to interrupt the boot sequence and type commands in the U-Boot command shell.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox