Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Linux Core I2C User's Guide

From Texas Instruments Wiki
Jump to: navigation, search

Introduction

The device contains high-speed (HS) inter-integrated circuit (I2C) controllers (I2Ci modules, where i = 1, 2, 3 ...), each of which provides an interface between a local host (LH), such as a digital signal processor (DSP), and any I2C-bus-compatible device that connects through the I2C serial bus. External components attached to the I2C bus can serially transmit and receive up to 8 bits of data to and from the LH device through the 2-wire I2C interface.

Each HS I2C controller can be configured to act like a slave or master I2C-compatible device. I2C controllers can work at different frequencies such as 100 KHz, 400 KHz and 3.4 MHz.

For more info, refer to the I2C controller chapter in the respective SOC TRM.

Setting up

Omap I2C is enabled by default in omap2plus_defconfig.

Testing

 Test1:
   Check for the following in the boot log
   omap_i2c reg.i2c: bus0 rev0.12 at X KHz
 Test2:
   Use the following utilities to check the i2c functionality.
   i2cdump -f -y bus slaveaddr b
      This will dump the register content of the slave at respective bus.
   i2cset -f -y bus slaveaddr register value b
      This will write a 'value' to the 'register' of the device with address 'slaveaddr'.
   i2cget -f -y bus slaveaddr register b
      This will read from the 'register' of the device with address 'slaveaddr'.
   Above testing helps if the slave address clocks are enabled and you can use the
   above tools to quickly get/set the value to just sanity check the i2c functionality.
 Test3:
     Check for the devices connected to the I2C.
     Run tests applicable for those devices to see if I2c read/write works fine.