Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Linux Core QSPI User's Guide

From Texas Instruments Wiki
Jump to: navigation, search

Introduction

Quad Serial Peripheral Interface(QSPI) is a SPI module that allows single, dual and quad read access to external SPI devices. This module has a memory mapped register interface, which provides a direct interface for accessing data from external SPI devices and thus simplifying software requirements. The QSPI works as a master only. The one QSPI in the device is primarily intended for fast booting from quad-SPI flash memories.
This user guide applies to kernel v4.9 and higher.
Top level kernel user's guide can be found at: http://processors.wiki.ti.com/index.php/Linux_Kernel_Users_Guide

Supported Devices

  • AM437x SK and AM437x IDK
  • DRA74x/DRA72x/DRA71x EVM
  • AM57x IDK

Hardware features

The QSPI supports the following features:

  • General SPI features:
     – Programmable clock divider
     – Six pin interface
     – Programmable length (from 1 to 128 bits) of the words transferred
     – Programmable number (from 1 to 4096) of the words transferred
     – 4 external chip-select signals
     – Support for 3-, 4-, or 6-pin SPI interface
     – Optional interrupt generation on word or frame (number of words) completion
     – Programmable delay between chip select activation and output data from 0 to 3 QSPI clock cycles
     – Programmable signal polarities
     – Programmable active clock edge
     – Software-controllable interface allowing for any type of SPI transfer
     – Control through L3_MAIN configuration port
   • Serial flash interface (SFI) features:
     – Serial flash read/write interface
     – Additional registers for defining read and write commands to the external serial flash device
     – 1 to 4 address bytes
     – Fast read support, where fast read requires dummy bytes after address bytes; 0 to 3 dummy bytes
       can be configured.
     – Dual read support
     – Quad read support
     – Little-endian support only
     – Linear increment addressing mode only

Driver Features

Supported Features

Following features are supported by QSPI driver:

Memory mapped read support

TI QSPI controller provides memory map port to read data from SPI flashes. Memory map port is enabled in QSPI_SPI_SWITCH_REG register. Control module register may also need to be accessed for DRA7xx. The QSPI_SPI_SETUP_REGx needs to be populated with flash specific information like read opcode, read mode(quad, dual, normal), address width and dummy bytes. Once, controller is in memory map mode, the whole flash memory is available as a memory region at SoC specific address. This region can be accessed using normal memcpy() (or mem-to-mem dma copy). The ti-qspi controller hardware will internally communicate with SPI flash over SPI bus and get the requested data.

Supported bus widths

  • Single bit write mode
  • Single bit read mode
  • Dual bit read mode
  • Quad bit read mode

Supported SPI modes

QSPI supportes all clock and polarity modes defined in table SPI Clock Modes Definition of particular SoC's TRM. But make sure that the selected mode is supported by the clocking requirements of the device as per the device's datasheet.

DMA support

Driver uses mem-to-mem DMA copy on top QSPI memory mapped port during read from flash for maximum throughput and reduced CPU load.

Hardware Architecture

The QSPI is composed of two blocks. The first one is the SFI memory-mapped interface (SFI_MM_IF) and the second one is the SPI core (SPI_CORE). The SFI_MM_IF block is associated only with SPI flash memories and is used for specifying typical for the SPI flash memories settings (read or write command, number of address and dummy bytes, and so on) unlike the SPI_CORE block, which is associated with the SPI interface itself and is used to configure typical SPI settings (chip-select polarity, serial clock inactive state, SPI clock mode, length of the words transferred, and so on).
The SFI_MM_IF comprises the following two subblocks:

  • SFI register control
  • SFI translator

The SPI_CORE comprises the following four subblocks:

  • SPI control interface (SPI_CNTIF)
  • SPI clock generator (SPI_CLKGEN)
  • SPI control state machine (SPI_MACHINE)
  • SPI data shifter (SPI_SHIFTER)

In addition, an interface bridge connects the two ports (configuration port and memory-mapped port) of the SFI_MM_IF block to the L3_MAIN interconnect. There are no software controls associated with this interface bridge. The QSPI supports long transfers through a frame-style sequence. In its generic SPI use mode, a word can be defined up to 128 bits and multiple words can be transferred during a single access. For each word, a device initiator must read or write the new data and then tell the QSPI to continue the current operation. Using this sequence, a maximum of 4096 128-bit words can be transferred in a single SPI read or write operation. This allows great flexibility when connecting the QSPI to various types of devices.

As opposed to the generic SPI use mode, the communication with serial flash-type devices requires sending a byte command, followed by sending bytes of data. Commands can be sent through the SPI_CORE block to communicate with a serial flash device; however, it is easier to do this using the SFI_MM_IF block because it is intended to ease the communication with serial flash devices. If the SPI_CORE is used to communicate with a serial flash device, software must load the command into the SPI data transfer register with additional configuration fields, perform the byte transfer, then place the data to be sent (or configure for receive) along with additional configuration fields, and perform that transfer. Reads and writes to serial flash devices are more specific. First, the read or write command byte is sent, followed by 1 to 4 bytes of address (corresponding to the address to read/write), then followed by the data write/receive phase. Data is always sent byte oriented. When the address is loaded, data can be continuously read or written, and the address will automatically increment to each byte address internally to the serial flash device. See memory mapped read for more info


QSPI Block Diagram

Driver Architecture

Following diagram shows the QSPI driver stack:

QSPI software stack

QSPI driver can be use both to access SPI flash devices via mtd subsystem or access generic SPI devices (like SPI touchscreen) via SPI framework.

Driver Configuration

Source Location

The source file for QSPI driver can be found at: drivers/spi/spi-ti-qspi.c under Linux kernel source tree.

Kernel Configuration Options

The driver can be built into the kernel or can be compiled as module and loaded into the kernel dynamically.

Enabling QSPI Driver Configurations

Following needs to be enabled to access QSPI flash: TI QSPI controller driver, SPI NOR framework and MTD M25P80 generic serial flash driver in the kernel via menuconfig.

start Linux Kernel Configuration tool.

    $ make menuconfig  ARCH=arm

To enable QSPI controller driver:

          Device Drivers  --->
           [*] SPI support  --->
             <*>   DRA7xxx QSPI controller support

To enable SPI NOR framework:

          Device Drivers  --->
            <*> Memory Technology Device (MTD) support  --->
              <*>   SPI-NOR device support  --->  

To enable M25P80 generic SPI flash driver:

          Device Drivers  --->
            <*> Memory Technology Device (MTD) support  --->
              Self-contained MTD device drivers  ---> 
                <*> Support most SPI Flash chips (AT26DF, M25P, W25X, ...)

To enable them as module make <*> as <M>

Enabling UBIFS filesystem support:

          File systems  --->
            [*] Miscellaneous filesystems  --->
              <*>   UBIFS file system support

DT Configuration

Refer to Documentation/devicetree/bindings/spi/ti_qspi.txt under kernel source tree for QSPI controller driver's DT bindings and their usage.
For generic SPI bus related DT bindings refer to: Documentation/devicetree/bindings/spi/ti_qspi.txt
To configure QSPI flash partitions and flash related DT bindings refer to: Documentation/devicetree/bindings/mtd/jedec,spi-nor.txt and Documentation/devicetree/bindings/mtd/partition.txt

Driver Usage

Load QSPI module using modprobe (this will take care of dependencies and load those modules as well)

   $modprobe spi-ti-qspi

This should create /dev/mtdX entries for every partitions defined in DT or via command line arguments. To see all MTD partitions in the system run:

   $cat /proc/mtd
    dev:    size   erasesize  name
    mtd0: 00080000 00010000 "QSPI.U_BOOT"
    mtd1: 00080000 00010000 "QSPI.U_BOOT.backup"
    mtd2: 00010000 00010000 "QSPI.U-BOOT-SPL_OS"
    mtd3: 00010000 00010000 "QSPI.U_BOOT_ENV"
    mtd4: 00010000 00010000 "QSPI.U-BOOT-ENV.backup"
    mtd5: 00800000 00010000 "QSPI.KERNEL"
    mtd6: 036d0000 00010000 "QSPI.FILESYSTEM"

Testing

Using mtd-utils

     $ cat /proc/mtd       /* Should list QSPI partitions */
     $ flash_erase  /dev/mtd6 0 0  /* Erase entire /dev/mtd6 */
     $ dd if=/dev/random of=tmp_write.txt bs=1 count=num  /* num = bytes to write to flash */
     $ mtd_debug write /dev/mtd6 0 num tmp_write.txt  /* write to num bytes to flash */
     $ mtd_debug read /dev/mtd6 0 num tmp_read.txt /* /* read to num bytes to flash */
     $ diff tmp_read.txt tmp_write.txt /* should be NULL */

Using dd command

     $ cat /proc/mtd       /* Should list QSPI partitions */
     $ flash_erase  /dev/mtd6 0 0  /* Erase entire /dev/mtd6 */
     $ dd if=/dev/random of=tmp_write.txt bs=1 count=num  /* num = bytes to write to flash */
     $ dd if=tmp_write.txt of=/dev/mtd6 bs=num count=1 /* write to num bytes to flash */
     $ dd if=/dev/mtd6 of=tmp_read.txt bs=num count=1  /* read to num bytes to flash */
     $ diff tmp_read.txt tmp_write.txt /* should be NULL */

Using UBIFS on flash

Make sure UBIFS filesystem is enabled in the kernel refer to this section.

     root~# ubiformat /dev/mtd9
     ubiformat: mtd9 (nor), size 23199744 bytes (22.1 MiB), 354 eraseblocks of 65536 bytes (64.0 KiB), min. I/O size 1 bytes
     libscan: scanning eraseblock 353 -- 100 % complete 
     ubiformat: 354 eraseblocks are supposedly empty
     ubiformat: formatting eraseblock 353 -- 100 % complete 
     root:~# ubiattach -p /dev/mtd9
     [  270.874428] ubi0: attaching mtd9
     [  270.914131] ubi0: scanning is finished
     [  270.921788] ubi0: attached mtd9 (name "QSPI.file-system", size 22 MiB)
     [  270.928405] ubi0: PEB size: 65536 bytes (64 KiB), LEB size: 65408 bytes
     [  270.935210] ubi0: min./max. I/O unit sizes: 1/256, sub-page size 1
     [  270.941491] ubi0: VID header offset: 64 (aligned 64), data offset: 128
     [  270.948102] ubi0: good PEBs: 354, bad PEBs: 0, corrupted PEBs: 0
     [  270.954215] ubi0: user volume: 0, internal volumes: 1, max. volumes count: 128
     [  270.961602] ubi0: max/mean erase counter: 0/0, WL threshold: 4096, image sequence number: 2077421476
     [  270.970887] ubi0: available PEBs: 350, total reserved PEBs: 4, PEBs reserved for bad PEB handling: 0
     [  270.980204] ubi0: background thread "ubi_bgt0d" started, PID 863
     UBI device number 0, total 354 LEBs (23154432 bytes, 22.1 MiB), available 350 LEBs (22892800 bytes, 21.8 MiB), LEB size 65408 bytes (63.9 KiB)
     root:~# ubimkvol /dev/ubi0 -N flash_fs -s 20MiB
     Volume ID 0, size 321 LEBs (20995968 bytes, 20.0 MiB), LEB size 65408 bytes (63.9 KiB), dynamic, name "flash_fs", alignment 1
     root:~# mkdir /mnt/flash
     root:~# mount -t ubifs ubi0:flash_fs /mnt/flash/   
     [  326.002602] UBIFS (ubi0:0): default file-system created
     [  326.008309] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 866
     [  326.027530] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "flash_fs"
     [  326.035157] UBIFS (ubi0:0): LEB size: 65408 bytes (63 KiB), min./max. I/O unit sizes: 8 bytes/256 bytes
     [  326.044615] UBIFS (ubi0:0): FS size: 20341888 bytes (19 MiB, 311 LEBs), journal size 1046528 bytes (0 MiB, 16 LEBs)
     [  326.055123] UBIFS (ubi0:0): reserved for root: 960797 bytes (938 KiB)
     [  326.061610] UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID 828AA98E-3A51-4B35-AD50-9E90144AD4C7, small LPT model
     root:~#

Now you can access filesystem at /mnt/flash/

Limitations

  • The QSPI supports only dual and quad reads. Dual or quad writes are not supported. In addition, there is no "pass through" mode supported where the data present on the QSPI input is sent to its output
  • QSPI IP is designed in such a way that after 4096 word transfer, chip select automatically gets de asserted. As a result of which, the entire flash cannot be read in a single chip select using (Single/Dual/Quad) bit read mode feature. While the serial flash linux framework and flash specification expects the entire read to happen with a single read command in a single chip select. This limitation is not applicable when QSPI is used in memory mapped mode for reads. The QSPI driver by default uses memory mapped reads.
  • For writes QSPI uses normal SPI interface instead of memory mapped mode, this is because there is an explicit write enable command that needs to be sent to flash for every page write (256 bytes) which is not handled by SPI_MM_IF.