Linux by Degrees

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

This is an "as is" document meant for Linux newbies (like myself) who are more comfortable with Code Composer.

Contents

Presentation and Support Files
 


3rd Version now updated for Community Linux (DaVinci_PSP_03.20.00.14), Code Composer V4/V5 on DA830/OMAP-L137/AM1808 EVM's.

The 3 .pdf's (split for filesize)

File:Linuxbydegreesda8x CommunityLinux TMDSOSKL137 25Jul2011 Part1a.pdf

File:Linuxbydegreesda8x CommunityLinux TMDSOSKL137 25Jul2011 Part1b.pdf

File:Linuxbydegreesda8x CommunityLinux TMDSOSKL137 19Jul2011 Part2.pdf

And 2 .zip's with images (split for filesize)

File:LbD files 19Jul2011a.zip

File:LbD files 19Jul2011b.zip

was mostly done on an OMAP-L137/TMS320C6747 Floating Point Starter Kit. I have now evolved to using VMWare Linux images over native WinXP. Archived much of the Montavista information for continuity. Much of the DevRocket functionality can be done with CCSv4/v5.

It has a bit more work with EASY boot.

Hopefully it helps you!


NOTE: ramdisk-base.gz is too large to post (3 Mbyte) in one file.

So you can download the following 3 files into a directory:

File:Ramdisk-base.gz.zip

File:Ramdisk-base.gz.z01.zip

File:Ramdisk-base.gz.z02.zip

Rename ramdisk-base.gz.z01.zip to ramdisk-base.gz.z01 and rename ramdisk-base.gz.z02.zip to ramdisk-base.gz.z02

Unzip ramdisk-base.gz.zip (and WinZip should find the .z01 and .z02 files to give you a single 3 MByte ramdisk-base.gz.txt file)

Rename ramdisk-base.gz.txt to ramdisk-base.gz

Or you can extract from DaVinci-PSP-SDK-03.20.00.05.tgz in http://software-dl.ti.com/dsps/dsps_public_sw/psp/LinuxPSP/DaVinci_03_20/03_20_00_05/index_FDS.html as documented at: http://processors.wiki.ti.com/index.php/GSG:_Setting_up_OMAP-L1/AM1x_Target_File_System#Exporting_a_Shared_File_System_for_Target_Access

ramdisk-base.gz is at: \OMAP-L138_PSP_1_00_00_04\LSP\OMAP_L138_arm_1_00_00_04\DaVinci-PSP-SDK-03.20.00.05\images\fs






2nd Version used an OMAP-L137/TMS320C6747 Floating Point Starter Kit using LSP 2.20.00.03 and MontaVista Pro Version 5.0.

The 2 .pdf's (split for filesize)

File:Linuxbydegreesda8xprimusdskswtools013009Part1.ppt.pdf

File:Linuxbydegreesda8xprimusdskswtools013009Part2.ppt.pdf

It has a bit more work with DSPLINK. The DevRocket is not necessary but convenient.





Original version was done for using DVEVM/DVSDK 1.20.00.10 and MontaVista Pro Version 4.0.1

Again the 2 .pdf's were split for filesize:

File:Linuxbydegreesda8xswtools103108Part1.ppt.pdf

File:Linuxbydegreesda8xswtools103108Part2.ppt.pdf

It has a bit more work with Codec Engine.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox