MSP-EXP430F5438 Experimenter Board

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

The MSP-EXP430F5438 Experimenter Board

The MSP430F5438 Experimenter Board (MSP-EXP430F5438) is a development platform for the latest generation MSP430 MCUs. It features a 100-pin socket which supports the MSP430F5438 (datasheet) and other devices with similar pinout. The socket allows for quick upgrades to newer devices or quick applications changes. It is compatible with many TI low-power RF wireless evaluation modules such as the[1]CC2520EMK. The Experimenter Board helps designers quickly learn and develop using the new F5xx MCUs, which provide the industry’s lowest active power consumption, more memory and leading integration for applications such as energy harvesting, wireless sensing and automatic metering infrastructure (AMI).

A TI Flash Emulation Tool, like the MSP-FET430UIF, is required to program and debug the MSP430 devices on the experimenter board.

Contents

Features

What's Included

Support Software

64-bit Drivers

USB drivers for 64-bit operating systems have not been officially released by Texas Instruments, however unsupported, as-is drivers are available for evaluation use. The below drivers are for use with the MSP-FET430UIF, the MSP-EXP430F5438, and TI's TUSB3410-based EVMs. Please do not contact TI support if you run into any issues. Please provide feedback on the MSP430 Forum.

E2e.jpg For technical support on MSP430 please post your questions on The MSP430 Forum. Please post only comments about the article MSP-EXP430F5438 Experimenter Board here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment

Comments

Comments on MSP-EXP430F5438 Experimenter Board


DanRinkes said ...

Some of the links to the support software in this article are dead. I updated the format to the appropriate wiki format, but the links to slac166l and slac305 point to revisions that no longer exist. These should be on a server that can resolve the latest version without needing to specify it. For example, the link http://www-s.ti.com/sc/techlit/spru360 will resolve to the latest version of that document (which today is SPRU360e.pdf, but in the future might be something different.)

--DanRinkes 10:17, 6 November 2009 (CST)

Blundeen said ...

Does anyone have a PDF version or ORcad version of the schematics for the MSP-EXP430F5438 board they could share with me.

--Blundeen 16:06, 22 April 2011 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox