MSP-FET430UIF

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

The MSP-FET430UIF Development Tool

The MSP-FET430UIF is a powerful flash emulation tool to quickly begin application development on the MSP430 MCU. It includes USB debugging interface used to program and debug the MSP430 in-system through the JTAG interface or the pin saving Spy Bi-Wire (2-wire JTAG) protocol. The flash memory can be erased and programmed in seconds with only a few keystrokes, and since the MSP430 flash is ultra-low power, no external power supply is required.

The debugging tool interfaces the MSP430 to the included integrated software environment and includes code to start your design immediately. The MSP-FET430UIF development tool supports all MSP430 flash devices.

Contents

Features

Documentation

MSP-FET430UIF Troubleshooting

Software Version

What version of the software tool are you using?

It is recommended that only the latest version be installed for proper functionality.

Updating to the latest version fixes bugs in previous releases and provides support for the latest MSP430 devices. Using the latest version will eliminate software variables as a cause of your issue.

Are you using a valid OS?

The USB FET (MSP-FET430UIF) drivers included with the latest IAR Kickstart and the TI Code Composer Studio IDEs support Windows XP, Vista, and Windows 7, both 32-bit and 64-bit versions. All drivers are Microsoft WHQL certified.

Hardware Self Test

When your device is plugged in do the LEDs blink? The pattern should be RED-RED-RED-GREEN and then the green should stay on. This indicates that the device is receiving power.

If the above does not happen: Sometimes updating the firmware will fix this problem, but if not the hardware could be damaged.

2nd PC Test

Have you tried to install the same questionable USB FET on other PCs (using the installation guide steps in appendix C) of the Hardware User's Guide

If your FET works on a second PC the issue probably is a PC driver conflict with your first PC.

Usage History

Was the tool in question ever recognized by any PC? If so were able to successfully program and debug with this tool at any time in the past?

If the tool used to work but no longer responds it could be damaged, or the drivers could have a conflict with newly installed 3rd party software.

Custom Board Comparison

Are you using a TI target board or a custom board design?

Hardware considerations can be ruled out by using a TI target board, available for order at www.MSP430.com

JTAG Connections

If you are using your own board, does your JTAG connections differ in any way from the recommendations we give in the Hardware User's Guide, page 23 (4-wire) or page 24 (2-wire/Spy-Bi-Wire)?

If there are significant differences this could very well be the source of your problem. See the Custom Board Comparison topic above.

New Project Test

After the above steps have been performed please do the following: If you create a new project using the steps in the attached word document (IAR [1], CCE V3 [2], CCS V4) and attempt to load a simple TI code example[3], do you see the same issue? This should rule out software considerations.

Device Manager Comparison

You should have a virtual com port (VCP) entry like the image below under PORTS (COM & LPT) If it does not then right-click and reinstall.

Device Manager

Still having problems?

Please open a new request at TI Support & reply to the Service Request bounce-back email with:


Once the above questions are answered we can identify and rule out any issues regarding:

References

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox