MSP430 COFF Parser

From Texas Instruments Wiki
Jump to: navigation, search

When using the CCS (Code Composer Studio), it is possible to parse the information in the generated COFF output file by using the ofd430. The following mini guide is written by using the CCS v5.2.x.

First of all, make sure that the COFF file format is selected as the output format:

Ccs selecting out coff file.PNG

Then add the following command as post-build step:

"${CG_TOOL_ROOT}/bin/ofd430" -v "${BuildArtifactFileName}" >> coff_parse.txt

Msp430 parse coff.PNG

The command above will also dump the output information into a file called "coff_parse.txt". After the project has been successfully compiled, the result should be available under the build folder.

Coff parse output.PNG