Moving from DSPLink 1 30 to 1 40

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Overview

This page gives information for users attempting to move applications from DSPLink v1.30.xx to v1.40.xx.

Details

Details of changes between v1.30.xx and v1.40.xx are available within ReleaseNotes of each subsequent release.

This page details the changes having significant impact on application writers.

New functionality

New modules and features have been added in the 1.40.xx versions of DSPLink. If the new modules are to be used, their description and usage are documented in the UserGuide document available within the DSPLink release package. New sample applications have also been written to demonstrate the functionality of these new modules. A summary of the major new modules & features added in 1.40.03 is:

Changes required in existing applications

If the user only requires existing features and wants to move from v1.30.xx to v1.40.xx, the subsequent sections detail important points for upgrading the application to the new version

Generic changes

GPP-side changes

DSP-side changes


Other information

Note that this does not cover the complete list, but only summarizes the major changes. For the complete list, you will need to refer to the Release Notes of all intermediate releases as mentioned earlier on this page

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox