OMAP-L1x/C674x/AM1x SoC Architectural Overview

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

System Interconnect Overview


The C674x DSP, ARM9 CPU Cores, System DMA, and device specific peripherals are interconnected within the OMAP-L1x devices by a low latency switch fabric. This switch fabric is described in detail in the subsequent articles.

The major components in the OMAP-L1x devices are:


In each of the below diagrams the Masters (Transaction Initiators) are shown on the left hand side of the diagram, and the Slaves (Transaction Responders) are shown on the right hand side of the diagram. The switch fabric is shown in between the Masters and the Slaves as Switch Central Resources (SCRs) and Bridges (BRs).

The arrows indicate the master/slave relationship. Each arrow originates at a master and terminates at a slave (or group of slaves). The direction of the arrow does not indicate the direction of data flow. Data flow is typically bi-directional for each of the documented bus paths but there are minor exceptions. One example of an exception are the read/write ports of the EDMA3 Transfer Controller. The read port reads data from source memory/peripherals, and the write port writes data to destination memory/peripheral.

Some modules are shown on both sides of SCRs or have multiple instances in the block diagram. This is because select peripherals have both a Master DMA Port as well as one or more slave port(s). This dual port functtonality allows the peripheral to act as both a Master and and Slave. Examples include HPI, USB0, USB1, etc.

On chip/Off chip memory controllers are considered slave end points (targets) and are always shown on the right side of main SCRs. The memory controllers can be classified as one of the following


OMAP-L137 System Interconnect Diagram

OMAP-L137 System Interconnect Diagram


OMAP-L138 System Interconnect Diagram

OMAP-L138 System Interconnect Diagram


Master(s)

Masters (Transaction Initiators) in the OMAP-L1x device are IP modules which are capable of initiating their own read/write transfer requests. This includes both CPUs (ARM9 / C674x DSP Megamodule), System DMAs (EDMA3), and select peripherals that utilize their own Master DMA Ports to initiate their own read/write transfers.


The following Table lists the Masters for the respective OMAP-L1x devices

List of Masters on OMAPL1x/C674x/AM1x
Masters Description OMAP-L137 OMAP-L138
Default Master Priority*

ARM9-I <span style="color: rgb(0,0,255)" />

ARM9 Instruction:Instruction/Program accesses. I-Cache accesses X
X
2

ARM9-D

ARM9 Data Port: Load/Store instructions, D-cache and peripheral register accessess X X
2
C674x DSP Megamodule Master DMA Port (MDMA)

C674x long distances memory access port (i.e. load/stores to external memory and shared RAM outside the DSP Mega Module Memory) and cache controller accesses to external memory and shared RAM.

Note:MDMA is a "port" name, has no relation to EDMA3 or the DSP Megamodule IDMA.

X
X
2
C674x DSP Megamodule Configuration Port (CFG) Provides access to the peripheral configuration bus. (i.e. accesses to McASP, PLLC, other Memory Mapped Peripherals) X
X
2
Ethernet Media Access Controller (EMAC) EMAC Master Port RX/TX DMA engine accesses to internal/external device memory X
X
2
Universal Serial Bus Controller (USB2.0) (VBUS) USB0 Queue Manager access to internal/external device memory
X
X
2
Universal Serial Bus Controller (USB2.0) (CDMA) USB0 internal DMA Master Port: accesses to/from internal/external device memory
X
X
2
Universal Serial Bus Controller (USB1.0) USB1 internal DMA Master Port: Accesses to/from internal/external device memory X
X
2
Host Port Interface (HPI) HPI Internal DMA Master Port: Accesses to/from device internal memory, external memory, and peripheral registers. X
X
2
EDMA3_0_TC0 (RD)** EDMA3_0 Transfer Controller 0 read accesses fromSRCperipheral/memory. EDMA3_0_CC0 Q0 submissions
X
X
0
EDMA3_0 Transfer Controller 0 (write)** EDMA3_0 Transfer Controller 0 write accesses to DSP/peripheral/memory. EDMA3_0_CC0 Q1 submissions X
X
0
EDMA3_0 Transfer Controller 1 (read)** EDMA3_0 Transfer Controller 1 read accesses from SRC peripheral/memory. EDMA3_1_CC0 Q0 submissions

X
X
0
EDMA3_0 Transfer Controller 1(write)** EDMA3_0 Transfer Controller 1 write accesses to DSP/peripheral/memory
X
X 0
EDMA3_0 Transfer Controller 0 (read)**

EDMA3_1 Tranfer Controller 0 read accesses from SRC peripheral/memory


X
0
EDMA3_1 Transfer Controller 1(write)**
EDMA3_1 Transfer Controller 0 write accesses to DST peripheral/memory

X
0
Liquid Crystal Display Controller (LCDC)

LCD DMA Port to read image data from external memory

 OMAPL137/AM17xx/C6747: EMIFB SDRAM, OMAPL138/AM18xx/C6748: mDDR/DDR2

X
X
2
Programmable Realtime Unit 0 (PRU0) PRU0 accesses to/from internal/external device memory and peripheral memory mapped registers (e.g McASP etc)

X
0
Programmable Realtime Unit 1 (PRU1) PRU1 accesses to/from internal/external device memory and peripheral memory mapped registers (e.g McASP etc)
X
0
Seral ATA Controller (SATA) SATA Tx/Rx FIFO Internal DMA port for accessing internal/external device memory

X
2
Video Port Interface (DMA 0) VPIF01 Port to write to memory video data that is input from an external component
X
2
Video Port Interface (VPIF)(DMA 1)) VPIF02 Port to read from memory video data that will be output to an external component
X
2
Universal Parallel Port Controller (uPP) uPP internal DMA Master Port: (DMA Channel I/Q)accesses to/from internal memory/external device memory to recieve/send data on uPPI/O bus

X
0


**TCRD/WR priority cannot be programmed individually. Single priority value controls both TC rd/wr port priority.


Slaves

Slaves (Transaction Request Recipients) in the device are IP modules that accept / service the transfer requests from the masters. Modules that fall under this category are peripherals (such as SPI, McASP, McBSP, UART, I2C, etc) that rely on CPU or EDMA3 to initiate transactions on their behalf. On-chip memory (DSP L1/L2, ARM RAM, Shared RAM) and off-chip memory (SDRAM, DDR2/mDDR, NOR/NAND flash, etc) are also considered to be slave modules.


List of Slaves in OMAPL1x/C674x/AM1x Devices
Masters Description OMAP-L137 OMAP-L138

C674x DSP Megamodule Slave DMA Port (SDMA) <span style="color: rgb(0,0,255)" />

DSP SDMA port allows accessing only the DSP memories. DSPSS registers (e.g. program counter, IDMA, Cache controller, DSP Interrupt Controller, etc) are only accessible by DSP (other masters like ARM and HPI cannot access these registers) X
X

ARM RAM

ARM RAM memory. On-chip/Internal memory X X

ARM ROM / ARM Interrupt Controller

ARM ROM and ARM interrupt controller (Only accessible by ARM) X X

Shared RAM

Accessible by ARM/DSP and all other masters (except LCDC) X X

EMIFA

SDRAM, NOR, NAND flash. Off-chip/External memory X X

EMIFB(SDRAM)

SDRAM. Off-chip/external memory X X

EMIFB(SDRAM)

SDRAM. Off-chip/external memory X X

mDDR/DDR2

mDDR/DDR2. Off-chip/external memory X X

Peripherals

Accesses to all peripheral memory mapped registers, including transmit/recieve registers for serial ports, DMA ports/FIFOs for peripherals like McASP/McBSP, PLL , PSC, master peripheral (EDMA, USB, SATA) configuration registers, etc.
X X


NOTE: Not all masters can access all slaves. For additional details on restrictions, if any, on a particular master's accessibility to a given slave memory/peripheral on the device, please refer to the section on Master/Slave Connectivity.


Switched Central Resource (SCR)

Switch Central Resources provides low-latency interconnectivity between the masters and slaves. SCRs (also called Switch Fabric or crossbars) direct the access requests by providing address decoding, arbitration, and routing of the requests to the various slaves.


For uniquely exclusive master/slave pairs, concurrent transactions can be sent in parallel through and SCR. For example, if a request from the C674x Megamodule to configure the McASP and another request from the ARM to configure the UART arrive at a particular SCR concurrently, both of the requests will pass through the SCR at the same time.

The interconnect of a device typically consists of one or two main SCRs and a number of smaller, satellite SCRs. The main SCR's handle the majority of the traffic and are typically clocked at a higher frequency than the satellite SCRs.

The figure below illustrates one such data flow example, where the highlighted paths are completely independent of each other and will allow true concurrency and parallelism.


SCRconcurrent data movement 
 
SCRConcurrency.png
SCRConcurrencyFootnote.png




Arbitration

Arbitration for the Switch Central Resources is a two layer arbitration scheme which occurs on the burst size boundary. Arbitration occurs when two competing resources attempt concurrent access to the same slave.


Layer 1: Master Priority Level Arbitration Each master in a device is assigned to a system priority level. Following a Power On Reset (POR), each masters priority level is reset to the its default as specified in the System Configuration (SYSCFG) Section of the device System Reference Guide.

All SCRs on the device perform arbitration based on the priority level of the master that sends the read/write access request. System programmers are expected to modify the default priority values in order to fine tune the system for their application requirements.

Level 0: Highest Priority Level
Level 1: 2nd Highest Priority Level
Level 2: 3rd Highest Priority Level
Level 3: 4th Highest Priority Level
Level 4: 5th Highest Priority Level
Level 5: 6th Highest Priority Level
Level 6: 7th Highest Priority Level
Level 7: Lowest Priority Level

If two concurrent requests to the same slave concurrently arrive from masters with different priority levels, the master with the highest priority level wins the arbitration.


Layer 2: Inter-Priority Level Aribitration

Inter-Priority Level Arbitration is implemented as round robin style arbitration. If two concurrent requests to the same slave arrive from masters with the same priority level, round robin arbitration decides which master is allowed to continue with the request, and which master must wait until the SCR is free before continuing with the request.


NOTE:Arbitration/Re-Arbitration occurs at burst size boundaries (or lower if a burst request is not used)



Default Burst Size

A transaction from a master is typically broken down into smaller bursts at the system interconnect level. This is done to increase the collective efficiency of transfers through the interconnect.

Since large burst sizes of higher priority threads will always win arbitration and subsequently block other low priority transactions until they are finished, It is assumed that the system programmer will fine tune the burst size of all the masters in the system. This allows the lower priority requests a chance to win arbitration between contiguous bursts of higher priority requests.

The default burst size for a master is shown in the table below.

Default Burst Size for Master Peripherals on OMAPL1x/c674x/AM1x
Master
Default Burst Size
Fixed/Configurable
DSP MDMA
Load/Store word/double word: 4 / 8 bytes

Cache Victims (MDMA writes): 16 bytes

Cache Misses (MDMA reads): 32 -128 bytes

Case Dependent


DSP CFG

Load/Store word/double word: 4/8 bytes

Case dependent
EDMA3_x_TCx
16/32/64 bytes
Configurable via CFGCHIPx register in the SYSCFG module
USB2.0
64 bytes
Fixed
HPI

4 words (16 bytes)

for HPID accesses

Multiplexed mode w/ auto-increment reads/writes produce 4 word reads/writes.

Multiplexed mode w/ non auto-increment reads/writes produce 1 word reads/writes.


EMAC
64 bytes
Fixed
VPIF
32/64/128/256 bytes
Configurable
SATA
32 bytes
Configurable (in words) 1/2/4/8 words




Bridges

Within the SoC/DSP, individual modules/peripherals/memories (or group of peripherals) may run at different clock rates and may have different bus width interfaces (typically 64 bit and 32 bit buses). Logic is needed to synchronize communication between two modules that operate at different clock rates and/or bus widths. Bridges provide the means of resolving these differences by performing bus-width conversion as well as bus operating clock frequency conversion.

Bridges are also responsible for buffering read and write commands and data. Buffering is implemented with First In First Out (FIFO) style buffering. One implication of this is that any high priority request that is passed into a bridge must wait until the bridge FIFO finishes its previous transactions before it is allowed to continue.

Bridge.PNG

There are two types of Bridges:



There are two main types of buses on the OMAP-L1x/c674x devices:

NOTE: An exception to the above description of buses is the 32-bit bus connecting the EMIFB (SDRAM) controller to the main SCR on the OMAPL137/c6747 family of devices. Even though it is a 32-bit bus, it behaves like the 64-bit bus allowing multiple read and write transactions to occur simultaneously.



Master Slave Connectivity

Not all masters can access all slaves in the device. For a detailed description of which masters can access which slaves, refer to the System Interconnect chapter of the device specific System Reference Guide.

E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article OMAP-L1x/C674x/AM1x SoC Architectural Overview here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox