OMAP-L1x 456MHz GEL
From Texas Instruments Embedded Processors Wiki
Translate this page to
Description
This CCS GEL file can be used to operate the device at the 456MHz OPP. It first adjusts the PMIC via I2C to supply 1.3V to the core logic supply. It then adjusts the CPU frequency to 456MHz.
The GEL was created to work with all OMAP-L13x, AM1x, and C674x devices on LogicPD and Spectrum Digital EVMs.
Download
Use the following GEL file with CCS3.3 or higher to automatically set the voltage and frequency after connecting:
Leave a Comment