OMAP-L1x Debug Gel Files

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Description

This CCS GEL file can be used to debug boot issues, determine ROM revisions, and display other information such as PLL settings.

The GEL was created to work with all OMAP-L13x, AM1x, and C674x devices.

Download

Use the following GEL file with CCS3.3 or higher to display debug information after connecting:

OMAPL1x_debug_v8.zip

Directions

OMAP-L1x-screenshot-ccs3.png

Directions for CCS 3.3


OMAP-L1x-screenshot-ccs4.png

Directions for CCS 4.x and higher


Note: Make sure the MMU is disabled when you run the scripts in order to properly read the registers. You can disable the ARM’s MMU in CCS by going to Tools -> Advanced ARM Features.

The GEL file will print out the following information:

Leave a Comment

Comments

Comments on OMAP-L1x Debug Gel Files


MikeH said ...

OMAPL1x_debug_v7.zip link is pointing to v6.

--MikeH 07:11, 28 September 2011 (CDT)

Stoupa said ...

Hi, there are missing brackets on line 404 in the version 7. It causes freeze (in fact division by zero) in the GEL file when PREDIV enabled.

--Stoupa 12:17, 20 October 2011 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox